8.1. General functions
8.1.1. emInitMonitor
-
EC_T_DWORD emInitMonitor(EC_T_DWORD dwInstanceId, EC_T_MONITOR_INIT_PARMS *pParms)
Initialize EC-Monitor.
- Parameters
dwInstanceId – [in] Instance ID
pParms – [in] Monitor initialization parameters
- Returns
EC_E_NOERROR or error code
-
struct EC_T_MONITOR_INIT_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Set to MONITOR_SIGNATURE
-
EC_T_DWORD dwSize
[in] Set to sizeof(EC_T_MONITOR_INIT_PARMS)
-
EC_T_LOG_PARMS LogParms
[in] Logging parameters
-
EC_T_OS_PARMS *pOsParms
[in] Operation system layer parameters
-
EC_T_LINK_PARMS *pLinkParms
[in] Link layer parameters
-
EC_T_ETHERNET_TAP_TYPE eEthTapType
[in] Type of Ethernet TAP
-
EC_T_DWORD dwBusCycleTimeUsec
[in] Bus cycle time [usec]
-
EC_T_DWORD dwMaxBusSlaves
[in] Maximum pre-allocated bus slave objects
-
EC_T_DWORD dwBacktraceFrames
[in] Number of frames held in backtrace buffer. Total memory requirements of the buffer:
-
EC_T_PERF_MEAS_INTERNAL_PARMS PerfMeasInternalParms
[in] Internal performance measurement parameters
-
EC_T_WORKER_THREAD_PARMS WorkerThreadParms
[in] Internal worker thread parameters
-
EC_T_DWORD dwCommunicationTimeoutMsec
[in] Timeout [msec] for communication on the Ethernet TAP. 0: defaults to 3 sec, EC_WAITINFINITE: disables monitoring
-
EC_T_BOOL bApiLockByApp
[in] EC_TRUE: Don’t lock pending API calls to increase performance
-
EC_T_CHAR szFileStoragePath[EC_FILESTORAGE_PATH_SIZE]
[in] Path used to store records and files, e.g. FoE transfers. EC_NULL: defaults to “”
-
EC_T_MBX_PARMS MbxParms
[in] Mailbox monitoring parameters
-
EC_T_DWORD dwSignature
-
enum EC_T_ETHERNET_TAP_TYPE
Values:
-
struct EC_T_OS_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Set to EC_OS_PARMS_SIGNATURE
-
EC_T_DWORD dwSize
[in] Set to sizeof(EC_T_OS_PARMS)
-
EC_PF_SYSTIME pfSystemTimeGet
[in] Function to get host time in nanoseconds since 1st January 2000. Used as time base for DC Initialization.
-
EC_T_DWORD dwSupportedFeatures
[in/out] reserved
-
EC_PF_HW_TIMER_GET_INPUT_FREQUENCY pfHwTimerGetInputFrequency
[in] Function to get input frequency of HW timer. This function is needed by some DCM modes described in the Class A manual
-
EC_T_DWORD dwSignature
-
struct EC_T_LOG_PARMS
Public Members
-
EC_T_DWORD dwLogLevel
[in] Log level. See EC_LOG_LEVEL_…
-
EC_PF_LOGMSGHK pfLogMsg
[in] Log callback function called on every message
-
EC_T_DWORD dwLogLevel
- group EC_LOG_LEVELS
-
typedef EC_T_DWORD (*EC_PF_LOGMSGHK)(struct _EC_T_LOG_CONTEXT *pContext, EC_T_DWORD dwLogMsgSeverity, const EC_T_CHAR *szFormat, ...)
- Parameters
pContext – [in] Context pointer. This pointer is used as parameter when the callback function is called
dwLogMsgSeverity – [in] Log message severity, EC_LOG_LEVEL_…
szFormat – [in] String that contains the text to be written. It can optionally contain embedded format specifiers that are replaced by the values specified in subsequent additional arguments and formatted as requested.
- Returns
EC_E_NOERROR or error code
-
struct EC_T_PERF_MEAS_INTERNAL_PARMS
Public Members
-
EC_T_BOOL bEnabled
[in] enable/disable internal performance counters.
-
EC_T_PERF_MEAS_COUNTER_PARMS CounterParms
[in] Timer function settings. When not provided OsMeasGetCounterTicks is used
-
EC_T_PERF_MEAS_HISTOGRAM_PARMS HistogramParms
[in] Histogram settings. When not provided the histogram is disabled.
-
EC_T_BOOL bEnabled
-
struct EC_T_PERF_MEAS_COUNTER_PARMS
Public Members
-
EC_PF_PERF_MEAS_GETCOUNTERTICKS pfGetCounterTicks
[in] Function returning the current counter ticks
-
EC_T_UINT64 qwFrequency
[in] Frequency in Hz used by the timer in GetCounterTicks
-
EC_PF_PERF_MEAS_GETCOUNTERTICKS pfGetCounterTicks
-
typedef EC_T_UINT64 (*EC_PF_PERF_MEAS_GETCOUNTERTICKS)(EC_T_VOID *pvContext)
- Parameters
pvContext – [in] Arbitrarily application-defined parameter passed to callback
-
struct EC_T_PERF_MEAS_HISTOGRAM_PARMS
Public Members
-
EC_T_DWORD dwBinCount
[in] amount of bins to use for the histogram.
-
EC_T_UINT64 qwMinTicks
[in] results below qwMinTicks are stored in the first bin
-
EC_T_UINT64 qwMaxTicks
[in] results above qwMaxTicks are stored in the last bin
-
EC_T_DWORD dwBinCount
-
struct EC_T_WORKER_THREAD_PARMS
Public Members
-
EC_T_DWORD dwPrio
[in] Priority to use for the worker thread
-
EC_T_DWORD dwPrio
-
struct EC_T_MBX_PARMS
Public Members
-
EC_T_DWORD dwMemoryPoolSize
[in] Memory for each slave supporting mailbox communication to record e.g. the CoE dictionary. The memory is asynchronously increased by dwBufferSize by the WorkerThread when it is over 80% full. 0: defaults to 1kb
-
struct _EC_T_MBX_PARMS_FOE
Public Members
-
EC_T_BOOL bDisableNotifications
[in] Disable all FoE related EC_NOTIFY_MBOXRCV notifications
-
EC_T_BOOL bDisableFileStorage
[in] Disable storage of FoE transfers as a file on the file system
-
EC_T_DWORD dwMaxQueuedMbxTransfers
[in] Maximum number of queued single FoE mailbox transfers that be used as a file write buffer. 0: defaults to 32
-
EC_T_BOOL bDisableNotifications
-
EC_T_DWORD dwMemoryPoolSize
8.1.2. emDeinitMonitor
-
EC_T_DWORD emDeinitMonitor(EC_T_DWORD dwInstanceId)
Deinitialize EC-Monitor.
- Parameters
dwInstanceId – [in] Instance ID
- Returns
EC_E_NOERROR or error code
8.1.3. emConfigureNetwork
-
EC_T_DWORD emConfigureNetwork(EC_T_DWORD dwInstanceID, EC_T_CNF_TYPE eCnfType, EC_T_PBYTE pbyCnfData, EC_T_DWORD dwCnfDataLen)
Configure EtherCAT network.
- Parameters
dwInstanceID – [in] Instance ID
eCnfType – [in] Type of configuration data provided
pbyCnfData – [in] Configuration data
dwCnfDataLen – [in] Length of configuration data in byte
- Returns
EC_E_NOERROR or error code
8.1.4. emGetMonitorStatus
-
EC_T_DWORD emGetMonitorStatus(EC_T_DWORD dwInstanceID, EC_T_MONITOR_STATUS *pStatus)
Get current Monitor status.
Information about the current status of the EtherCAT frame / cycle processing
- Parameters
dwInstanceID – [in] Instance ID
pStatus – [out] Monitor status descriptor
- Returns
EC_E_NOERROR on success
EC_E_INVALIDSTATE if Monitor isn’t initialized
EC_E_INVALIDPARM if pStatus invalid
-
struct EC_T_MONITOR_STATUS
Public Members
-
EC_T_BOOL bNextFramesReceived
[out] Indicates whether further unprocessed frames form the next EtherCAT cycle were received
-
EC_T_DWORD dwCyclesProcessed
[out] Number of EtherCAT cycles processed
-
EC_T_WORD wEthTapPositionAutoIncAddr
[out] Ethernet tap position as auto increment address
-
EC_T_BOOL bNextCyclicEntryReceived
[out] Indicates whether all frames from the next EtherCAT cycle have been received and have not yet been processed
-
EC_T_BOOL bNextFramesReceived
8.1.5. emSetLicenseKey
-
EC_T_DWORD emSetLicenseKey(EC_T_DWORD dwInstanceID, const EC_T_CHAR *pszLicenseKey)
Sets the license key for the protected version of EC-Master.
Must be called after initialization and before configuration. This function may not be called if a non protected version is used.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pszLicenseKey – [in] License key as zero terminated string with 26 characters.
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_INVALIDSIZE the format of the license key is wrong. The correct length is 26 characters
EC_E_LICENSE_MISSING the license key doesn’t match to the MAC Address
Example
dwRes = emSetLicenseKey(dwInstanceId, "DA1099F2-15C249E9-54327FBC");
if (dwRes != EC_E_NOERROR)
{
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "ERROR: Cannot set license key: %s (0x%lx))\n",
ecatGetText(dwRes), dwRes));
}
See also
8.1.6. emRegisterClient
-
EC_T_DWORD emRegisterClient(EC_T_DWORD dwInstanceID, EC_PF_NOTIFY pfnNotify, EC_T_VOID *pCallerData, EC_T_REGISTERRESULTS *pRegResults)
Registers a client on the EC-Master.
It must be called after configuration, otherwise the registration handle is lost. This function may not be called from within the JobTask’s context.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pfnNotify – [in] Notification callback function. This function will be called every time a state change occurs, an error occurs or a mailbox transfer terminates.
pCallerData – [in] Pointer to a caller data area which will be passed to the client on every notification callback.
pRegResults – [out] Registration results, a pointer to a structure of type EC_T_REGISTERRESULTS.
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_NOMEMORY if some memory cannot be allocated
-
typedef EC_T_DWORD (*EC_PF_NOTIFY)(EC_T_DWORD dwCode, EC_T_NOTIFYPARMS *pParms)
- Parameters
dwCode – [in] Notification code, see EC_NOTIFY_…, e.g. EC_NOTIFY_STATECHANGED
pParms – [in] Notification code depending data.
-
struct EC_T_REGISTERRESULTS
Public Members
-
EC_T_DWORD dwClntId
[out] Client ID
-
EC_T_BYTE *pbyPDIn
[out] Pointer to process data input memory
-
EC_T_DWORD dwPDInSize
[out] Size of process data input memory (in bytes)
-
EC_T_BYTE *pbyPDOut
[out] Pointer to process data output memory
-
EC_T_DWORD dwPDOutSize
[out] Size of process data output memory (in bytes)
-
EC_T_DWORD dwClntId
8.1.7. emUnregisterClient
-
EC_T_DWORD emUnregisterClient(EC_T_DWORD dwInstanceID, EC_T_DWORD dwClntId)
Unregister a client from the EtherCAT master.
This function may not be called from within the JobTask’s context.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwClntId – [in] Client ID determined when registering with the master.
- Returns
EC_E_NOERROR or error code
8.1.8. emGetSrcMacAddress
-
EC_T_DWORD emGetSrcMacAddress(EC_T_DWORD dwInstanceID, ETHERNET_ADDRESS *pMacSrc)
Gets the source MAC address.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMacSrc – [out] 6-byte buffer to write source MAC address to.
- Returns
EC_E_NOERROR or error code
See also
8.1.9. emExecJob
-
EC_T_DWORD emExecJob(EC_T_DWORD dwInstanceID, EC_T_USER_JOB eUserJob, EC_T_USER_JOB_PARMS *pUserJobParms)
Execute or initiate the requested master job.
To achieve maximum speed, this function is implemented non re-entrant. It is highly recommended that only one single task is calling all required jobs to run the stack. If multiple tasks are calling this function, the calls have to be synchronized externally. Calling it in a context that doesn’t support operating system calls can lead to unpredictable behavior.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
eUserJob – [in] user requested job
pUserJobParms – [in] optional user job parameters
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_LINK_DISCONNECTED if the link is disconnected
EC_E_FEATURE_DISABLED for eUsrJob_SwitchEoeFrames if EC_IOCTL_SET_EOE_DEFFERED_SWITCHING_ENABLED hasn’t be called before
EC_E_ADS_IS_RUNNING if ADS server is running
Brief job overview:
-
union EC_T_USER_JOB_PARMS
Public Members
-
EC_T_BOOL bAllCycFramesProcessed
-
EC_T_DWORD dwNumFramesSent
-
EC_T_DWORD dwTaskIdToSend
-
struct EC_T_USER_JOB_PARMS::_SEND_CYCFRAME_BY_TASKID SendCycFramesByTaskId
-
struct EC_T_USER_JOB_PARMS::_PROCESS_RXFRAME_BY_TASKID ProcessRxFramesByTaskId
-
struct EC_T_USER_JOB_PARMS::_SWITCH_EOE_FRAMES SwitchEoeFrames
-
struct EC_T_USER_JOB_PARMS::_START_TASK StartTask
-
struct EC_T_USER_JOB_PARMS::_STOP_TASK StopTask
-
struct _SEND_CYCFRAME_BY_TASKID
Public Members
-
EC_T_DWORD dwTaskId
-
EC_T_DWORD dwTaskId
-
struct _START_TASK
Public Members
-
EC_T_DWORD dwTaskId
-
EC_T_DWORD dwTaskId
-
struct _STOP_TASK
Public Members
-
EC_T_DWORD dwTaskId
-
EC_T_DWORD dwTaskId
-
EC_T_BOOL bAllCycFramesProcessed
Detailed job description:
eUsrJob_ProcessAllRxFrames
When the Link Layer operates in polling mode this call will process all currently received frames, when the Link Layer operates in interrupt mode all received frames are processed immediately and this call just returns with nothing done.
pUserJobParms->bAllCycFramesProcessed
This flag is set to a value of
EC_TRUE
it indicates that all previously initiated cyclic frames (eUsrJob_SendAllCycFrames
) are received and processed within this call. Not used if pUserJobParms set toEC_NULL
.Return: EC_E_NOERROR if successful, error code in case of failures.
eUsrJob_MonitorTimer
To trigger the monitor and slave state machines as well as the mailbox handling this call has to be executed cyclically. The monitor cycle time is determined by the period between calling
emExecJob()
(eUsrJob_MonitorTimer
). The state-machines are handling the EtherCAT state change transfers.Return: EC_E_NOERROR if successful, error code in case of failures.
8.1.10. emGetMonitorParms
-
EC_T_DWORD emGetMonitorParms(EC_T_DWORD dwInstanceID, EC_T_MONITOR_INIT_PARMS *pParms, EC_T_DWORD dwParmsBufSize)
Gets current Monitor Init Parameters.
If the given buffer is larger than the actual size of struct EC_T_MONITOR_INIT_PARMS, the parameters of EC_T_MONITOR_INIT_PARMS.pOsParms, EC_T_MONITOR_INIT_PARMS.pLinkParms are appended.
- Parameters
dwInstanceID – [in] Instance ID
pParms – [out] Buffer to store parameters
dwParmsBufSize – [in] Size of buffer in bytes
- Returns
EC_E_NOERROR on success
EC_E_INVALIDSTATE if Monitor isn’t initialized
EC_E_INVALIDPARM if buffer pParms is too small
Example
/* Read all monitor init parameters, including OS and Link parameters */
EC_T_BYTE abyBuffer[sizeof(EC_T_MONITOR_INIT_PARMS) + sizeof(EC_T_OS_PARMS) + 512 /* LinkLayer parameters */];
EC_T_MONITOR_INIT_PARMS* pParms = (EC_T_MONITOR_INIT_PARMS*)abyBuffer;
OsMemset(abyBuffer, 0, sizeof(abyBuffer));
dwRes = emGetMonitorParms(dwInstanceId, pParms, sizeof(abyBuffer));
if (EC_E_NOERROR != dwRes)
{
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "Cannot get monitor parameters: %s (0x%lx))\n",
ecatGetText(dwRes), dwRes));
}
See also
8.1.11. emSetMonitorParms
-
EC_T_DWORD emSetMonitorParms(EC_T_DWORD dwInstanceID, EC_T_MONITOR_INIT_PARMS *pParms)
Change Monitor Init Parameters.
OS parms, Main Link parms cannot be changed.
- Parameters
dwInstanceID – [in] Instance ID
pParms – [in] New Monitor init parameters
- Returns
EC_E_NOERROR on success
EC_E_INVALIDSTATE if Monitor isn’t initialized
See also
8.1.12. emGetVersion
-
EC_T_DWORD emGetVersion(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwVersion)
Gets the version number as a 32-bit value.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwVersion – [out] Pointer to EC_T_DWORD to carry out version number
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
8.1.13. emGetText
-
const EC_T_CHAR *emGetText(EC_T_DWORD dwInstanceID, EC_T_DWORD dwTextId)
Return text tokens by ID.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns
Textual description of the given ID
Since the texts are instance independent, a variant without instance id is also available:
-
const EC_T_CHAR *ecatGetText(EC_T_DWORD dwTextId)
8.1.14. emGetMemoryUsage
-
EC_T_DWORD emGetMemoryUsage(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwCurrentUsage, EC_T_DWORD *pdwMaxUsage)
Returns information about memory usage.
All calls to malloc/free and new/delete are monitored.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwCurrentUsage – [out] Current memory usage in Bytes at the time where this function is called
pdwMaxUsage – [out] Maximum memory usage in Bytes since initialization at the time where this function is called
- Returns
EC_E_NOERROR or error code
8.1.15. emGetMasterState
-
EC_T_STATE emGetMasterState(EC_T_DWORD dwInstanceID)
Get the EtherCAT master current state.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns
EtherCAT master state
8.1.16. emGetMasterStateEx
-
EC_T_DWORD emGetMasterStateEx(EC_T_DWORD dwInstanceID, EC_T_WORD *pwCurrState, EC_T_WORD *pwReqState)
Get the EtherCAT master current and requested state. Possible return values for current and requested state:
DEVICE_STATE_UNKNOWN
DEVICE_STATE_INIT
DEVICE_STATE_PREOP
DEVICE_STATE_SAFEOP
DEVICE_STATE_OP
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pwCurrState – [out] Current master state.
pwReqState – [out] Requested master state
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointers are EC_NULL
Limitation
Since it is not possible to determine the actual requested master state, the highest slave state of all slaves is assumed to be the requested master state.
8.1.17. emFindInpVarByName - “Inputs.DevicesState”
The device status of all slaves (OR-linked) is part of the process data with name “Inputs.DevicesState”.
-
EC_T_DWORD emFindInpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
8.1.18. emFindInpVarByName - “Inputs.BusTime”
The DC system time (written to ESC register 0x0910) is part of the process data with name “Inputs.BusTime”.
-
EC_T_DWORD emFindInpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
8.1.19. emIoControl
With emIoControl
a generic control interface exists between the application and the EC-Monitor and its Link Layers.
-
struct EC_T_IOCTLPARMS
Public Members
-
EC_T_BYTE *pbyInBuf
[in] Pointer to control input parameter.
-
EC_T_DWORD dwInBufSize
[in] Size of the input buffer provided at pbyInBuf in bytes
-
EC_T_BYTE *pbyOutBuf
[out] Pointer to control output buffer where the results will be copied into
-
EC_T_DWORD dwOutBufSize
[in] Size of the output buffer provided at pbyOutBuf in bytes
-
EC_T_DWORD *pdwNumOutData
[out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer
-
EC_T_BYTE *pbyInBuf
8.1.20. emIoControl - EC_IOCTL_REGISTER_CYCFRAME_RX_CB
This function call registers an callback function which is called after the cyclic frame is received. Typically this is used when the Link Layer operates interrupt mode to get an event when the new input data (cyclic frame) is available.
The callback function has to be registered after calling emInitMonitor()
before starting the job task.
- emIoControl - EC_IOCTL_REGISTER_CYCFRAME_RX_CB
- Parameter
pbyInBuf
: [in] Cyclic frame received callback descriptor (EC_T_CYCFRAME_RX_CBDESC)dwInBufSize
: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf
: [out] Should be set to EC_NULLdwOutBufSize
: [in] Should be set to 0pdwNumOutData
: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
-
struct EC_T_CYCFRAME_RX_CBDESC
Public Members
-
EC_T_VOID *pCallbackContext
[in] Context pointer. This pointer is used as parameter every time when the callback function is called
-
EC_PF_CYCFRAME_RECV pfnCallback
[in] This function will be called after the cyclic frame is received, if there is more than one cyclic frame after the last frame. The application has to assure that these functions will not block.
-
EC_T_VOID *pCallbackContext
-
typedef EC_T_VOID (*EC_PF_CYCFRAME_RECV)(EC_T_DWORD dwTaskId, EC_T_VOID *pvContext)
- Parameters
dwTaskId – [in] Task ID of the received cyclic frame
pvContext – [in] Arbitrarily application-defined parameter passed to callback
8.1.21. emIoControl - EC_IOCTL_GET_CYCLIC_CONFIG_INFO
Get cyclic configuration details from ENI configuration file.
- emIoControl - EC_IOCTL_GET_CYCLIC_CONFIG_INFO
- Parameter
pbyInBuf
: [in] Pointer to dwCycEntryIndex: cyclic entry index for which to get informationdwInBufSize
: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf
: [out] Pointer to EC_T_CYC_CONFIG_DESC data typedwOutBufSize
: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData
: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Return
EC_E_NOERROR or error code
-
struct EC_T_CYC_CONFIG_DESC
Public Members
-
EC_T_DWORD dwNumCycEntries
[out] Total number of cyclic entries
-
EC_T_DWORD dwTaskId
[out] Task id of selected cyclic entry
-
EC_T_DWORD dwPriority
[out] Priority of selected cyclic entry
-
EC_T_DWORD dwCycleTime
[out] Cycle time of selected cyclic entry
-
EC_T_DWORD dwNumCycEntries
8.1.22. emIoControl - EC_IOCTL_IS_SLAVETOSLAVE_COMM_CONFIGURED
Determine if any slave-to-slave communication is configured.
- emIoControl - EC_IOCTL_IS_SLAVETOSLAVE_COMM_CONFIGURED
- Parameter
pbyInBuf
: [in] Should be set to EC_NULLdwInBufSize
: [in] Should be set to 0pbyOutBuf
: [out] Pointer to EC_T_DWORD. If value is EC_TRUE slave-to-slave communication is configured, if EC_FALSE it is not.dwOutBufSize
: [in] Size of the output buffer in bytes.pdwNumOutData
: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Return
EC_E_NOERROR or error code