9. Add an additional Ubuntu guest [OPTIONAL]
To clone an existing VM, follow the same steps as described in the Hypervisor manual.
As an alternative to cloning the installed Ubuntu image, it’s also possible to use the ubuntu.iso installation media again – like in the previous chapters – and install it into another guest folder /hv/guests/examples/ubuntu2.
See the Hypervisor manual for more details.
Hint
The same changes of this chapter applies accordingly for more Ubuntu guests (like ubuntu3, ubuntu4, etc).