Index Symbols | E | M | P | R | S | W Symbols /? EcLyser.exe command line option /CAPTURE=”C:/myfile.ecd:0”: EcLyser.exe command line option /ENI=”eni.xml”: EcLyser.exe command line option /HELP EcLyser.exe command line option /LOCAL=”127.0.0.1”: EcLyser.exe command line option /REMOTE=”127.0.0.1:6000:0:0”: EcLyser.exe command line option E EcLyser.exe command line option /? /CAPTURE=”C:/myfile.ecd:0”: /ENI=”eni.xml”: /HELP /LOCAL=”127.0.0.1”: /REMOTE=”127.0.0.1:6000:0:0”: MainDevice instance is set to 0 and protocol is set to RAS. It is also supported to use the DNS name instead of the IP address port is 6000 Runs diagnosis with a remote system Runs diagnosis with the local system and the network adapter with IP address “127.0.01” will be chosen Runs diagnosis with the offline diagnosis system Sets the path to the ENI file which should be used where IP address is “127.0.0.1” where the path to the capture file is :file:`c:/myfile.ecd` and the selected snapshot is “0” M MainDevice instance is set to 0 and protocol is set to RAS. It is also supported to use the DNS name instead of the IP address EcLyser.exe command line option P port is 6000 EcLyser.exe command line option R Runs diagnosis with a remote system EcLyser.exe command line option Runs diagnosis with the local system and the network adapter with IP address “127.0.01” will be chosen EcLyser.exe command line option Runs diagnosis with the offline diagnosis system EcLyser.exe command line option S Sets the path to the ENI file which should be used EcLyser.exe command line option W where IP address is “127.0.0.1” EcLyser.exe command line option where the path to the capture file is :file:`c:/myfile.ecd` and the selected snapshot is “0” EcLyser.exe command line option