emllDpdk

Linux® DPDK. Hardware independent network driver.

See also

User Manual

Supported OS and Arch

Linux

Architecture

ARM_64
x86_64

Interrupt supported

❌

Fingerprint supported

❌

Supported NICs

The following reference Network Interface Cards have been successfully tested.

  • NXP Layerscape 1046A

  • NXP i.MX95

  • Intel Ethernet Network Adapter X710

  • Intel Ethernet-Controller I210

The complete list of NICs supported by DPDK is available at https://core.dpdk.org/supported/nics/