emllFslEnetc

NXP® ENETC4 Ethernet MAC.

See also

User Manual

Supported OS and Arch

Linux

Architecture

ARM_64

Interrupt supported

❌

Fingerprint supported

❌

Supported SoC’s

enum EC_T_FSLENETC_TYPE

Values:

enumerator eFslEnetc_iMX95

ENETC4 MAC on NXP i.MX95

Supported Reference Boards

The following reference boards have been successfully tested and predefined parameter sets in EcSelectLinkLayer.cpp are available.

  • Toradex Verdin iMX95