1.4. Known restrictions
Some SubDevices require extended information to be simulated.
The “<ExtendedInfo>”-Tag in EXI is currently not importable to EC-Engineer and must be removed before importing EXI as ENI file. Simulator settings contained in the extended information are stored in the .ecc file and can be copied between EC-Engineer instances using Copy and Paste.
Value Information (Default, Min, Max) from object dictionary cannot be retrieved using SSC, see SSC\sdoserv : „the transmission of the value info is not supported yet of the sample code”.
Occasional start up error (timeout) in case of DCM Bus Shift (DC control loop not included in EC-Simulator), work-around with OsQueryMsecCount() replacement possible.