2. Part A - Development Host Configuration¶
Start the System Manager
Hint
if it is the first launch of the System Manager a dialog to enter a workspace directory opens.
Select My Computer node on the tree view and add a RTOS to the configuration.
Select the
Application
node of theRTOS #1
section and push theCreate New Application Project (Debug Only)
button.Select for ex. RealtimeDemo and push OK button.
Scroll to
<Development|Debugging>
section and push theSettings
button.Edit DEBUG Connection Settings
dialog will pop up.Select
Remote Debugging
and enter the IP address of the target. Please note, this IP address must not be in use by other computers in your network and it has to fit into your company’s IP environment. You may have to ask your System Administrator to get a free IP address for that purpose. Both, host and target computer must be in the same network. In following steps this IP address will be called$Target-IP$
Push the OK button.
Check if remote debugging and changed
$Target-IP$
has been saved.Push
Open Project with Visual Studio
button.Project will be created and all needed settings are set.
Adjust
$Target-IP$
in generated Visual Studio Loader project.Select the file
Vmftarget.cfg
in the Visual Studio Loader project and edit the settingCOMPort Ethernet $Target-IP$
.Press
F7
to compile the project.