4. Configuration Mode

4.1. Overview

At startup of EC-Monitor, the user will see this page:
_images/overview.png

4.2. Monitor Settings

4.2.1. Monitor

In this tab, the user can configure the cycle time. If he wants to connect to a control system, this can also be configured. After one of these modes is selected, the ENI file will be imported to show the configuration:
_images/monitor-general.png
General
Cycle Time:

Interval in microseconds for the EC-Monitor.

TAP connected to local system
LinkLayer:

Select the Link-Layer which should be used.

Network Adapter:

Network adapter which is connected to TAP or the switch.

TAP Type:

Select the type of TAP adapter which is used. Generic is for a standard switch. Supported is also the ET2000. More will be supported in the future.

ENI File:
Path to the ENI which is used in the network that should be monitored. The ENI file can be exported in EC-Engineer. It is also possible to export an ENI file from TwinCAT.

In the EtherCAT tab in TwinCAT is a button “Export Configuration File…”. The “Export Configuration File…” button opens a “Save as” dialog for saving the XML master configuration file. This file describes the process data and the transfer frames that are sent during the EtherCAT state transitions.

_images/system_architecture_inspector.png
EtherCAT snapshot by EC-Inspector
Capture File:

Path to the capture file, which contains one or more snapshots ecd

For more information about the snapshots and capture files, see Capture File

EtherCAT frames captured by Wireshark
Capture File:

Path to the capture file pcap

ENI File:

Path to the ENI which was used for the captured network.

For more information about the capture files, see Wireshark File

4.2.2. Process Data Image

In this tab, the user can see all variables of the process data image.
_images/monitor-process-data-image.png

The variables can also be added to the watchlist, to have a better overview in diagnosis mode.

4.2.3. Watchlist Monitor

In this tab, the user can see the watchlist and remove variables from the watchlist.
_images/monitor-watchlist.png

4.2.4. Tasks + Sync Units

In this tab, the user can see the tasks and master sync units of the ENI file.
_images/master-su.png
Tasks:

List of cyclic tasks and master sync units.

4.2.5. Data Acquisition

In this tab, the user can configure our Data Acuisition (DAQ) library. This library can used from EC-Insepector to record process data in realtime.

After adding a new recorder, the user can select the variables which should be recorded and specify some triggers:
_images/master-daq.png
Variables:
Add/Remove:

Used for adding or removing the selected variable to the recording.

Triggers:
New/Edit/Delete:

Used for changing the trigger list.

If user wants to edit a recorder, he will see the following dialog:
_images/master-daq_2.png
Name:

Name of the recorder

File:

Absolute path of the recorder file on the master system

Format:
Format of the recorder file, e.g.
  • MDF (Measurement Data Format)

  • CSV (Comma Separated Values)

Sample Rate:

Sample rate of the recorded data e.g. every cycle or every second cycle, …

Real time stamp:

Adds a real time stamp to the recorded data

Cycle counter:

Adds a cycle counter to the recorded data

If user wants to edit a trigger, he will see the following dialog:
_images/master-daq_3.png
General
Left variable:

Name of the left variable

Operator:

Operator of the trigger (e.g. =, >, >=, <, <=, !=)

Right value:

Value of the right operand to compare the left variable against a static value e.g. trigger, if variable is greater than 5

Right variable:

Name of the right variable to compare the left variable against the value of another variable e.g. trigger, if variable 1 is smaller than variable 2

Enable:

Enabled or disabled trigger (can be enabled from application later)

Start:

Start or stop trigger

Optional
Duration:

Duration in ms (0 = infinite) e.g. trigger should start recording for 500 ms

Count:

Trigger count (0 = infinite) e.g. trigger should hit only for 5 times

For more information please refer the manual of the EC-Master-Data-Acquisition-Library.

4.2.6. Trigger

In this tab, the user can create, edit und remove trigger. When a trigger is hit, the monitor will stop and show the actual state. At the moment trigger for process data are supported.
_images/monitor-trigger.png
Trigger:

List of trigger.

Edit Trigger:
New: When new is clicked the following dialog pops up:
_images/monitor-new-trigger.png

The user can select variable which should be compared and the select if he wants to compare with a value or another variable. With enable the trigger can be enababled and disabled.

Edit: Edit the selected trigger

Remove: Remove the selected trigger from project

If the EC-Inspector stops because of a trigger it can be restarted with Run. It is also possible to pause the EC-Inspector without a trigger:
_images/run-pause.png

4.3. Slave Settings

4.3.1. General

In this tab, the user can see general slave settings like station address or the name of the slave. He can also see the connected ports.
_images/device-editor.png
Address
Station Address:

Station address of the slave. By default, the first station address is 1001.

Information
Name:

Name of the slave. By default the following format is used “Slave_N [TYPE]”

Vendor:

Name of the vendor the slave

Product Code:

Product Code of the slave

Revision Number:

Revision Number of the slave

Identification Value:

Identification Value of the slave

Ports
Connected Devices:

List of connected devices

4.3.2. Variables

In this tab, the user can see the variables of the slave.
_images/slave-variables.png
Lists of Variables

Variables comes from the import of the ENI file.

Buttons
Add to watchlist:

Adds the variable into the watchlist