7. Customization
7.1. Multi-Language-Support
EC-Inspector supports multiple languages, which can be changed at runtime. Adding support for further lanuages is quite easy because it is just a simple XML file which must be added to the kit.
All language files are stored in: "%ProgramFiles%/acontis_technologies/EC-Inspector/Languages/...
- EC-Inspector has also full UNICODE support, which means that it is also possible to support Asian languages:
7.2. Themes
EC-Inspector supports multiple themes, which can be changed during compile time. Adding support for further themes is quite easy because a theme consists of a couple of XAML files which must be added to the kit.
Five themes are already included into EC-Inspector:
- IG Theme
- Office 2010 Blue Theme
- Office 2007 Black Theme
- Office 2007 Sliver Theme
- Luna Theme