9. FAQ, Tips
9.1. Help in case of a problem
If you have a problem with EC-Inspector or something does not run as expected, please try first the following things:
Read messages in message window
Increase message level
Read log file for more information
Restart EC-Inspector and try to do it again
- Contact support by sending a mail to ecsupport@acontis.com and attach the following information
Project file
.eciEC-Inspector Version
Log file
Short description how the reproduce it
9.2. Shortcuts
EC-Inspector supports shortcuts for the most commonly used actions, like:
- Menu
Ctrl + N: Create new project
Ctrl + O: Open project
Ctrl + S: Save project
Alt + F4: Exit program
9.3. FAQ
Solutions for possible problems:
- EC-Inspector reports a message with ErrCode: 0x…
Error Codes sent directly from the EC-Monitor. If you want to know what to know how to solve this problem, please refer the manual of EC-Monitor.
- Connect to local system is not possible
Is Npcap / NDIS installed?
Is at least one network adapter installed?
- Permanent fram loss while monitoring TwinCAT
Please try with Npcap instead of NDIS driver
- WebAdmin in Dongle-Version shows page not found, what can I do?
You have to download and install the Code Meter Runtime from WIBU https://www.wibu.com/