1. Introduction
1.1. Overview
EC-Inspector is a diagnosis tool for EtherCAT networks that are controlled by any EtherCAT master (EC-Master, TwinCAT, CoDeSys 4.2.0.0 and higher, …) with help of the EC-Monitor.
The user needs an ENI file to start the EC-Monitor. The EC-Monitor will collect the data from the EtherCAT network.
The EtherCAT network does not have to be changed. Only a TAP or switch is needed to collect the data.
1.2. Requirements
Microsoft Windows 10 and above
Microsoft .NET Framework 4 Client Profile
Screen resolution at least 1024x768 pixel
Memory as recommended for operating system
Disk space approximately 40 MB