1.4. Programmer’s Guide
1.4.1. emDcConfigure
-
EC_T_DWORD emDcConfigure(EC_T_DWORD dwInstanceID, EC_T_DC_CONFIGURE *pDcConfigure)
Configure the distributed clocks.
Set the DC synchronization settling time ([ms]).
Set the DC slave limit for the wire or’ed clock deviation value. This value determines whether the slave clocks are synchronized or not.
Configure the ARMW burst frames to compensate the static deviations of the clock speeds.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pDcConfigure – [in] Configuration parameter a pointer to a structure of type EC_T_DC_CONFIGURE.
- Returns
EC_E_NOERROR or error code
-
struct EC_T_DC_CONFIGURE
Public Members
-
EC_T_DWORD dwTimeout
[in] Timeout [ms] for the DC initialization in which time offsets and propagation delays are evaluated.
-
EC_T_DWORD dwDevLimit
[in] Maximum permissible deviation of the individual slave clock and the DC reference clock. The maximum deviation is determined by wire or’ed the deviations of the individual slave clocks with one another. The check against the limit is only active if “Sync Window Monitoring” is set in the configuration tool (EC Engineer), which generates a BRD command to read the slave register 0x092C in every cycle. The limit is calculated as follows:
2^n - 1 ns, e.g. a dwDevLimit of 4 corresponds to 14 ns.
A value of 0 disables the “Sync Window Monitoring”
-
EC_T_DWORD dwSettleTime
[in] Settle time [ms]. At the beginning of the synchronization the slave clocks oscillate strongly. To prevent multiple in-sync and out-of-sync notifications from being generated, a settling time can be set in which no notifications are generated.
-
EC_T_DWORD dwBurstBulk
[in] Amount of burst frames per cycle during initialization burst. Default 12.
-
EC_T_BOOL bBulkInLinkLayer
[in] If EC_TRUE, bulk is realized by link layer, otherwise by master. The MAC needs to support the frame repeating function. In this case the link layer will repeat the DC burst frames itself, reducing the hardware accesses of the master to the MAC.
-
EC_T_DWORD dwDcStartTimeGrid
[in] Time grid [ns] to align DC start time. With the help of the grid, several EtherCAT networks can be synchronized without a random shift value between the SYNC signals.
-
EC_T_DWORD dwTimeout
See also
Chapter “Drift Compensation” of the ETG Document “ESC Datasheet Section 1 - Technology”
1.4.2. emDcIsEnabled
1.4.3. emGetBusTime
1.4.4. emDcContDelayCompEnable
-
EC_T_DWORD emDcContDelayCompEnable(EC_T_DWORD dwInstanceID)
Enable the continuous propagation delay compensation.
Calling this function generate a propagation delay measurement every 30s. The result of the measurement is used to correct the propagation delay values on the bus.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns
EC_E_NOERROR or error code
1.4.5. emDcContDelayCompDisable
1.4.6. emIoControl - EC_IOCTL_DC_SLV_SYNC_STATUS_GET
Get the last generated emNotify - EC_NOTIFY_DC_SLV_SYNC notification.
- emIoControl - EC_IOCTL_DC_SLV_SYNC_STATUS_GET
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_DC_SYNC_NTFY_DESC data typedwOutBufSize: [in] Size of the output buffer in bytespdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer pbyOutBuf
- Return
EC_E_NOERROR or error code
See also
emNotify - EC_NOTIFY_DC_SLV_SYNC describes EC_T_DC_SYNC_NTFY_DESC
1.4.7. emIoControl - EC_IOCTL_DC_SETSYNCSTARTOFFSET
Set the safety offset applied to the “set DC start time” InitCmd during the PS transition.
- emIoControl - EC_IOCTL_DC_SETSYNCSTARTOFFSET
- Parameter
pbyInBuf: [in] Pointer to EC_T_DC_STARTCYCSAFETY_DESC data typedwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
Default: 50000000ns
1.4.8. emIoControl - EC_IOCTL_DC_FIRST_DC_SLV_AS_REF_CLOCK
Enable or disable the usage of the first DC slave on bus overriding the configured reference clock.
- emIoControl - EC_IOCTL_DC_FIRST_DC_SLV_AS_REF_CLOCK
- Parameter
pbyInBuf: [in] pointer to EC_T_BOOL. EC_FALSE: disable, EC_TRUE: enable.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
1.4.9. emFindInpVarByName - “Inputs.BusTime”
The DC system time (written to ESC register 0x0910) is part of the process data with name “Inputs.BusTime”.
-
static EC_T_DWORD ecatFindInpVarByName(const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
-
EC_T_DWORD emFindInpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
See also
emFindInpVarByName() in the EC-Master Class B documentation
1.4.10. emIoControl - EC_IOCTL_DC_ENABLE_ALL_DC_SLV
Enable or disable the usage of DC at all supporting slaves on bus overriding the configured settings. Perhaps emIoControl - EC_IOCTL_DC_FIRST_DC_SLV_AS_REF_CLOCK is necessary to set the reference clock at an allowed position.
- emIoControl - EC_IOCTL_DC_ENABLE_ALL_DC_SLV
- Parameter
pbyInBuf: [in] pointer to EC_T_BOOL. EC_FALSE: disable, EC_TRUE: enable.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
1.4.11. emNotify - EC_NOTIFY_REFCLOCK_PRESENCE
Distributed clocks reference clock presence notification. It will be received before emNotify - EC_NOTIFY_DC_SLV_SYNC as soon as reference clock was found on bus or removed from bus.
This notification is disabled by default.
- emNotify - EC_NOTIFY_REFCLOCK_PRESENCE
- Parameter
pbyInBuf: [in] pointer to notification descriptor EC_T_REFCLOCK_PRESENCE_NTFY_DESCdwInBufSize: [in] sizeof(EC_T_REFCLOCK_PRESENCE_NTFY_DESC)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
See also
emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED in the EC-Master Class B documentation for how to control the activation
1.4.12. emNotify - EC_NOTIFY_DC_STATUS
Distributed clocks status notification. It will be received after emNotify - EC_NOTIFY_DC_SLV_SYNC as soon as DC is initialized or topology change was done . After topology was changed it may be received without emNotify - EC_NOTIFY_DC_SLV_SYNC if slaves did not get out of sync.
If EC_E_NOERROR is returned and window monitoring is enabled, all slaves are in SYNC
- emNotify - EC_NOTIFY_DC_STATUS
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD (EC_E_NOERROR on success, Error code otherwise)dwInBufSize: [in] sizeof(EC_T_DWORD)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
See also
emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED in the EC-Master Class B documentation for how to control the deactivation
1.4.13. emNotify - EC_NOTIFY_DC_SLV_SYNC
DC slave synchronization notification. Every time the slaves are coming in sync or getting out of sync the clients will be notified here. The notification is raised in any case if any DC slaves are configured. Slaves can only be out of sync if Sync Window Monitoring is enabled otherwise they are considered in sync
This notification is enabled by default.
- emNotify - EC_NOTIFY_DC_SLV_SYNC
- Parameter
pbyInBuf: [in] pointer to notification descriptor EC_T_DC_SYNC_NTFY_DESCdwInBufSize: [in] sizeof(EC_T_DC_SYNC_NTFY_DESC)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_DC_SYNC_NTFY_DESC
Public Members
-
EC_T_DWORD IsInSync
[in] EC_TRUE : Wire or’ed deviation value meets limit requirements. EC_FALSE: Wire or’ed deviation value does not meet limit requirements.The limit is set by ecatDcConfigure()
-
EC_T_DWORD IsInSync
See also
emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED in the EC-Master Class B documentation for how to control the deactivation