2.3. Programmer’s Guide

2.3.1. emDcmConfigure

static EC_T_DWORD ecatDcmConfigure(struct _EC_T_DCM_CONFIG *pDcmConfig, EC_T_DWORD dwInSyncTimeout)
EC_T_DWORD emDcmConfigure(EC_T_DWORD dwInstanceID, EC_T_DCM_CONFIG *pDcmConfig, EC_T_DWORD dwInSyncTimeout)

Configure DC master synchronization.

Parameters
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • pDcmConfig – [in] Configuration information, a pointer to a structure of type EC_T_DCM_CONFIG.

  • dwInSyncTimeout – [in] Currently not implemented.

Returns

EC_E_NOERROR or error code

struct EC_T_DCM_CONFIG

Public Members

EC_T_DCM_MODE eMode

[in] DCM mode

EC_T_DCM_CONFIG_BUSSHIFT BusShift

[in] BusShift configuration. Valid if eMode is set to eDcmMode_BusShift

EC_T_DCM_CONFIG_MASTERSHIFT MasterShift

[in] MasterShift configuration. Valid if eMode is set to eDcmMode_MasterShift

EC_T_DCM_CONFIG_LINKLAYERREFCLOCK LinkLayerRefClock

[in] LinkLayerRefClock configuration. Valid if eMode is set to eDcmMode_LinkLayerRefClock

EC_T_DCM_CONFIG_MASTERREFCLOCK MasterRefClock

[in] MasterRefClock configuration. Valid if eMode is set to eDcmMode_MasterRefClock

EC_T_DCM_CONFIG_DCX Dcx

[in] DCX configuration. Valid if eMode is set to eDcmMode_Dcx

enum EC_T_DCM_MODE

Values:

enumerator eDcmMode_Off

DCM disabled

enumerator eDcmMode_BusShift

DCM BusShift mode

enumerator eDcmMode_MasterShift

DCM MasterShift mode

enumerator eDcmMode_LinkLayerRefClock

DCM LinkLayer Ref Clock mode

enumerator eDcmMode_MasterRefClock

DCM Master Ref Clock mode

enumerator eDcmMode_Dcx

DCM DCX External synchronization mode

enumerator eDcmMode_MasterShiftByApp

DCM MasterShift controlled by application mode

struct EC_T_DCM_CONFIG_BUSSHIFT

Public Members

EC_T_INT nCtlSetVal

[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero).

EC_T_INT nCtlGain

[in] Proportional gain in ppt (part per thousand). Default is value 2. A value of 0 let the current setting unmodified.

EC_T_INT nCtlDriftErrorGain

[in] Multiplier for drift error. Default value is 3. A value of 0 let the current setting unmodified

EC_T_INT nMaxValidVal

[in] Error inputs above this value are considered invalid. If error input prediction is valid then the difference between the error input and the expected value is taken. Default value is 3000. A value of 0 let the current setting unmodified

EC_T_BOOL bLogEnabled

[in] If set to EC_TRUE, logging information are generated and can be get calling emDcmGetLog

EC_T_DWORD dwInSyncLimit

[in] Limit [ns] for InSync monitoring. Default value is 4000. A value of 0 let the current setting unmodified

EC_T_DWORD dwInSyncSettleTime

[in] Settle time [ms] for InSync monitoring. Default value is 1500. A value of 0 let the current setting unmodified

EC_T_BOOL bCtlOff

[in] If set to EC_TRUE, control loop is disabled. Combined with bLogEnabled, it makes possible to analyze the natural drift between the stack cycle and the reference clock

EC_T_BOOL bUseDcLoopCtlStdValues

[in] If set to EC_TRUE, the values of ESC DC time loop control register 0x930 and 0x934 are not changed by master. This could increase the time it takes to get the InSync. Use only if there are a problems with the reference clock to get InSync

EC_T_DWORD dwInSyncStartDelayCycle

[in] Delay time [ms] before InSync monitoring start

struct EC_T_DCM_CONFIG_MASTERSHIFT

Public Members

EC_T_INT nCtlSetVal

[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero)

EC_T_INT nCtlGain

[in] Proportional gain in ppt (part per thousand). Default is value 2. A value of 0 let the current setting unmodified

EC_T_INT nCtlDriftErrorGain

[in] Multiplier for drift error. Default value is 3. A value of 0 let the current setting unmodified

EC_T_INT nMaxValidVal

[in] Error inputs above this value are considered invalid. If error input prediction is valid then the difference between the error input and the expected value is taken. Default value is 3000. A value of 0 let the current setting unmodified

EC_T_BOOL bLogEnabled

[in] If set to EC_TRUE, logging information are generated and can be get calling emDcmGetLog

EC_T_DWORD dwInSyncLimit

[in] Limit [ns] for InSync monitoring. Default value is 4000. A value of 0 let the current setting unmodified

EC_T_DWORD dwInSyncSettleTime

[in] Settle time [ms] for InSync monitoring. Default value is 1500. A value of 0 let the current setting unmodified

EC_T_BOOL bCtlOff

[in] If set to EC_TRUE, control loop is disabled. Combined with bLogEnabled, it makes possible to analyze the natural drift between the stack cycle and the reference clock. Also it provides reading of current adjustment value using emDcmGetAdjust function

EC_T_DWORD dwInSyncStartDelayCycle

[in] Delay time [ms] before InSync monitoring start

EC_T_DC_STARTTIME_CB_DESC DcStartTimeCallbackDesc

[in] If not null, DC start time calculated by application, otherwise by master. See also EC_T_DC_STARTTIME_CB_DESC. Shift value configured in ENI will still be applied

struct EC_T_DCM_CONFIG_LINKLAYERREFCLOCK

Public Members

EC_T_INT nCtlSetVal

[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero)

EC_T_BOOL bLogEnabled

[in] If set to EC_TRUE, logging information are generated and can be get calling emDcmGetLog

EC_T_DC_STARTTIME_CB_DESC DcStartTimeCallbackDesc

[in] If not null, DC start time calculated by application, otherwise by master. See also EC_T_DC_STARTTIME_CB_DESC. Shift value configured in ENI will still be applied.

struct EC_T_DCM_CONFIG_MASTERREFCLOCK

Public Members

EC_T_INT nCtlSetVal

[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero)

EC_T_BOOL bLogEnabled

[in] If set to EC_TRUE, logging information are generated and can be get calling emDcmGetLog

EC_T_DWORD dwInSyncLimit

[in] Limit [ns] for InSync monitoring. Default value is 4000. A value of 0 let the current setting unmodified

EC_T_DWORD dwInSyncSettleTime

[in] Settle time [ms] for InSync monitoring. Default value is 1500. A value of 0 let the current setting unmodified

EC_T_DWORD dwInSyncStartDelayCycle

[in] Delay time [ms] before InSync monitoring start

struct EC_T_DCM_CONFIG_DCX

Contains the configuration information for the DCX external synchronization mode.

See also

Feature Pack “External Synchronization” for further details.

struct EC_T_DC_STARTTIME_CB_DESC

Public Members

EC_T_VOID *pvContext

[in] Arbitrarily application-defined parameter passed to pfnCallback

EC_PF_DC_STARTTIME_CB pfnCallback

[in] DC start time callback function pointer. If not EC_NULL, DC start time calculated by application, otherwise by master

typedef EC_T_DWORD (*EC_PF_DC_STARTTIME_CB)(EC_T_VOID *pvContext, EC_T_WORD wSlaveFixedAddr, EC_T_UINT64 *pqwDcStartTime)

EC-Master requests DC start time for every single slave from a given callback DcStartTimeCallbackDesc with slave station address as input parameter. The slave specific DC start time value will be passed directly to the slave without modifications by master. This means no other values like nCtlSetVal will be added. Shift value configured in ENI will still be applied.

Parameters
  • pvContext – [in] Arbitrarily application-defined parameter passed to callback

  • wSlaveFixedAddr – [in] Slave fixed address

  • pqwDcStartTime – [out] DC start time for specific slave

Returns

EC_E_NOERROR or error code

2.3.2. emDcmGetStatus

static EC_T_DWORD ecatDcmGetStatus(EC_T_DWORD *pdwErrorCode, EC_T_INT *pnDiffCur, EC_T_INT *pnDiffAvg, EC_T_INT *pnDiffMax)
EC_T_DWORD emDcmGetStatus(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwErrorCode, EC_T_INT *pnDiffCur, EC_T_INT *pnDiffAvg, EC_T_INT *pnDiffMax)

Get DC master synchronization controller status.

Parameters
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • pdwErrorCode – [out] Pointer to current error code of the DCM controller. Possible values are:

    • EC_E_NOTREADY DCM control loop is not running

    • EC_E_BUSY DCM control loop is running and try to get InSync

    • DCM_E_MAX_CTL_ERROR_EXCEED Set if the controller error exceeds the InSyncLimit

    • DCM_E_DRIFT_TO_HIGH DCM control loop not able to compensate drift. Drift above 600ppm.

  • pnDiffCur – [out] Pointer to current difference between set value and actual value of controller in nanoseconds.

  • pnDiffAvg – [out] Pointer to average difference between set value and actual value of controller in nanoseconds

  • pnDiffMax – [out] Pointer to maximum difference between set value and actual value of controller in nanoseconds

Returns

  • EC_E_NOERROR if status retrieval was successful

  • EC_E_NOTSUPPORTED the DC feature is not supported/switched off. EC-Master stack has to be compiled with DC support see “define INCLUDE_DC_SUPPORT”

  • EC_NULL does not appear in normal flow, if EC_NULL is returned we are in a very exceptional case where m_poDcm == NULL (SW error detection)

2.3.3. emDcmResetStatus

static EC_T_DWORD ecatDcmResetStatus(EC_T_VOID)
EC_T_DWORD emDcmResetStatus(EC_T_DWORD dwInstanceID)

Reset DC master synchronization controller status, average and maximum difference between set value and actual value.

Parameters

dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

Returns

EC_E_NOERROR or error code

2.3.4. emDcmGetBusShiftConfigured

static EC_T_DWORD ecatDcmGetBusShiftConfigured(EC_T_BOOL *pbBusShiftConfigured)
EC_T_DWORD emDcmGetBusShiftConfigured(EC_T_DWORD dwInstanceID, EC_T_BOOL *pbBusShiftConfigured)

Determines if DCM Bus Shift is configured/possible in configuration (ENI file)

Parameters
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • pbBusShiftConfigured – [out] EC_TRUE if DCM bus shift mode is supported by the current configuration

Returns

EC_E_NOERROR or error code

2.3.5. emDcmGetLog

static EC_T_DWORD ecatDcmGetLog(EC_T_CHAR **pszLog)
EC_T_DWORD emDcmGetLog(EC_T_DWORD dwInstanceID, EC_T_CHAR **pszLog)

Get logging information from the DCM controller.

This function returns non-zero pointer only if bLogEnabled was set to EC_TRUE in EC_T_DCM_CONFIG.

Parameters
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • pszLog – [out] Pointer to a string containing the current logging information

Returns

EC_E_NOERROR or error code

See also

Controller adjustment for content description of pszLog

2.3.6. emIoControl - EC_IOCTL_DCM_GET_LOG

Get logging information from the DCM controller.

emIoControl - EC_IOCTL_DCM_GET_LOG
Parameter
  • pbyInBuf: [in] Should be set to EC_NULL

  • dwInBufSize: [in] Should be set to 0

  • pbyOutBuf: [out] Pointer to struct EC_T_DCM_LOG

  • dwOutBufSize: [in] Size of the output buffer in bytes

  • pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer pbyOutBuf

Return

EC_E_NOERROR or error code

struct EC_T_DCM_LOG

Public Members

EC_T_DWORD dwMsecCounter

[out] Current MsecCounter

EC_T_INT nCtlSetVal

[out] Configured controller set val [ns]

EC_T_UINT64 qwBusTime

[out] Current BusTime

EC_T_INT nCtlErrorNsec

[out] Current controller error [ns]

EC_T_INT nDrift

[out] Current calculated drift [ppm]

EC_T_DWORD dwErrorCode

[out] Last returned error code by controller

EC_T_BOOL bDcmInSync

[out] EC_TRUE if DCM is in sync, EC_FALSE if out of sync

EC_T_BOOL bDcInSync

[out] EC_TRUE if DC is in sync, EC_FALSE if out of sync

EC_T_UINT64 qwDcStartTime

[out] Last used DC StartTime

EC_T_INT nSystemTimeDifference

[out] Last read System Time Difference (ESC register 0x092C)

2.3.7. emDcmShowStatus

static EC_T_DWORD ecatDcmShowStatus(EC_T_VOID)
EC_T_DWORD emDcmShowStatus(EC_T_DWORD dwInstanceID)

Show DC master synchronization status as DbgMsg (for development purposes only).

Parameters

dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

Returns

EC_E_NOERROR or error code

2.3.8. emDcmGetAdjust

static EC_T_DWORD ecatDcmGetAdjust(EC_T_INT *pnAdjustPermil)
EC_T_DWORD emDcmGetAdjust(EC_T_DWORD dwInstanceID, EC_T_INT *pnAdjustPermil)

Returns the current adjustment value for the timer.

bCtlOff must be set to EC_TRUE in EC_T_DCM_CONFIG to enable external adjustment.

Parameters
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • pnAdjustPermil – [out] Current adjustment value of the timer.

Returns

EC_E_NOERROR or error code

2.3.9. DCM specific error codes

DCM_E_ERROR

0x981201C0: Unspecific DCM Error

DCM_E_NOTINITIALIZED

0x981201C1: Not initialized

DCM_E_MAX_CTL_ERROR_EXCEED

0x981201C2: DCM controller - synchronization out of limit

DCM_E_NOMEMORY

0x981201C3: Not enough memory

DCM_E_INVALID_HWLAYER

0x981201C4: Hardware layer - (BSP) invalid

DCM_E_TIMER_MODIFY_ERROR

0x981201C5: Hardware layer - error modifying timer

DCM_E_TIMER_NOT_RUNNING

0x981201C6: Hardware layer - timer not running

DCM_E_WRONG_CPU

0x981201C7: Hardware layer - function called on wrong CPU

DCM_E_INVALID_SYNC_PERIOD

0x981201C8: Invalid DC sync period length (invalid clock master?)

DCM_E_INVALID_SETVAL

0x981201C9: DCM controller SetVal to small

DCM_E_DRIFT_TO_HIGH

0x981201CA: DCM controller - Drift between local timer and ref clock to high

DCM_E_BUS_CYCLE_WRONG

0x981201CB: DCM controller - Bus cycle time (dwBusCycleTimeUsec) doesn’t match real cycle

DCX_E_NO_EXT_CLOCK

0x981201CC: DCX controller - No external synchronization clock found

DCM_E_INVALID_DATA

0x981201CD: DCM controller - Invalid data

2.3.10. Notifications

At startup the master raises the notifications emNotify - EC_NOTIFY_DC_SLV_SYNC, emNotify - EC_NOTIFY_DC_STATUS and emNotify - EC_NOTIFY_DCM_SYNC at master state transition from INIT to PREOP.

The order is typically as follows ( emNotify - EC_NOTIFY_DCM_SYNC may be before or after reaching PREOP):

EC_NOTIFY_STATECHANGED(INIT)[…]

EC_NOTIFY_DC_SLV_SYNC […]

EC_NOTIFY_DC_STATUS […]

[EC_NOTIFY_DCM_SYNC] […]

EC_NOTIFY_STATECHANGED(PREOP) […]

[EC_NOTIFY_DCM_SYNC] […]

EC_NOTIFY_STATECHANGED(SAFEOP) […]

EC_NOTIFY_STATECHANGED(OP) […]

2.3.11. emNotify - EC_NOTIFY_DCM_SYNC

DCM InSync notification.

This notification is enabled by default.

emNotify - EC_NOTIFY_DCM_SYNC
Parameter
  • pbyInBuf: [in] pointer to notification descriptor EC_T_DCM_SYNC_NTFY_DESC

  • dwInBufSize: [in] sizeof(EC_T_DCM_SYNC_NTFY_DESC).

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

struct EC_T_DCM_SYNC_NTFY_DESC

Public Members

EC_T_DWORD IsInSync

[in] EC_TRUE as long as time of master and reference clock are in sync. False if the InSyncLimit from the bus shift configuration is exceeded

EC_T_INT nCtlErrorNsecCur

[in] Current difference [ns] between set value and actual value of controller

EC_T_INT nCtlErrorNsecAvg

[in] Average difference [ns] between set value and actual value of controller

EC_T_INT nCtlErrorNsecMax

[in] Maximum difference [ns] between set value and actual value of controller

See also

emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED in the EC-Master Class B documentation for how controls the deactivation