4. Guest Configuration

4.1. Guest Types

The RTOSVisor supports Real-time operating system guests (e.g. Real-time Linux) as well as non Real-time (General Purpose) operating systems (e.g. Windows). While the Real-time operating systems are adapted (para-virtualized) to the underlying Real-time hypervisor and shipped as part of the RTOSVisor, the General Purpose operating systems can be used without modification and need to be installed prior to using them.

All guests can use the Communication Subsystem which provides various means to communicate between the guests. General Purpose operating systems may optionally be used without a connection to the Communication Subsystem. They may interact with the other guests using TCP/IP bridging, see the Hypervisor Manual for details.

_images/CommSubsystemOverview.png

The following guest types are supported.

_images/SysMgrGuestTypes.jpg
  • Real-time Linux: Real-time Linux real-time guest

  • VxWorks: VxWorks real-time guest

  • On Time RTOS-32: RTOS-32 real-time guest

  • General Purpose + CommSubsystem: A General Purpose guest which can attach to the Communication Subsystem

  • General Purpose: A General Purpose guest without Communication Subsystem access

Caution

In case you intend to add at least one Real-time guest or one General Purpose guest with Communication Subsystem access, the first guest must be a Real-time guest!

4.2. Add RTOS guests

Select Guests and then + Add Guest.
A list of operating systems is shown.
_images/CreateGuestList.jpg

Then select one of the RTOS guests (e.g. Real-time Linux). You should also assign a reasonable name for this guest (e.g. RT-Linux).

_images/NewRTLinuxGuest.jpg

4.2.1. Select the RTOS image to boot

The RTOS may offer multiple binary images which can be booted (e.g. different RTOS versions).
You need to select the RTOS in the Overview tab.
_images/RT-LinuxImage.jpg

Then select the image you like to use.

4.3. Add General Purpose guests

Adding a General Purpose guest is done in a very similar way as for Real-time guests. You can select whether such a guest shall be able to attach to the Communication Subsystem or not.

Select Guests and then + Add Guest.
A list of operating systems is shown.
_images/SysMgrGuestTypes.jpg
Then select either the General Purpose or General Purpose + CommSubsys guest.
If you want the Guest to use the communication subsystem (virtual network, shared memory etc.) to communicate with the RTOS, then you need to select the latter one.
Please note, the number of OSes which can use the communication subsystem is limited (depending on the version of the software).
_images/NewWindowsGuest.jpg

Hint

If the guest is configured to get access to the Communication Subsystem, by default access is enabled. Prior to starting such a guest, the VMF (Virtual Machine Framework) needs to be started. You may optionally disable access to the Communication Subsystem, then you do not need to start the VMF.

_images/SysMgrDisableCommSubsys.jpg

4.3.1. Install Windows/Linux guest

If you want to install a new Windows or Linux guest, please follow the steps below.

First you need to copy the installation media ISO file to the Hypervisor Host (e.g. /hv/iso)
Then you need to configure the guest hardware: Memory (RAM), number of CPUs, disk size, disk image path.
The installation media file must be set appropriately.
By specifying the Disk Image File, the location and name of the guest image files can be determined. The Disk Image File entry always consists of a path (starting with /hv/VMs) and filename with the .qcow2 extension (e.g., /hv/VMs/windows/win10_20h2.qcow2).

Caution

If no Disk Image File is specified, then the image will be created in the guest folder, and if the guest is deleted, the image and thus the entire installation and all settings in the Windows or Ubuntu guest will also be deleted.

_images/WindowsProperties.jpg

You must set the “OS Type” to the appropriate type.

_images/SelectOsType.jpg

To install the guest, you need to synchronize the configuration with the Hypervisor Host first and then run the guest. See Guest Operation for more details. The Hypervisor Windows Guest Guide also shows step by step, how to install a new Windows guest.

4.3.2. Select existing Windows/Linux guest

If you want to re-use an existing Windows or Linux guest image, please follow the steps below.

First you need to copy the guest image files to the Hypervisor Host.
Assure the guest image files are complete, they consist of one or multiple .qcow2 file(s) and two EFI BIOS files: OVMF_CODE.fd and OVMF_VARS.fd.
Then you need to configure the guest hardware: Memory (RAM), number of CPUs and the disk image path.
The guest disk image filename must be set appropriately.
_images/ExistingWindowsGuest.jpg

Set the “OS Type” appropriately.

_images/SelectOsType.jpg

To run the guest, you need to synchronize the configuration with the Hypervisor Host first and then run the guest. See Guest Operation for more details.

4.3.3. Step by step example

For an example, how to add a Windows guest, see here.

4.4. Remove guests

To remove a guest, you need to select the respective guest and then press the Remove Guest button.

_images/SysMgrRemoveGuest.jpg

Caution

All configuration settings for this guest will be removed, it is not possible to restore those settings. You may save the current project to preserve the settings of all currently configured guests: Project Management.

4.5. Synchronization

Before the configuration becomes effective, you must synchronize the System Manager configuration with the Hypervisor Host. Take a look into the Synchronization chapter for details.

Caution

Writing a new configuration to the Hypervisor Host will destroy the currently active configuration!

4.6. Guest Identifiers

When adding a new guest, it will be assigned a unique Guest Identifier GUEST0001, GUEST0002 etc.. All configuration settings of the guests are located in the respective guest folders, for example /hv/guests/guest0001 or /hv/guests/guest0002.

All Real-time guests as well as General Purpose guests with access to the Communication Subsystem will get a unique identifier, the RTOS Identifier. The number of such guests is currently limited to 5, the range for the RTOS Identifier will be from 0 to 4. This RTOS identifier is required as a parameter for General Purpose guests when they attach to the Communication Subsystem.

All General Purpose guests, regardless whether they have access to the Communication Subsystem will also get a unique identifier, the GPOS Identifier. The number of such guests is currently limited to 9, the range for the GPOS Identifier will be from 1 to 9.

This following example shows a Ubuntu guest with access to the Communication Subsystem. The guest id is GUEST0004, which means that all settings are stored in /hv/guests/guest0004. The RTOS identifier is 2 which means that the guest needs to use this value when attaching to the Communication Subsystem. The GPOS identifier is 3 which means it is the third General Purpose guest configured in this project.

_images/SysMgrGuestIdentifier.jpg

4.7. Configuration Files

All configuration files for a specific guest are located in /hv/guests/guest0001, /hv/guests/guest0002 and so on. See also Guest Identifiers.

The following files are created automatically, when any guest is generated:

  • guest_config.sh

    Basic guest settings, needed when starting the guest. Do not change!

  • usr_guest_config.sh

    User specific guest settings, used when starting the guest. You may override settings defined in guest_config.sh.

  • guest.config

    Default guest configuration settings. Do not change!

  • usr.config

    User specific guest configuration settings. You may override settings defined in guest.config (and/or in device.config for Real-time guests).

  • hv_guest_autostart_xfce.sh

    Helper script to launch the guest console, used if a guest shall be started automatically. Do not change!

  • sysmgr_guest.config

    System Manager specific configuration information. Do not change!

  • vm_shutdown_hook.sh

    Script which is executed after the guest was shutdown.

4.7.1. RTOS guests

The following files are created automatically, when an RTOS guest is generated:

  • device.config

    Guest device configuration settings. Do not change!

  • hv_guest_autostart.service

    Service file, used if the guest shall be started automatically. Do not change!

4.7.2. General Purpose guests

The following files are created automatically, when a General Purpose guest is generated:

  • guest_gateway.config

    Guest gateway configuration settings. Specific ports inside the guest can be forwarded to a specific IP address and port. Currently only supported for Windows guests.

  • hv_guest_autostart.service

    Service file, used if the guest shall be started automatically. Do not change!

  • hv_guest_autostart_standalone.service

    Service file, used if the guest shall be started automatically in standalone mode. Do not change!

  • OVMF_CODE.fd, OVMF_VARS.fd

    Default EFI files, used if the guest is configured to use UEFI BIOS. These files can be removed if Legacy BIOS is used.

4.8. User specific configuration

If settings not supported by the System Manager need to be changed, they must be modified by adjusting the corresponding usr.config or usr_guest_config.sh files. See Configuration Files for an overview of all configuration files.

Especially for General Purpose guests there are many settings which can only be adjusted in the usr_guest_config.sh file.

4.9. RTOS-32 guests

4.9.1. Boot Image

The image file which is loaded into memory is defined in guest_config.sh using the osImage setting. By default the RTOS-32 application Loader image will be booted.

4.9.2. Filesystem

The file system root is defined in guest.config (section [Host\FileServer], parameter "HomeDir"). By default it will point to the RTOS-32 example guest. You may change this to another location, for example the guest folder (e.g. /hv/guests/guest0001).

4.9.3. DLL Loading

If the default image (the RTOS-32 Loader image) is booted, the application itself is stored in one or multiple DLLs (DLMs). The main DLL is defined in guest.config (section [Rtos\Loader], parameter "DllName"). By default it will point to a link defined in the RTOS-32 example guest.

Caution

All DLLs must be located in the filesystem root folder.

4.10. RTOS Guest (Project) Templates

The System Manager provides two XML‐based template files under /hv/templates/ that define the “skeleton” of any new RTOS guest:

  • os.xml Defines the available operating system templates (types, subfolders to copy into the guest folder, etc.). See excerpt below:

    <?xml version="1.0" encoding="utf-8"?>
    <Config>
      <OperatingSystem>
        <Property Key="Id" Value="RtLinux_SMPAUTO" />
        <Property Key="Name" Value="Real-time Linux (RT)" />
        <Property Key="Type" Value="linux_SMPAUTO" />
        <Property Key="SubFolders" Value="rtos_generic;rt-linux;rt-linux_SMPAUTO" />
        <Property Key="HasRtSupport" Value="true" />
        <Property Key="HasVmfAccess" Value="true" />
        <Property Key="HasRtAnalyzer" Value="true" />
        <Property Key="HasAutoSmpSupport" Value="true" />
      </OperatingSystem></Config>
    
  • images.xml Defines the VMF-loadable RTOS guest images (paths, memory sizing, alignment, SMP flags, etc.). See excerpt below:

    <?xml version="1.0" encoding="utf-8"?>
    <Config>
      <Image>
        <Property Key="Id" Value="Linux515x64" />
        <Property Key="Name" Value="Linux 5.15 x64" />
        <Property Key="Type" Value="linux" />
        <Property Key="Path" Value="../../templates/rt-linux/rtlinux515.x64.bin" />
        <Property Key="Arch" Value="64" />
        <Property Key="MinSize" Value="192M" />
        <Property Key="DefaultSize" Value="192M" />
        <Property Key="Align" Value="4M" />
        <Property Key="ShmAsOsHeap" Value="multiple" />
      </Image></Config>
    

4.10.1. Example: Adding a New Real‐time Linux SMP Image

To add add a new custom Real-time Linux image with SMP support, edit images.xml as follows:

  1. Open /hv/templates/images.xml.

  2. Duplicate an appropriate existing image entry <Image> block inside the top-level <Config>: In our example, this would be Linux515x64_SMPAUTO for a SMP supported Linux image. Take specific care of the Type property which defines the operating system type: Linux_SMPAUTO. This value must match with the Type property in the os.xml configuration file. Adjust the other values according to your need (e.g. image name to load, RAM size).

    <Image>
      <Property Key="Id"                     Value="Linux_Custom_SMPAUTO" />
      <Property Key="Name"                   Value="Linux Custom SMP" />
      <Property Key="Type"                   Value="linux_SMPAUTO" />
      <Property Key="Path"                   Value="../../templates/rt-linux/rtlinux_custom.bin" />
      <Property Key="Arch"                   Value="64" />
      <Property Key="MinSize"                Value="512M" />
      <Property Key="DefaultSize"            Value="512M" />
      <Property Key="Align"                  Value="4M" />
      <Property Key="ShmAsOsHeap"            Value="multiple" />
    </Image>
    
  3. Save the file.

  4. In the Config mode of the System Manager, select the Hypervisor in the Navigator tab. Then select More - Update Project Templates to update the template.

_images/SysMgrUpdateProjectTemplate.png
  1. The new entry Linux Custom SMP will now appear in the RTOS Image combobox when a Real-time Linux guest is configured.

_images/SysMgrCustomLinuxImage.png