1. Introduction

The System Manager is a web based tool (a Web Application) for configuration and diagnosis of the acontis hypervisor products. To show the graphical user interface, a web browser is required. Hypervisor configuration can be executed on the Hypervisor Host or remote via an IP connection. In addition, it is possible to connect to the Hypervisor Host via an MQTT gateway over the cloud.

The System Manager consists of several components:

  • Hypervisor backend: this is the interface to the Hypervisor Host. This backend interacts with the hypervisor (running on the same Hypervisor Host), e.g. to add guests, adjust configuration files etc. (see chapter Hypervisor Backend)

  • GUI backend (Web Application): this is the interface to the web browser. The web browser always connects to the GUI backend.

  • TCP/IP server: If the GUI backend and the Hypervisor backend run on different computers in the same network, they can be connected via TCP/IP. The Hypervisor Host and the GUI backends will then communicate over TCP/IP.

  • MQTT gateway: If the GUI backend and the Hypervisor backend run on different computers in different networks or even at different physical locations, they can be connected via an MQTT broker.

  • MQTT test broker: The test broker may be used in conjunction with the MQTT gateway if there is no MQTT broker available. This is NOT recommended and NOT supported for production environments!

1.1. Architectures

The modular design of the software allows different system architectures.


All components on the Hypervisor Host

_images/ArchitectureStandalone.jpg

Using the web browser on a System Manager Client

_images/ArchitectureExtBrowser.jpg

With TCP/IP Server

_images/ArchitectureTCPServer.jpg

MQTT Broker in the cloud

_images/ArchitectureMQTT.jpg

1.2. Installation and Update

There are various options, how to run the System Manager or System Manager components.
By default, the System Manager will be installed on the Hypervisor Host only and a browser is used to configure this (local) Hypervisor Host.
Another option is to run the GUI backend on a Windows machine, while the hypervisor backend runs on the Hypervisor Host (and both are connected via TCP or MQTT).
It is always required to install the System Manager on the Hypervisor Host.
If the GUI backend shall run on another computer, the System Manager must also be installed on this computer.

1.2.1. RTOSVisor - Default Installation

The RTOSVisor is shipped with a default installation of the System Manager, its location is in /hv/sysmgr. The System Manager can only be used after the basic RTOSVisor initialization was executed. How to initialize the RTOSVisor is described in the Hypervisor Quickstart Guide.

1.2.2. Windows Installation

If the System Manager (or the GUI backend) shall be executed on a Windows computer, you will have to manually install the System Manager on such a computer.

  • you have to request the system manager deliverable from the acontis support

  • copy the compressed system manager deliverable (e.g. HvWebApp_Windows-x64_V1.0.16.zip) into any folder where you want to use it later

  • uncompress the deliverables and then remove the compressed file

  • copy everything from _patches

md V1.0.16\HvWebApp_Windows
uncompress to V1.0.16\HvWebApp_Windows
xcopy /e V1.0.16\HvWebApp_Windows\Templates\_patches\*.* V1.0.16\.
call V1.0.16\HvWebApp_Windows\HvSystemManager.exe

1.2.3. Linux Installation

If the System Manager GUI backend shall be executed on a separate Linux computer (i.e. not the Hypervisor Host), you will have to manually install the System Manager on such a computer.

Caution

On the Hypervisor Host you must install the System Manager in /hv/sysmgr. On other Linux machines you can store the System Manager in any folder where you want to use it.

  • you have to request the system manager deliverable from the acontis support

  • copy the compressed system manager deliverable (e.g. HvWebApp_Linux-x64_V1.0.16.tar.gz) into this folder

  • uncompress the deliverables and then remove the compressed file

  • copy patch files

  • create doc directory

cd /hv/sysmgr
tar -xvzf HvWebApp_Linux-x64_V*.tar.gz
rm HvWebApp_Linux-x64_V*.tar.gz
cd ..
mkdir doc

1.2.4. RTOSVisor - System Manager Update

This section shows how to update to a later version of the System Manager for the RTOSVisor.

  • Stop the System Manager

    hv_sysmgr stop
    
  • Preserve the old version and create a new folder in the Hypervisor Host

    mv /hv/sysmgr /hv/sysmgr.orig
    mkdir /hv/sysmgr
    
  • Then follow the steps in Linux Installation

  • Start the System Manager

    hv_sysmgr start
    

1.3. System Manager control

Once the Hypervisor Host has been initialized, the System Manager backend will be executed automatically (as a service) when the computer is booted. This is controlled by the /hv/services/hv_sysmgr.service file.

Various commands are provided for System Manager control and diagnosis by calling the hv_sysmgr command.

You can execute this command to see a quick overview of the supported commands.

hv_sysmgr
System Manager running as a service. Output stored in /hv/sysmgr/sysmgr.log
System Manager Service running
Syntax /usr/bin/hv_sysmgr [status | debug=on | debug=off | log | clearlog | start | restart | stop | enable | disable ]
  • status: show current status.

  • log: show log file.

  • clearlog: clear log file content.

  • stop: stop the System Manager.

  • start: start the System Manager.

  • restart: restart (stop, then start) the System Manager.

  • disable: disable System Manager service (it will not be started automatically after reboot).

  • enable: enable System Manager service (it will be started automatically after reboot).

  • debug=on: enable additional debug messages.

  • debug=off: disable additional debug messages.

1.4. Local operation

Local operation means the Hypervisor backend as well as the GUI backend run on the Hypervisor Host.

_images/SysMgrLocalOperation.jpg

1.4.1. The System Manager backend

Caution

Prior to configuring the system using the System Manager you have to initialize the Hypervisor and reboot the system. See the Hypervisor Quickstart Guide for details.

The RTOSVisor will automatically start the System Manager backend.

Hint

If you want to directly start the System Manager backend in the RTOSVisor (without using the hv_sysmgr command), you need to stop the System Manager first.

hv_sysmgr stop

Then you can execute the following commands.

cd /hv/sysmgr
sudo ./HvSystemManager

Hint

You can type ./HvSystemManager /help to get information about supported commandline arguments

1.4.2. Local Browser

The RTOSVisor is shipped with the Chromium browser to be able to locally configure the system. Open the browser and type in the localhost IP address 127.0.0.1 and connect to port 5000. The following URL can be used: http://127.0.0.1:5000

_images/BrowserIpAddressLocal.jpg

1.4.3. Remote Browser

If you want to run the browser on another system (e.g. on your Windows or Linux workstation), you need to have a TCP/IP connection between the computer where the browser is running and the Hypervisor Host.

Open the browser and type in the IP address or the computer name of the Hypervisor Host and connect to port 5000. The computer name can be determined by calling the following command on the Hypervisor Host:

hostname

In case the hostname is hypervisor-PC1, the following URL can be used: http://hypervisor-PC1:5000

Alternatively, in case the IP address is 192.168.178.184, the following URL can be used: http://192.168.178.184:5000

_images/BrowserIpAddressRemote.jpg