12. System Manager for Windows
Caution
The System Manager for Windows is not yet available. This is preliminary documentation.
12.1. Installation
Install LxWin to “C:\Program Files\acontis_technologies\LxWin\” (default)
Unpack SystemManager HvWebApp_Windows-x64_V1.0.10.zip to “C:\Program Files\acontis_technologies\SysMgr\”
Copy “C:\Program Files\acontis_technologies\SysMgr\Templates\_patch\” to “C:\Program Files\acontis_technologies\”
12.2. Optional
Copy VxWin to “C:\Program Files\acontis_technologies\VxWin\”
Copy RTOS32Win to “C:\Program Files\acontis_technologies\RTOS32Win\”
12.3. Execution
Start System Manager
C:\Program Files\acontis_technologies\SysMgr\HvSystemManager.exe
Open in Browser
Select as Hypervisor
LxWin (can be used for LxWin, VxWin, RTOS32Win)
VxWin (for future use)
RTOSVisor (required for Hypvervisor remote configuration over TCP/MQTT)
12.4. Known Issues
First start of RTLinux fails with following error code because the uploader changes the memory configuration, after reboot it will work:
Uploader return code: 0x00000037 (Visible, if all messages are enabled!)
Install “Microsoft Visual C++ 2015 Redistributable Update 3 RC”
https://www.microsoft.com/en-US/download/details.aspx?id=52685 (vc_redist.x64.exe)
required by RtosLibDotNet.dll / RtosLibDotNetNative.dll
All folders are in “C:\Program Files\acontis_technologies\” because SystemManager must be relative to LxWin, VxWin, … (like in Linux)
Memory configuration is hard-coded (copied from trace)
Uploader can dump memory configuration into log with trace on
Uploader requires a cmdline option to dump memory configuration (This will remove the additional reboot after first start)