5. Real-time Ethernet Driver
The EC-Simulator stack currently supports a variety of different Real-time Ethernet Driver modules, each of which contained in a single library file, which is loaded by the core library dynamically. Which library actually is loaded, is depending on the Real-time Ethernet Driver parameters at runtime.
Real-time means operating directly on the network device’s register set instead of using the operating system’s native driver.
The principle of the Real-time Ethernet Driver selection is that the Ethernet Driver name (Ethernet Driver identification) is used to determine the location and name of a registration function called by EC-Simulator and registers function pointers that allow access to the Real-time Ethernet Driver functional entries.
The EtherCAT Real-time Ethernet Driver will be initialized using a Real-time Ethernet Driver specific configuration parameter set.
A pointer to this parameter set is part of EC-Simulator’s initialization settings when calling the function esInitSimulator() .
EC-Simulator supports two Real-time Ethernet Driver operating modes:
- Interrupt mode all received Ethernet frames will be processed immediately in the context of the Real-time Ethernet Driver receiver task.
- Polling mode, the application must cyclically call esExecJob() with job eUsrJob_ProcessAllRxFrames in order to trigger EC-Simulator to call the Real-time Ethernet Driver receiver polling function and process received frames.
Important
In polling mode, the master cycle time must be at least two times higher than the simulator cycle time. E.g. if the simulator runs with 1 ms, the master cycle time must be at least 2 ms. If the Real-time Ethernet Driver is running in interrupt mode (non-standard), processing of received frames is done immediately after the frame is received.
Note
Real-time Ethernet Driver modules not listed here may be available if purchased additionally. Not all Real-time Ethernet Driver modules support interrupt mode.