1.2. Configuration with EC-Engineer

The EC-Engineer automatically chooses the DC settings for SubDevices as proposed by the device’s vendor and sets DCM mode to bus shift.

The settings can be changed according to the project’s needs. DC options are part of the EC-Engineer Expert Mode. The Expert Mode can be activated from the menu:

EC-Engineer menu showing how to activate Expert Mode for accessing Distributed Clocks configuration options

1.2.1. Distributed Clocks MainDevice settings (Expert)

In this tab, the user can change distributed clocks related settings. The tab is only available if the configuration contains SubDevices.

EC-Engineer Expert Mode Distributed Clocks MainDevice settings tab showing Reference Clock, MainDevice Shift, Bus Shift, and Sync Window Monitoring options
  • Reference Clock Name: Name of the reference clock. By default, this is the first SubDevice with DC support.

  • MainDevice Shift: The reference clock controls the MainDevice time

  • Bus Shift: The MainDevice time controls the reference clock. A command will be inserted in the Cyclic frame to adjust the reference clock system time (write to register 0x0910).

  • Continuous Propagation Compensation: A command will be inserted in the Cyclic frame which allows the EtherCAT® MainDevice to measure and compensate the propagation delay time by time.

  • Sync Window Monitoring: A command will be inserted in the cyclic frame to read the ESC registers 0x092C. If this is selected the MainDevice will throw a notification.

  • Show 64Bit System Time: MainDevice supports SubDevices with 32bit and 64bit system time register (0x0910). If this is selected he will interpret it as 64bit system time.

Note

If no reference clock is displayed, please ensure at least one SubDevice in the network is configured for DC operation mode Distributed Clocks SubDevice settings (Expert)

1.2.2. Distributed Clocks SubDevice settings (Expert)

In this tab, the user can change distributed clocks related settings. The tab is only available if the vendor of the device specified the DC usage. Sync signal generation or DC latching is selected automatically according to Operation Mode.

EC-Engineer Expert Mode Distributed Clocks SubDevice settings tab showing DC operation modes and Sync Unit Cycle configuration
  • Operation Mode: Selectable DC operation modes. The modes cannot be edited.

  • Sync Unit Cycle: Base interval in microseconds which will be used from MainDevice. The Sync Units can be activated and configured to generate signals.

See also

SyncSignal Generation in the ET1100 Datasheet for time describing

Examples of Various SYNC0/SYNC1 Cycle Time Combinations