DCM Modes

2.1.1. DCM Modes

The following DCM Modes are available:

Name

Purpose

BusShift

Synchronize SubDevices to MainDevice timer (Default)

MasterShift

Synchronize MainDevice timer to SubDevice. Feasibility depending on target HW and SW.

LinkLayerRefClock

Bus Shift using Link Layer clock. Special HW needed.

MasterRefClock

Bus Shift excluding reference clock controlling. Lowers CPU usages, but very high timer accuracy needed.

DCX

Synchronization of two or more EtherCAT® segments by a bridge device. Only available with Feature Pack External Synchronization.

The Distributed Clocks MainDevice Synchronization (DCM) in Bus Shift mode adjusts the bus time register of the DC reference clock. All DC SubDevices converge to this time. This mode is useful to synchronize multiple EtherCAT® networks or if it is not possible to adjust the timing of the MainDevice.

See also

emDcmConfigure()