2.3. Programmer’s Guide
2.3.1. emDcmConfigure
-
static EC_T_DWORD ecatDcmConfigure(const EC_T_DCM_CONFIG *pDcmConfig, EC_T_DWORD dwInSyncTimeout)
-
EC_T_DWORD emDcmConfigure(EC_T_DWORD dwInstanceID, const EC_T_DCM_CONFIG *pDcmConfig, EC_T_DWORD dwInSyncTimeout)
Configure DC master synchronization.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pDcmConfig – [in] Configuration information, a pointer to a structure of type EC_T_DCM_CONFIG
dwInSyncTimeout – [in] Currently not implemented
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_DCM_CONFIG
Public Members
-
EC_T_DCM_MODE eMode
[in] DCM mode
-
EC_T_DCM_CONFIG_BUSSHIFT BusShift
[in] BusShift configuration. Valid if eMode is set to eDcmMode_BusShift.
-
EC_T_DCM_CONFIG_MASTERSHIFT MasterShift
[in] MasterShift configuration. Valid if eMode is set to eDcmMode_MasterShift.
-
EC_T_DCM_CONFIG_LINKLAYERREFCLOCK LinkLayerRefClock
[in] LinkLayerRefClock configuration. Valid if eMode is set to eDcmMode_LinkLayerRefClock.
-
EC_T_DCM_CONFIG_MASTERREFCLOCK MasterRefClock
[in] MasterRefClock configuration. Valid if eMode is set to eDcmMode_MasterRefClock.
-
EC_T_DCM_CONFIG_DCX Dcx
[in] DCX configuration. Valid if eMode is set to eDcmMode_Dcx.
-
EC_T_DCM_MODE eMode
-
struct EC_T_DCM_CONFIG_BUSSHIFT
Public Members
-
EC_T_INT nCtlSetVal
[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero).
-
EC_T_INT nCtlGain
[in] Proportional gain in ppt (part per thousand). Default is value 2. A value of 0 sets the default value.
-
EC_T_INT nCtlDriftErrorGain
[in] Multiplier for drift error. Default value is 3. A value of 0 sets the default value.
-
EC_T_INT nMaxValidVal
[in] Error inputs above this value are considered invalid. If error input prediction is valid then the difference between the error input and the expected value is taken. Default value is 3000. A value of 0 sets the default value.
-
EC_T_BOOL bLogEnabled
[in] If set to EC_TRUE, logging information are generated and can be got by calling emDcmGetLog()
-
EC_T_DWORD dwInSyncLimit
[in] Limit [ns] for InSync monitoring. Default value is 20% of the cycle time. A value of 0 sets the default value.
-
EC_T_DWORD dwInSyncSettleTime
[in] Settle time [ms] for InSync monitoring. Default value is 1500ms. A value of 0 sets the default value.
-
EC_T_BOOL bCtlOff
[in] If set to EC_TRUE, control loop is disabled. Combined with bLogEnabled, it makes possible to analyze the natural drift between the stack cycle and the reference clock.
-
EC_T_BOOL bUseDcLoopCtlStdValues
[in] If set to EC_TRUE, the values of ESC DC time loop control register 0x930 and 0x934 are not changed by master. This could increase the time it takes to get the InSync. Use only if there are problems with the reference clock to get InSync.
-
EC_T_VOID *pGetTimeElapsedSinceCycleStartContext
[in] Optional context for the pfnGetTimeElapsedSinceCycleStart function, will be passed as first parameter to this function/static method
-
EC_PF_DC_GETTIMEELAPSEDSINCECYCLESTART pfnGetTimeElapsedSinceCycleStart
[in] Setting this function enables synchronising the DC SYNC0 to the CycleStart instead of the time frame send. DC SYNC0 is therefore related to the CycleStart instead of the time frame send. Function must return EC_E_NOERROR to work. If 0 (nullptr, EC_NULL) EC_E_NOTSUPPORTED will be returned on attempt to call.
-
EC_T_INT nCtlSetVal
-
struct EC_T_DCM_CONFIG_MASTERSHIFT
Public Members
-
EC_T_INT nCtlSetVal
[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero).
-
EC_T_INT nCtlGain
[in] Proportional gain in ppt (part per thousand). Default is value 2. A value of 0 sets the default value.
-
EC_T_INT nCtlDriftErrorGain
[in] Multiplier for drift error. Default value is 3. A value of 0 sets the default value.
-
EC_T_INT nMaxValidVal
[in] Error inputs above this value are considered invalid. If error input prediction is valid then the difference between the error input and the expected value is taken. Default value is 3000. A value of 0 sets the default value.
-
EC_T_BOOL bLogEnabled
[in] If set to EC_TRUE, logging information are generated and can be got by calling emDcmGetLog()
-
EC_T_DWORD dwInSyncLimit
[in] Limit [ns] for InSync monitoring. Default value is 20% of the cycle time. A value of 0 sets the default value.
-
EC_T_DWORD dwInSyncSettleTime
[in] Settle time [ms] for InSync monitoring. Default value is 1500ms. A value of 0 sets the default value.
-
EC_T_BOOL bCtlOff
[in] If set to EC_TRUE, control loop is disabled. Combined with bLogEnabled, it makes possible to analyze the natural drift between the stack cycle and the reference clock. Also it provides reading of current adjustment value using emDcmGetAdjust function.
-
EC_T_DC_STARTTIME_CB_DESC DcStartTimeCallbackDesc
[in] If not null, DC start time calculated by application, otherwise by master. See also EC_T_DC_STARTTIME_CB_DESC. Shift value configured in ENI will still be applied.
-
EC_T_VOID *pGetTimeElapsedSinceCycleStartContext
[in] Optional context for the pfnGetTimeElapsedSinceCycleStart function, will be passed as first parameter to this function/static method
-
EC_PF_DC_GETTIMEELAPSEDSINCECYCLESTART pfnGetTimeElapsedSinceCycleStart
[in] Setting this function enables synchronising the DC SYNC0 to the CycleStart instead of the time frame send. DC SYNC0 is therefore related to the CycleStart instead of the time frame send. Function must return EC_E_NOERROR to work. If 0 (nullptr, EC_NULL) EC_E_NOTSUPPORTED will be returned on attempt to call.
-
EC_T_INT nCtlSetVal
-
struct EC_T_DCM_CONFIG_LINKLAYERREFCLOCK
Public Members
-
EC_T_INT nCtlSetVal
[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero).
-
EC_T_BOOL bLogEnabled
[in] If set to EC_TRUE, logging information are generated and can be got by calling emDcmGetLog()
-
EC_T_DWORD dwInSyncLimit
[in] Limit [ns] for InSync monitoring. Default value is 20% of the cycle time. A value of 0 sets the default value.
-
EC_T_DWORD dwInSyncSettleTime
[in] Settle time [ms] for InSync monitoring. Default value is 1500ms. A value of 0 sets the default value.
-
EC_T_DC_STARTTIME_CB_DESC DcStartTimeCallbackDesc
[in] If not null, DC start time calculated by application, otherwise by master. See also EC_T_DC_STARTTIME_CB_DESC. Shift value configured in ENI will still be applied.
-
EC_T_INT nCtlSetVal
-
struct EC_T_DCM_CONFIG_MASTERREFCLOCK
Public Members
-
EC_T_INT nCtlSetVal
[in] Controller set value [ns]. This is the time distance between the cyclic frame send time and the DC base on bus (SYNC0 if shift is zero).
-
EC_T_BOOL bLogEnabled
[in] If set to EC_TRUE, logging information are generated and can be got by calling emDcmGetLog()
-
EC_T_DWORD dwInSyncLimit
[in] Limit [ns] for InSync monitoring. Default value is 20% of the cycle time. A value of 0 sets the default value.
-
EC_T_DWORD dwInSyncSettleTime
[in] Settle time [ms] for InSync monitoring. Default value is 1500ms. A value of 0 sets the default value.
-
EC_T_VOID *pGetHostTimeContext
[in] Optional context for the pfnGetHostTime function, will be passed as first parameter to this function/static method
-
EC_PF_DC_GETHOSTTIME pfnGetHostTime
[in] Mandatory function to offer the host time for the MasterRefClock mode. This time will be distributed to the slaves. If 0 (nullptr, EC_NULL) MasterRefClock mode will not work.
-
EC_T_DC_STARTTIME_CB_DESC DcStartTimeCallbackDesc
[in] If not null, DC start time calculated by application, otherwise by master. See also EC_T_DC_STARTTIME_CB_DESC. Shift value configured in ENI will still be applied.
-
EC_T_INT nCtlSetVal
Contains the configuration information for the DCX external synchronization mode.
See also
Feature Pack “External Synchronization” for further details.
-
struct EC_T_DC_STARTTIME_CB_DESC
Public Members
-
EC_PF_DC_STARTTIME_CB pfnCallback
[in] DC start time callback function pointer. If not EC_NULL, DC start time calculated by application, otherwise by master.
-
EC_PF_DC_STARTTIME_CB pfnCallback
-
typedef EC_T_DWORD (*EC_PF_DC_STARTTIME_CB)(EC_T_VOID *pvContext, EC_T_WORD wSlaveFixedAddr, EC_T_UINT64 *pqwDcStartTime)
EC-Master requests DC start time for every single slave from a given callback DcStartTimeCallbackDesc with slave station address as input parameter. The slave specific DC start time value will be passed directly to the slave without modifications by master. This means no other values like nCtlSetVal will be added. Shift value configured in ENI will still be applied.
- Param pvContext:
[in] Arbitrarily application-defined parameter passed to callback
- Param wSlaveFixedAddr:
[in] Slave fixed address
- Param pqwDcStartTime:
[out] DC start time for specific slave
- Return:
EC_E_NOERROR or error code
2.3.2. emDcmGetStatus
-
static EC_T_DWORD ecatDcmGetStatus(EC_T_DWORD *pdwErrorCode, EC_T_INT *pnDiffCur, EC_T_INT *pnDiffAvg, EC_T_INT *pnDiffMax)
-
EC_T_DWORD emDcmGetStatus(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwErrorCode, EC_T_INT *pnDiffCur, EC_T_INT *pnDiffAvg, EC_T_INT *pnDiffMax)
Get DC master synchronization controller status.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwErrorCode – [out] Pointer to current error code of the DCM controller. Possible values are:
EC_E_NOTREADY DCM control loop is not running
EC_E_BUSY DCM control loop is running and try to get InSync
DCM_E_MAX_CTL_ERROR_EXCEED Set if the controller error exceeds the InSyncLimit
DCM_E_DRIFT_TO_HIGH DCM control loop not able to compensate drift. Drift above 600ppm
pnDiffCur – [out] Pointer to current difference between set value and actual value of controller in nanoseconds
pnDiffAvg – [out] Pointer to average difference between set value and actual value of controller in nanoseconds
pnDiffMax – [out] Pointer to maximum difference between set value and actual value of controller in nanoseconds
- Returns:
EC_E_NOERROR if status retrieval was successful
EC_E_NOTSUPPORTED if the DC feature is not supported/switched off. EC-Master stack has to be compiled with DC support see “define INCLUDE_DC_SUPPORT”.
EC_NULL does not appear in normal flow, if EC_NULL is returned we are in a very exceptional case where m_poDcm == NULL (SW error detection)
2.3.3. emDcmResetStatus
2.3.4. emDcmGetBusShiftConfigured
-
EC_T_DWORD emDcmGetBusShiftConfigured(EC_T_DWORD dwInstanceID, EC_T_BOOL *pbBusShiftConfigured)
Determines if DCM Bus Shift is configured/possible in configuration (ENI file).
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pbBusShiftConfigured – [out] EC_TRUE if DCM bus shift mode is supported by the current configuration
- Returns:
EC_E_NOERROR or error code
2.3.5. emDcmGetLog
-
EC_T_DWORD emDcmGetLog(EC_T_DWORD dwInstanceID, EC_T_CHAR **pszLog)
Get logging information from the DCM controller.
This function returns non-zero pointer only if bLogEnabled was set to EC_TRUE in EC_T_DCM_CONFIG.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pszLog – [out] Pointer to a string containing the current logging information
- Returns:
EC_E_NOERROR or error code
See also
Controller adjustment for content description of pszLog
2.3.6. emIoCtl - EC_IOCTL_DCM_GET_LOG
-
EC_IOCTL_DCM_GET_LOG
Get logging information from the DCM controller.
- Parameters:
pbyInBuf – [in] Should be set to EC_NULL
dwInBufSize – [in] Should be set to 0
pbyOutBuf – [out] Pointer to struct EC_T_DCM_LOG
dwOutBufSize – [in] Size of the output buffer in bytes
pdwNumOutData – [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer pbyOutBuf
- Returns:
EC_E_NOERROR or error code
See also
emIoCtl() in the EC-Master Class B documentation
2.3.7. emDcmShowStatus
2.3.8. emDcmGetAdjust
-
EC_T_DWORD emDcmGetAdjust(EC_T_DWORD dwInstanceID, EC_T_INT *pnAdjustPermil)
Returns the current adjustment value for the timer.
bCtlOff must be set to EC_TRUE in EC_T_DCM_CONFIG to enable external adjustment.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pnAdjustPermil – [out] Current adjustment value of the timer
- Returns:
EC_E_NOERROR or error code
2.3.9. DCM specific error codes
2.3.10. Notifications
At startup the MainDevice raises the notifications emNotify - EC_NOTIFY_DC_SLV_SYNC, emNotify - EC_NOTIFY_DC_STATUS and emNotify - EC_NOTIFY_DCM_SYNC at MainDevice state transition from INIT to PREOP.
The order is typically as follows ( emNotify - EC_NOTIFY_DCM_SYNC may be before or after reaching PREOP):
EC_NOTIFY_STATECHANGED(INIT)[…]
EC_NOTIFY_DC_SLV_SYNC […]
EC_NOTIFY_DC_STATUS […]
[EC_NOTIFY_DCM_SYNC] […]
EC_NOTIFY_STATECHANGED(PREOP) […]
[EC_NOTIFY_DCM_SYNC] […]
EC_NOTIFY_STATECHANGED(SAFEOP) […]
EC_NOTIFY_STATECHANGED(OP) […]
2.3.11. emNotify - EC_NOTIFY_DCM_SYNC
DCM InSync notification.
This notification is enabled by default.
- emNotify - EC_NOTIFY_DCM_SYNC
- Parameter
pbyInBuf: [in] Pointer to notification descriptor EC_T_DCM_SYNC_NTFY_DESCdwInBufSize: [in] sizeof(EC_T_DCM_SYNC_NTFY_DESC)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_DCM_SYNC_NTFY_DESC
Public Members
-
EC_T_DWORD IsInSync
[in] EC_TRUE as long as time of master and reference clock are in sync. False if the InSyncLimit from the bus shift configuration is exceeded.
-
EC_T_INT nCtlErrorNsecCur
[in] Current difference [ns] between set value and actual value of controller
-
EC_T_DWORD IsInSync
See also
emIoCtl - EC_IOCTL_SET_NOTIFICATION_ENABLED in the EC-Master Class B documentation for controlling the deactivation