8. Application programming interface, reference
Function prototypes, definitions etc. of the API can be found in the header file EcMonitor.h which is the main header file to include when using EC-Monitor.
Fundamental types
-
typedef void *EC_T_PVOID
Pointer of type void
-
typedef int EC_T_BOOL
Boolean
-
typedef char EC_T_CHAR
Character, 8 bit
-
typedef unsigned short EC_T_WCHAR
Wide-character, 16 bit
-
typedef unsigned char EC_T_BYTE
Byte, unsigned integer 8 bit
-
typedef unsigned char *EC_T_PBYTE
Pointer of type EC_T_BYTE
-
typedef unsigned short EC_T_WORD
Word, unsigned integer 16 bit
-
typedef unsigned int EC_T_DWORD
Double word, unsigned integer 32 bit
-
typedef signed char EC_T_SBYTE
Signed-Byte, signed integer 8 bit
-
typedef signed short EC_T_SWORD
Signed-Word, signed integer 16 bit
-
typedef signed int EC_T_SDWORD
Signed-Double-Word, signed integer 32 bit
-
typedef int EC_T_INT
Integer
-
typedef unsigned int EC_T_UINT
Unsigned-Integer
-
typedef short EC_T_SHORT
Short
-
typedef unsigned short EC_T_USHORT
Unsigned-Short
-
typedef float EC_T_REAL
Real, floating point
-
typedef double EC_T_LREAL
long Real, floating point
-
typedef unsigned long long EC_T_UINT64
Unsigned integer 64 bits
-
typedef signed long long EC_T_INT64
Signed integer 64 bits
-
EC_T_VOID
Void type