5.2. Event notification

The EC-Monitor provides event notification for a great number of events. These events are for example:

  • Bus state change

  • Link state change

  • Working counter errors

  • …

Any thread can register for these events to be notified. This is achieved by calling the API function

EC_T_DWORD emRegisterClient(EC_T_DWORD dwInstanceID, EC_PF_NOTIFY pfnNotify, EC_T_VOID *pCallerData, EC_T_REGISTERRESULTS *pRegResults)

An example implementation for processing notifications is contained in the class CEmNotification of the EcMonitorDemo example, see Examples/Common/EcNotification.cpp.. It implements the full framework to catch and process the EC-Monitor notifications. The class is instantiated once and registered at the EC-Monitor with the call emRegisterClient(). It contains the method ecatNotify() as major entry point (or callback function) for every event notification.

There are two different ways events can be handled. The method of handling an event is primarily determined by the time required to handle the event and the processing context in which the event is to be handled.

5.2.1. Direct event notification handling

Minor events that take a very short time to process can be handled directly in the context in which they are recognized. A possible example of such an event is the detection of a false working counter (WKC).

skinparam monochrome true
skinparam SequenceMessageAlign direction
hide footbox

participant JobTask as "EcMonitorJobTask"
participant EcEmbedded as "EC-Monitor"
participant EcNotification

activate JobTask
JobTask->EcEmbedded : emExecJob(ProcessAllRxFrames)

activate EcEmbedded
EcEmbedded->EcEmbedded : Receive Frames
EcEmbedded->EcEmbedded : Process Frames
EcEmbedded->EcEmbedded : Detect Errors
activate EcEmbedded
EcEmbedded->EcNotification : invoke NotifyCallback()

activate EcNotification
EcNotification->EcNotification : ecatNotify()
EcNotification->: Error Log Message
return

deactivate EcEmbedded
return

JobTask->JobTask : myAppWorkPd()

The event handling is reduced to simply issuing a log message, which is not time critical. The event is handled directly within the context of the emExecJob() function.

5.2.2. Postponed notification handling

Events that require more time-consuming processing cannot be handled directly in the context in which they are detected. The handling or processing of the event must be postponed. This is accomplished through a queue, which is also readily implemented using the CEmNotification class.

skinparam monochrome true
skinparam SequenceMessageAlign direction
skinparam SequenceBoxBorderColor transparent
hide footbox

participant EcDemoApp
participant JobTask as "EcMonitorJobTask"
participant EcEmbedded as "EC-Monitor"
box
    participant EcNotification
    database Notifications
end box

activate EcDemoApp
activate JobTask
JobTask->EcEmbedded : emExecJob(ProcessAllRxFrames)

activate EcEmbedded
EcEmbedded->EcEmbedded : Receive Frames
EcEmbedded->EcEmbedded : Process Frames
EcEmbedded->EcEmbedded : Detect Errors
activate EcEmbedded
EcEmbedded->EcNotification : invoke NotifyCallback()

activate EcNotification
EcNotification->EcNotification : ecatNotify()
activate EcNotification
EcNotification->Notifications : EnqueueJob()
deactivate EcNotification
return

deactivate EcEmbedded
return
deactivate JobTask
...
EcDemoApp->EcNotification : ProcessNotificationJobs()
activate EcNotification
EcNotification->Notifications : DequeueJob()
EcNotification<--Notifications
activate EcNotification
EcNotification->EcNotification : Process()
deactivate EcNotification
return

By calling periodically CEmNotification::ProcessNotificationJobs(), the application checks and handles all queued notifications.

Important

The call of CEmNotification::ProcessNotificationJobs() shall NOT be executed in the context of EcMonitorJobTask(). As the CPU time consumption may be high, this would have a high impact to the real-time behavior of the cyclic operation.