8.10. Hot Connect
8.10.1. emHCGetNumGroupMembers
-
EC_T_DWORD emHCGetNumGroupMembers(EC_T_DWORD dwInstanceID, EC_T_DWORD dwGroupIndex)
Get number of slaves belonging to a specific Hot-Connect group.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwGroupIndex – [in] Index of Hot-Connect group, 0 is the mandatory group
- Returns
Number of slaves
8.10.2. emHCGetSlaveIdsOfGroup
-
EC_T_DWORD emHCGetSlaveIdsOfGroup(EC_T_DWORD dwInstanceID, EC_T_DWORD dwGroupIndex, EC_T_DWORD *adwSlaveId, EC_T_DWORD dwMaxNumSlaveIds)
Get a list of Slave ID’s belonging to a specific Hot-Connect group.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwGroupIndex – [in] Index of Hot-Connect group, 0 is the mandatory group
adwSlaveId – [out] Preallocated Slave ID list buffer
dwMaxNumSlaveIds – [in] Size of Slave ID list buffer
- Returns
EC_E_NOERROR or error code
8.10.3. emNotify - EC_NOTIFY_HC_DETECTADDGROUPS
This notification is raised when HotConnect group detection is finished, after slave addition.
- emNotify - EC_NOTIFY_HC_DETECTADDGROUPS
- Parameter
pbyInBuf: [in] pointer to notification descriptor EC_T_HC_DETECTALLGROUP_NTFY_DESCdwInBufSize: [in] sizeof(EC_T_HC_DETECTALLGROUP_NTFY_DESC)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_HC_DETECTALLGROUP_NTFY_DESC
Public Members
-
EC_T_DWORD dwResultCode
Result of Group detection
-
EC_T_DWORD dwGroupCount
Total number of Groups
-
EC_T_DWORD dwGroupsPresent
Number of connected groups
-
EC_T_DWORD dwGroupMask
Bitmask of first 32 Groups. 1 = present, 0 = absent
-
EC_T_DWORD adwGroupMask[100]
Bitmask of first 3200 Groups.
-
EC_T_DWORD dwResultCode
8.10.4. emNotify - EC_NOTIFY_HC_PROBEALLGROUPS
This notification is raised when HotConnect Group Detection is finished, after Slave Disappearance.
- emNotify - EC_NOTIFY_HC_PROBEALLGROUPS
- Parameter
pbyInBuf: [in] pointer to notification descriptor EC_T_HC_DETECTALLGROUP_NTFY_DESCdwInBufSize: [in] sizeof(EC_T_HC_DETECTALLGROUP_NTFY_DESC)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
8.10.5. emNotify - EC_NOTIFY_HC_TOPOCHGDONE
This notification is raised when HotConnect has completely processed a topology change.
- emNotify - EC_NOTIFY_HC_TOPOCHGDONE
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD (EC_E_NOERROR on success, Error code otherwise)dwInBufSize: [in] sizeof(EC_T_DWORD)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The notification is raised when the slaves reached the current bus state.