7.2. Windows NDIS - emllNdis
As default EC-Monitor for Windows contains emllNdis.dll to use a native Windows driver for EtherCAT.
The acontis ECAT Protocol Driver is needed to use the NDIS Link Layer and can be installed from
Bin/Windows/x64/EcatNdisSetup-x86_64Bit.msiorBin/Windows/x86/EcatNdisSetup-x86_32Bit.msi
respectively depend on the Windows Operating System Type of 64 Bit or 32 Bit.
IPv4 must be installed for the network adapter as the NDIS Link Layer uses the IP address to identify the network adapter.
The parameters to the NDIS Link Layer are setup-specific. The function CreateLinkParmsFromCmdLineNDIS() in EcSelectLinkLayer.cpp demonstrates how to initialize the Link Layer instance.
-
struct EC_T_LINK_PARMS_NDIS
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_NDIS
-
EC_T_CHAR szAdapterName[EC_NDIS_ADAPTER_NAME_SIZE]
ServiceName of network adapter, see HKLM\SOFTWARE\Microsoft\Windows NT\CurrentVersion\NetworkCards in registry (zero terminated)
-
EC_T_BYTE abyIpAddress[4]
IP address of network adapter
-
EC_T_BOOL bDisablePromiscuousMode
Disable adapter promiscuous mode
-
EC_T_BOOL bDisableForceBroadcast
Don’t change target MAC address to FF:FF:FF:FF:FF:FF
-
EC_T_LINK_PARMS linkParms
In case of problems while using the Link layer, it is advised to set the windows registry entry DontSetPromiscuousMode of the ECAT NDIS Protocol driver. This option is available since V3.1.3.02 of the driver. This can be done through the following steps:
Install ECAT NDIS Protocol driver (V3.1.3.02 or newer version)
Open the registry editor
Switch to Computer\HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\Ecatndis, or just look for Ecatndis in the editor
Create a new entry named DontSetPromiscuousMode
Change the value of DontSetPromiscuousMode to 1
Close the registry editor and restart your computer