8.5. Diagnosis
In case of errors on the bus or in one or multiple slaves the EtherCAT monitor stack will notify the application about such an event.
The error notifications can be separated into two classes:
- Slave unrelated errors
Notifications don’t contain this information even if one specific slave has caused an error. For example if one or multiple slaves are powered off the working counter of the cyclic commands would be wrong. In that case the emNotify - EC_NOTIFY_CYCCMD_WKC_ERROR error notification will be generated.
- Slave related errors
Notifications will also contain the information about which slave has generated an error.
Example Error Scenario
Slave is powered off or disconnected while bus is operational
If the monitor is operational it cyclically sends EtherCAT commands to read and write the slave’s process data. It expects the working counter to be incremented to the appropriate value. If one slave is powered off the monitor will generate the emNotify - EC_NOTIFY_CYCCMD_WKC_ERROR to indicate such an event. Also the monitor detects a DL status event and performs a bus scan as reaction on this. For the not reachable slaves (powered off or disconnected) the monitor generates the notification emNotify - EC_NOTIFY_SLAVE_PRESENCE.
A possible error recovery scenario would be to stay operational and in parallel wait until the slave is powered on again. The next step would be to determine the slave’s state and set it operational again:
- Monitor calls emNotify - EC_NOTIFY_CYCCMD_WKC_ERROR
Application gets informed
WKC State in Diagnosis Image changes
Use cases
- Slave is disconnected or powered off:
EtherCAT Master detects a DL status event interrupt an performs a bus scan.
Monitor calls emNotify - EC_NOTIFY_SLAVE_PRESENCE
- Slave is re-connected or powered on:
EtherCAT Master detects a DL status event interrupt an performs a bus scan.
Monitor calls emNotify - EC_NOTIFY_SLAVE_PRESENCE.
Application could wait until all slaves are re-connected by calling the functions
emGetNumConnectedSlaves()andemGetNumConfiguredSlaves().
8.5.1. emIoControl - EC_IOCTL_SB_STATUS_GET
This call will get the status of the last bus scan.
- emIoControl - EC_IOCTL_SB_STATUS_GET
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_SB_STATUS_NTFY_DESC.dwOutBufSize: [in] Size of the output buffer in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Return
EC_E_NOERROR or error code
See also
8.5.2. emIoControl - EC_IOCTL_GET_SLVSTATISTICS
Get Slave’s statistics counter. Counters are collected on a regularly base (default: off) and show errors on Ethernet Layer.
- emIoControl - EC_IOCTL_GET_SLVSTATISTICS
- Parameter
pbyInBuf: [in] Pointer to a EC_T_DWORD type variable containing the slave id.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Pointer to struct EC_T_SLVSTATISTICS_DESCdwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Return
EC_E_NOERROR or error code
-
struct EC_T_SLVSTATISTICS_DESC
Public Members
-
EC_T_BYTE abyInvalidFrameCnt[ESC_PORT_COUNT]
[out] Invalid Frame Counters per Slave Port
-
EC_T_BYTE abyRxErrorCnt[ESC_PORT_COUNT]
[out] RX Error Counters per Slave Port
-
EC_T_BYTE abyFwdRxErrorCnt[ESC_PORT_COUNT]
[out] Forwarded RX Error Counters per Slave Port
-
EC_T_BYTE byProcessingUnitErrorCnt
[out] Processing Unit Error Counter
-
EC_T_BYTE byPdiErrorCnt
[out] PDI Error Counter
-
EC_T_WORD wAlStatusCode
[out] AL Status Code
-
EC_T_BYTE abyLostLinkCnt[ESC_PORT_COUNT]
[out] Lost Link Counters per Slave Port
-
EC_T_UINT64 qwReadTime
[out] Timestamp of the last read [ns]
-
EC_T_UINT64 qwChangeTime
[out] Timestamp of the last counter change [ns]
-
EC_T_BYTE abyInvalidFrameCnt[ESC_PORT_COUNT]
8.5.3. emGetSlaveStatistics
-
EC_T_DWORD emGetSlaveStatistics(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_SLVSTATISTICS_DESC *pSlaveStatisticsDesc)
Get Slave’s statistics counter.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave id
pSlaveStatisticsDesc – [out] Pointer to structure EC_T_SLVSTATISTICS_DESC
- Returns
EC_E_NOERROR or error code
8.5.4. emIoControl - EC_IOCTL_CLR_SLVSTATISTICS
Clear all buffered error registers for all slaves. The actual counters on the slaves remain unchanged.
- emIoControl - EC_IOCTL_CLR_SLVSTATISTICS
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
8.5.5. emClearSlaveStatistics
-
EC_T_DWORD emClearSlaveStatistics(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId)
Clears all error registers of a slave.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave Id, INVALID_SLAVE_ID clears all slaves
- Returns
EC_E_NOERROR or error code
Note
Only the buffered error register values are deleted. The actual counters on the slaves remain unchanged.
See also
8.5.6. emGetDiagnosisImagePtr
-
EC_T_BYTE *emGetDiagnosisImagePtr(EC_T_DWORD dwInstanceID)
Gets the diagnosis image pointer.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns
Diagnosis image pointer
8.5.7. emGetMasterSyncUnitInfoNumOf
-
EC_T_DWORD emGetMasterSyncUnitInfoNumOf(EC_T_DWORD dwInstanceID)
Get number of Master Sync Units info entries.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns
Number of Master Sync Units info entries
8.5.8. emGetMasterSyncUnitInfo
-
EC_T_DWORD emGetMasterSyncUnitInfo(EC_T_DWORD dwInstanceID, EC_T_WORD wMsuId, EC_T_MSU_INFO *pMsuInfo)
Get information about specific Master Sync Unit.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
wMsuId – [in] Master Sync Unit to get the information from
pMsuInfo – [out] Pointer to an EC_T_MSU_INFO structure receiving the Master Sync Unit information
- Returns
EC_E_NOERROR or error code
MSU_ID_ALL_INFO_ENTRIES retrieves the information from all master sync units at once. The application must ensure that pMsuInfo is capable for all entries.
-
struct EC_T_MSU_INFO
Public Members
-
EC_T_WORD wMsuId
[out] master sync unit ID
-
EC_T_DWORD dwBitOffsIn
[out] input bit offset of master sync unit in process data image
-
EC_T_DWORD dwBitSizeIn
[out] input bit size of master sync unit
-
EC_T_DWORD dwBitOffsOut
[out] output bit offset of master sync unit in process data image
-
EC_T_DWORD dwBitSizeOut
[out] output bit size of master sync unit
-
EC_T_WORD wWkcStateDiagOffsIn
[out] Offset of WkcState bit in diagnosis image WkcState bit values: 0 = Data Valid, 1 = Data invalid
-
EC_T_WORD wWkcStateDiagOffsOut
[out] Offset of WkcState bit in diagnosis image WkcState bit values: 0 = Data Valid, 1 = Data invalid
-
EC_T_DWORD adwReserved[16]
reserved
-
EC_T_WORD wMsuId
See also