8.9. File access over EtherCAT (FoE)
The EC-Monitor can record file transfers via the FoE protocol between an EtherCAT master and a slave. These FoE transfers can be forwarded to the application as segmented packets in real time via the notifications emNotify - eMbxTferType_FOE_SEG_DOWNLOAD and emNotify - eMbxTferType_FOE_SEG_UPLOAD.
- In addition, the FoE transfers can be stored as a file on the file system. The files are automatically created and stored in
EC_T_MONITOR_INIT_PARMS::szFileStoragePath. The file name consists of the following: <TimeStamp[msec]>_Slave<StationAddress>_<FoeFileName>
- For example:
0123456789_Slave1001_firmware.bin
The notifications for FoE can be deactivated using the EC_T_MBX_PARMS::_EC_T_MBX_PARMS_FOE::bDisableNotifications parameter if they are not required or to save computing time.
If no file system is available or file storage is not desired, it can be disabled using the EC_T_MBX_PARMS::_EC_T_MBX_PARMS_FOE::bDisableFileStorage parameter.
If both parameters EC_T_MBX_PARMS::_EC_T_MBX_PARMS_FOE::bDisableNotifications and EC_T_MBX_PARMS::_EC_T_MBX_PARMS_FOE::bDisableFileStorage are set, the FoE monitoring is completely deactivated.
8.9.1. Notification sequence
Once the EC-Monitor detects an FoE transfer, the application is notified via an emNotify - eMbxTferType_FOE_DOWNLOAD_REQ or emNotify - eMbxTferType_FOE_UPLOAD_REQ notification. This notification contains basic information about the upcoming transfer, e.g. requested file name.
After that, each individual packet is transmitted via an emNotify - eMbxTferType_FOE_SEG_DOWNLOAD or emNotify - eMbxTferType_FOE_SEG_UPLOAD notification. The end of the transfer is set via the EC_T_MBXTFER::eTferStatus = eMbxTferStatus_TferDone.
Download
Upload
8.9.2. emNotify - eMbxTferType_FOE_DOWNLOAD_REQ
Notifies a FoE download request from the EtherCAT master to a slave.
- emNotify - eMbxTferType_FOE_DOWNLOAD_REQ
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, this structure contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The parameters that the master has requested from the slave are stored in the structure EC_T_MBX_DATA::FoE_Request which is part of EC_T_MBXTFER::MbxData.
-
struct EC_T_MBX_DATA_FOE_REQ
Public Members
-
EC_T_WORD wStationAddress
[out] Station address of the slave
-
EC_T_DWORD dwPassword
[out] FoE read/write request password
-
EC_T_CHAR szFileName[EC_MAX_FILE_NAME_SIZE]
[out] Name of the file to be read/write
-
EC_T_WORD wStationAddress
8.9.3. emNotify - eMbxTferType_FOE_SEG_DOWNLOAD
Transmits a data segment of the ongoing FoE download.
- emNotify - eMbxTferType_FOE_SEG_DOWNLOAD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, this structure contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The FoE download data segment is stored at EC_T_MBXTFER::pbyMbxTferData with size EC_T_MBXTFER::dwDataLen and may have to be buffered by the application.
Access to the memory area EC_T_MBXTFER::pbyMbxTferData outside of the notification caller context is illegal and the results are undefined.
Information about the current transfer are in structure EC_T_MBX_DATA::FoE which is part of EC_T_MBXTFER::MbxData. Among other things, it contains the slave station address EC_T_MBX_DATA_FOE::wStationAddress and the number of bytes already transmitted EC_T_MBX_DATA_FOE::dwTransferredBytes.
-
struct EC_T_MBX_DATA_FOE
Public Members
-
EC_T_DWORD dwTransferredBytes
[out] amount of transferred bytes
-
EC_T_DWORD dwRequestedBytes
[out] amount of bytes to be provided by application
-
EC_T_DWORD dwBusyDone
[out] If slave is busy: 0 … dwBusyEntire
-
EC_T_DWORD dwBusyEntire
[out] If dwBusyEntire > 0: Slave is busy
-
EC_T_CHAR szBusyComment[EC_FOE_BUSY_COMMENT_SIZE]
[out] Busy Comment from slave
-
EC_T_DWORD dwFileSize
[out] File size
-
EC_T_WORD wStationAddress
[out] Station address of the slave
-
EC_T_DWORD dwTransferredBytes
Note
The elements EC_T_MBX_DATA_FOE::dwRequestedBytes and EC_T_MBX_DATA_FOE::dwFileSize are not used by the EC-Monitor because they are not known at runtime.
8.9.4. emNotify - eMbxTferType_FOE_UPLOAD_REQ
Notifies a FoE upload request from the EtherCAT master to a slave.
- emNotify - eMbxTferType_FOE_DOWNLOAD_REQ
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, this structure contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The parameters that the master has requested from the slave are stored in the structure EC_T_MBX_DATA::FoE_Request which is part of EC_T_MBXTFER::MbxData.
-
struct EC_T_MBX_DATA_FOE_REQ
-
EC_T_WORD wStationAddress
-
EC_T_DWORD dwPassword
-
EC_T_CHAR szFileName[EC_MAX_FILE_NAME_SIZE]
-
EC_T_WORD wStationAddress
8.9.5. emNotify - eMbxTferType_FOE_SEG_UPLOAD
Transmits a data segment of the ongoing FoE upload.
- emNotify - eMbxTferType_FOE_SEG_UPLOAD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, this structure contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The FoE upload data segment is stored at EC_T_MBXTFER::pbyMbxTferData with size EC_T_MBXTFER::dwDataLen and may have to be buffered by the application.
Access to the memory area EC_T_MBXTFER::pbyMbxTferData outside of the notification caller context is illegal and the results are undefined.
Information about the current transfer are in structure EC_T_MBX_DATA::FoE which is part of EC_T_MBXTFER::MbxData. Among other things, it contains the slave station address EC_T_MBX_DATA_FOE::wStationAddress and the number of bytes already transmitted EC_T_MBX_DATA_FOE::dwTransferredBytes.
-
struct EC_T_MBX_DATA_FOE
Note
The elements EC_T_MBX_DATA_FOE::dwRequestedBytes and EC_T_MBX_DATA_FOE::dwFileSize are not used by the EC-Monitor because they are not known at runtime.
8.9.6. emNotify - EC_NOTIFY_FOE_MBSLAVE_ERROR
This error will be indicated in case a FoE mailbox slave send an error message.
Detailed error information is stored in structure EC_T_MBOX_FOE_ABORT_DESC which is part of EC_T_ERROR_NOTIFICATION_DESC.
-
struct EC_T_MBOX_FOE_ABORT_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_DWORD dwErrorCode
Error code
-
EC_T_CHAR achErrorString[MAX_STD_STRLEN]
FoE error string
-
EC_T_SLAVE_PROP SlaveProp
8.9.7. emConvertEcErrorToFoeError
-
EC_T_DWORD emConvertEcErrorToFoeError(EC_T_DWORD dwInstanceID, EC_T_DWORD dwErrorCode)
Convert master error code to FoE error code.
- Returns
FoE error code according to ETG1000.6 Table 92 - Error codes of FoE