2.3. Mixed mode of real SubDevices and simulated SubDevices
In order to implement restbus simulation it is possible to mix real SubDevices and simulated SubDevices like this:
All real SubDevices must be configured accordingly:
See also /EtherCATConfig/ExtendedConfig/Slaves/Slave/Simulated in the EXI file:
The EC-Simulator will automatically assign the network adapters to the corresponding ports in order of configuration.
See also
EC_T_SIMULATOR_INIT_PARMS::apLinkParms at esInitSimulator().