tenAsys INtime

4.1. tenAsys INtime

Real-time Ethernet Drivers are available for INtime. If using INtime with Windows running in parallel on the same host the network adapter has to be assigned to INtime. The network adapters should be passed to INtime using the INtime Device Manager. Please refer to the INtime user manual for this.

Search locations for Real-time Ethernet Drivers can be adjusted using the PATH environment variable.

4.1.1. OS Compiler settings

Besides the general settings from OS Compiler settings the following settings are necessary to build the example application for INtime.

Extra include paths
<InstallPath>\SDK\INC\INtime
<InstallPath>\Examples\Common\INtime
Extra source paths
<InstallPath>\Examples\Common\INtime
<InstallPath>\Sources\OsLayer\INtime
Extra library paths to the main EtherCAT® components
<InstallPath>\SDK\LIB\INtime