Error detection and diagnosis

3.6. Error detection and diagnosis

The EC-Simulator API functions generally return EC_E_NOERROR or an error code.

Messages are logged as described in esInitSimulator().

Important

Logging is typically done from within the JobTask context so the handler should queue the messages and process them in a low priority task. See logging in EcSimulatorSilDemo .