Broadcom NetXtreme - emllBcmNetXtreme

5.5. Broadcom NetXtreme - emllBcmNetXtreme

The parameters to the Real-time Ethernet Driver Broadcom® NetXtreme are setup-specific. The function CreateLinkParmsFromCmdLineBcmNetXtreme() in EcSelectLinkLayer.cpp demonstrates how to initialize the Link Layer instance.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_BCMNETXTREME.

Receive buffer count. Must be a power of 2, maximum 1024.

Transmit buffer count. Must be a power of 2, maximum 1024.

5.5.1. Supported PCI devices

Broadcom 571x PCI specific definitions (VendorId, DeviceId)

  • PCI_DEVICE_BCM5717 (0x14E4, 0x1655)

  • PCI_DEVICE_BCM571X (0x14E4, 0x1656)

  • PCI_DEVICE_BCM5719 (0x14E4, 0x1657)

  • PCI_DEVICE_BCM5720 (0x14E4, 0x1656)