5.7. Texas Instruments CPSW - emllCPSW
The parameters to the Real-time Ethernet Driver CPSW are setup-specific.
The function CreateLinkParmsFromCmdLineCPSW() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.
-
struct EC_T_LINK_PARMS_CPSW
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_CPSW.
-
EC_T_CPSW_TYPE eCpswType
CPSW type
-
EC_T_DWORD dwPhyAddr
PHY address
-
EC_T_DWORD dwPortPrio
0 (lowest), 1 (highest)
-
EC_T_BOOL bMaster
EC_TRUE: Initialize MAC
-
EC_T_BOOL bPhyRestartAutoNegotiation
EC_TRUE: Restart auto negotiation on initialization
-
EC_T_PHYINTERFACE ePhyInterface
PHY connection type
-
EC_T_DWORD dwRxInterrupt
Receive interrupt number (IRQ)
-
EC_T_BOOL bNotUseDmaBuffers
Use buffers from DMA (EC_FALSE) or from heap for receive. AllocSend is not supported, when EC_TRUE. EcLinkAllocSendFrame is not supported if bNotUseDmaBuffers = EC_TRUE.
-
EC_T_BOOL bNoPhyAccess
Don’t use MDIO to set up the PHY
-
EC_T_BOOL bAleBypass
Enable bAleBypass, similar to promiscuous mode
-
EC_T_DWORD dwExtendRxFrameLength
Receive longer Rx Frames
-
EC_T_LINK_PARMS linkParms
5.7.1. CPSW usage under Linux
Due to the lacking unbind-feature of the CPSW driver, the target’s Kernel must not load the CPSW driver when starting. If the CPSW was built as a module, it can be renamed or removed to ensure it never gets loaded. If it was compiled into the Kernel, the Kernel needs to be recompiled without it.
It is possible to use one CPSW port for Linux kernel (TCP/IP) and another CPSW port for EC-Simulator. To do this, the CPSW kernel driver must be patched.
Currently following Linux versions are supported:
linux-4.1.6 from TI Linux SDK 2.0
linux-4.4.4-rt11 from Lenze
linux-3.10.93-rt101 from Canon
Note
A patch for other Linux versions can also be created on request.
The patch needs:
Linux kernel with enabled CPSW driver.
Patch applied to Linux kernel.
EC_ETHERNET_PORT defined according to target in cpsw.c and davinci_mdio.c files.
Kernel must be rebuilt and installed
After that Linux will have only 1 Ethernet device, another can be used by EC-Simulator.
Note
EtherCAT® ports should be used as “slave” since “master” is the Linux driver.