5.1. Real-time Ethernet Driver initialization
The different Real-time Ethernet Driver modules are selected and parameterized by a Real-time Ethernet Driver specific structure.
The size of the Real-time Ethernet Driver parameter structure depends on the adapter type.
All Real-time Ethernet Driver parameter structures start with EC_T_LINK_PARMS followed by adapter type specific parameters.
The linkParms.dwSize must be set to sizeof(EC_T_LINK_PARMS_INTELGBE) or the used structure respectively. It may not be 0.
The following example shows how to pass Real-time Ethernet Driver parameters to emInitMaster():
/* master init parms */
EC_T_INIT_MASTER_PARMS oInitMasterParms;
OsMemset(&oInitMasterParms, 0, sizeof(EC_T_INIT_MASTER_PARMS));
/* simulator parms */
EC_T_LINK_PARMS_SIMULATOR oLinkParmsSimulator;
OsMemset(&oLinkParmsSimulator, 0, sizeof(EC_T_LINK_PARMS_SIMULATOR));
/* license Link Layer parms */
EC_T_LINK_PARMS_INTELGBE oLinkParmsIntelGbe;
OsMemset(&oLinkParmsIntelGbe, 0, sizeof(EC_T_LINK_PARMS_INTELGBE));
/* identify simulator Link Layer in the common structure */
oLinkParmsSimulator.linkParms.dwSignature = EC_LINK_PARMS_SIGNATURE_SIMULATOR;
oLinkParmsSimulator.linkParms.dwSize = sizeof(EC_T_LINK_PARMS_SIMULATOR);
OsSafeStrncpy(oLinkParmsSimulator.linkParms.szDriverIdent, EC_LINK_PARMS_IDENT_SIMULATOR, EC_DRIVER_IDENT_NAME_SIZE);
oLinkParmsSimulator.linkParms.dwInstance = dwSimulatorId;
oLinkParmsSimulator.linkParms.eLinkMode = EcLinkMode_POLLING;
/* specific simulator parameters should be set here */
/* oLinkParmsSimulator.pbyCnfData = ENI/EXI; */
/* identify license Link Layer in the common structure */
oLinkParmsIntelGbe.linkParms.dwSignature = EC_LINK_PARMS_SIGNATURE_INTELGBE;
oLinkParmsIntelGbe.linkParms.dwSize = sizeof(EC_T_LINK_PARMS_INTELGBE);
OsSafeStrncpy(oLinkParmsIntelGbe.linkParms.szDriverIdent, EC_LINK_PARMS_IDENT_INTELGBE, EC_DRIVER_IDENT_NAME_SIZE);
oLinkParmsIntelGbe.linkParms.dwInstance = 1; /* instance ID of the adapter */
oLinkParmsIntelGbe.linkParms.eLinkMode = EcLinkMode_POLLING;
/* specific Link Layer parameters should be set here */
/* oLinkParmsIntelGbe.wRxBufferCnt = 128; */
/* pass license Link Layer parameters to simulator Link Layer */
oLinkParmsSimulator.apLinkParms[0] = (EC_T_LINK_PARMS*)&oLinkParmsIntelGbe;
/* more parameters should be set here */
oInitMasterParms.dwSignature = ATECAT_SIGNATURE;
oInitMasterParms.dwSize = sizeof(EC_T_INIT_MASTER_PARMS);
/* pass simulator Link Layer to master init parms */
oInitMasterParms.pLinkParms = (EC_T_LINK_PARMS*)&oLinkParmsSimulator;
/* initialize master */
dwRes = emInitMaster(dwInstanceId, &oInitMasterParms);
-
struct EC_T_LINK_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Signature of the adapter specific structure containing the EC_T_LINK_PARMS structure
-
EC_T_DWORD dwSize
[in] Size of the adapter specific structure containing the EC_T_LINK_PARMS structure
-
EC_T_LOG_PARMS LogParms
[in] Logging parameters
-
EC_T_CHAR szDriverIdent[EC_DRIVER_IDENT_NAME_SIZE]
[in] Name of Link Layer module (driver identification) for Link Layer Selection
-
EC_T_DWORD dwInstance
[in] Instance of the adapter. If EC_LINKUNIT_PCILOCATION is set: contains PCI address.
-
EC_T_LINKMODE eLinkMode
[in] Mode of operation
-
EC_T_DWORD dwIstPriority
[in] Task priority of the interrupt service task (not used in polling mode)
-
EC_T_DWORD dwIstStackSize
[in] Task stack size
-
EC_T_DWORD dwLinkSpeed
[in] 10, 100, 1000 Mbit/s
-
EC_T_LINKLAYER_TIMINGTASK oLinkLayerTimingTask
[in] LinkLayer timimg task parameters
-
EC_T_CHAR szLoadPath[EC_DRIVER_PATH_SIZE]
[in] Path from which the libraries should be loaded
-
EC_T_DWORD dwSignature
-
struct EC_T_LINKLAYER_TIMINGTASK
Public Members
-
EC_T_LINKLAYER_TIMING eLinkLayerTiming
[in] LinkLayer timing task mode
-
EC_T_DWORD dwCycleTimeNsec
[in] Cycle time between 2 pfnStartCycle calls in ns. Will be set by the master stack for the link layer.
-
EC_T_LINK_STARTCYCLE_CALLBACK pfnStartCycle
[in] Callback function called cyclically according to dwCycleTimeNsec
-
EC_T_DWORD dwTtsSendOffsetUsec
[in] Time between pfnStartCycle call and TTS frame transmission
-
EC_T_UINT64 nSystemTime
[in] System
-
EC_T_LINKLAYER_TIMING eLinkLayerTiming
5.1.1. Real-time Ethernet Driver instance selection via PCI location
For some operating systems it is possible to address the Real-time Ethernet Driver instance using its PCI address as an alternative. To do this, EC_LINKUNIT_PCILOCATION (0x01000000) and the PCI location must be set as EC_T_LINK_PARMS::dwInstance.
On Linux the PCI address can be shown using e.g.:
$ lspci | grep Ethernet
$ 00:19.0 Ethernet controller: Intel Corporation Ethernet Connection I217-LM (rev 04)
$ 04:00.0 Ethernet controller: Intel Corporation 82574L Gigabit Network Connection
$ 05:00.0 Ethernet controller: Intel Corporation 82574L Gigabit Network Connection
The format of EC_T_LINK_PARMS::dwInstance using PCI bus address is:
- 0x01bbddff
bb Bus Number
dd Device Number
ff Function Number
EC_T_LINK_PARMS::dwInstance = 0x01001900; //"0000:00:19.0"
On Windows the integer value displayed in the properties dialog must be converted to HEX. E.g the number from the following dialog (PCI bus 11, device 0, function 0) corresponds to 0x010B0000 (bus 0x0B).