10. Example Guests
The example guests, located in /hv/guests/examples cannot be used in conjunction with the System Manager.
Furthermore, once you have stored a configuration using the System Manager, it is not possible to use the example guests anymore.
You may either use the example guests OR use guests configured by the System Manager.
If you have configured guests using the System Manager, you need to run the hv_resethv command to switch back to use the example guests. See also section Reset Hypervisor Initialization in the Hypervisor Manual.
Caution
After calling hv_resethv you may have to re-create the guests which are managed by the System Manager.