9. Hypervisor Host Control

It is possible to reboot or shutdown the Hypervisor Host from within the System Manager.

_images/SysMgrTgtControl.jpg

Rebooting is required in some cases, especially if the memory configuration is changed (when adding or removing RTOS guests). In some cases a regular reboot or shutdown is not possible (e.g. if guests are running), then you may use the (Force) option to ignore such restrictions.

You can determine whether a reboot is required by pressing the Refresh button in the Run mode.

_images/SysMgrRebootRequiredRefresh.jpg

If you try to start a guest while a reboot is required, the System Manager will throw an error message. Then you should reboot the system.

_images/SysMgrRebootRequired.jpg