5.1. Real-time Ethernet Driver initialization
The different Real-time Ethernet Driver modules are selected and parameterized by a Real-time Ethernet Driver specific structure. Each Real-time Ethernet Driver specific structure start with a common EC_T_LINK_PARMS structure, followed by some Real-time Ethernet Driver specific members. The common link parameter structure is passed to EC_T_INIT_MASTER_PARMS::pLinkParms with the call of emInitMaster() like in the following example:
/* identify Link Layer in the common struture */
oLinkParmsSockRaw.linkParms.dwSignature = EC_LINK_PARMS_SIGNATURE_SOCKRAW;
oLinkParmsSockRaw.linkParms.dwSize = sizeof(EC_T_LINK_PARMS_SOCKRAW);
OsStrncpy(&oLinkParmsSockRaw.linkParms.szDriverIdent, EC_LINK_PARMS_IDENT_SOCKRAW, EC_DRIVER_IDENT_MAXLEN);
/* specific Link Layer parameters should be set here */
/* pass Link Layer parameters */
oInitMasterParms.dwSignature = ATECAT_SIGNATURE;
oInitMasterParms.dwSize = sizeof(EC_T_INIT_MASTER_PARMS);
oInitMasterParms.pLinkParms = &oLinkParmsSockRaw.linkParms;
/* more parameters should be set here */
/* initialize master */
emInitMaster(dwInstanceId, &oInitMasterParms);
-
struct EC_T_LINK_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Signature of the adapter specific structure containing the EC_T_LINK_PARMS structure
-
EC_T_DWORD dwSize
[in] Size of the adapter specific structure containing the EC_T_LINK_PARMS structure
-
EC_T_LOG_PARMS LogParms
[in] Logging parameters
-
EC_T_CHAR szDriverIdent[EC_DRIVER_IDENT_NAMESIZE]
[in] Name of Link Layer module (driver identification) for Link Layer Selection
-
EC_T_DWORD dwInstance
[in] Instance of the adapter. if EC_LINKUNIT_PCILOCATION is set: contains PCI address
-
EC_T_LINKMODE eLinkMode
[in] Mode of operation
-
EC_T_DWORD dwIstPriority
[in] Task priority of the interrupt service task (not used in polling mode)
-
EC_T_LINKLAYER_TIMINGTASK oLinkLayerTimingTask
[in] LinkLayer timimg task parameters
-
EC_T_DWORD dwSignature
-
struct EC_T_LINKLAYER_TIMINGTASK
Public Members
-
EC_T_LINKLAYER_TIMING eLinkLayerTiming
[in] LinkLayer timing task mode
-
EC_T_DWORD dwCycleTimeUsec
[in] Cycle time between 2 pfnStartCycle calls in us. Will be set by the master stack for the linklayer.
-
EC_T_LINKLAYER_TIMING eLinkLayerTiming
5.1.1. Real-time Ethernet Driver instance selection via PCI location
For some operating systems it is possible to address the Real-time Ethernet Driver instance using its PCI address as an alternative. To do this, EC_LINKUNIT_PCILOCATION (0x01000000) and the PCI location must be set as EC_T_LINK_PARMS::dwInstance.
On Linux the PCI address can be shown using e.g.:
$ lspci | grep Ethernet
$ 00:19.0 Ethernet controller: Intel Corporation Ethernet Connection I217-LM (rev 04)
$ 04:00.0 Ethernet controller: Intel Corporation 82574L Gigabit Network Connection
$ 05:00.0 Ethernet controller: Intel Corporation 82574L Gigabit Network Connection
The format of EC_T_LINK_PARMS::dwInstance using PCI bus address is:
- 0x01bbddff
bb Bus Number
dd Device Number
ff Function Number
EC_T_LINK_PARMS::dwInstance = 0x01001900; //"0000:00:19.0"
On Windows the integer value displayed in properties dialog must be converted to HEX. E.g the number from the following dialog (PCI bus 11, device 0, function 0) corresponds to 0x010B0000 (bus 0x0B).