1. Introduction

1.1. What is EtherCAT?

EtherCAT® (Ethernet for Control Automation Technology) is a high-performance Ethernet Fieldbus technology that provides a reliable, efficient, and cost-effective communication solution for a wide variety of industrial automation applications. Originally developed as an open technology by Beckhoff Automation in 2003, and subsequently turned over to an independent organization known as the EtherCAT Technology Group, EtherCAT has since become one of the most widely used industrial Ethernet protocols in the world.

See also

A comprehensive introduction to EtherCAT technology can be found at https://www.acontis.com/en/what-is-ethercat-communication-protocol.html.

1.2. The EC-Master - Features

Feature ID: Unique identification used in ETG.1500 EtherCAT Master Classes

*1: According to ETG.1500 Master Classes not mandatory for Class A

*2: According to ETG.1500 Master Classes not mandatory for Class B

Feature name

Short description

Class A

Class B

Feature ID

Basic Features

Service Commands

Support of all commands

✅

✅

101

IRQ field in datagram

Use IRQ information from Slave in datagram header

✅

✅

102

Slaves with Device Emulation

Support Slaves with and without application controller

✅

✅

103

EtherCAT State Machine

Support of ESM special behavior

✅

✅

104

Error Handling

Checking of network or slave errors, e.g. Working Counter

✅

✅

105

VLAN

Support VLAN Tagging

– (*1)

– (*2)

106

EtherCAT Frame Types

Support EtherCAT Frames

✅

✅

107

UDP Frame Types

Support UDP Frames

– (*1)

– (*2)

108

Process Data Exchange

Cyclic PDO

Cyclic process data exchange

✅

✅

201

Multiple Tasks

Different cycle tasks Multiple update rates for PDO

✅

✅

202

Frame repetition

Send cyclic frames multiple times to increase immunity

– (*1)

– (*2)

203

Network Configuration

Online scanning

Network configuration functionality included in EtherCAT Master

✅

✅

301

Reading ENI

Network Configuration taken from ENI file

✅

✅

301

Compare Network configuration

Compare configured and existing network configuration during boot-up

✅

✅

302

Explicit Device identification

Identification used for Hot Connect and prevention against cable swapping

✅

✅

303

Station Alias Addressing

Support configured station alias in slave, i.e. enable 2nd Address and use it

✅

✅

304

Access to EEPROM

Support routines to access EEPROM via ESC register

✅

✅

305

Mailbox Support

Support Mailbox

Main functionality for mailbox transfer

✅

✅

401

Mailbox Resilient Layer

Support underlying resilient layer

✅

✅

402

Multiple Mailbox channels

✅

✅

403

Mailbox polling

Polling Mailbox state in slaves

✅

✅

404

CAN application layer over EtherCAT (CoE)

SDO Up/Download

Normal and expedited transfer

✅

✅

501

Segmented Transfer

Segmented transfer

✅

✅

502

Complete Access

Transfer the entire object (with all subindices) at once

✅

✅

503

SDO Info service

Services to read object dictionary

✅

✅

504

Emergency Message

Receive Emergency messages

✅

✅

505

PDO in CoE

PDO services transmitted via CoE

– (*1)

– (*2)

506

EoE

EoE protocol

Services for tunneling Ethernet frames. includes all specified EoE services

✅

✅

601

Virtual Switch

Virtual Switch functionality

✅

✅

602

EoE Endpoint to Operation Systems

Interface to the Operation System on top of the EoE layer

FP

– (*2)

603

FoE

FoE Protocol

Support FoE Protocol

✅

✅

701

Firmware Up-/Download

Password, FileName should be given by the application

✅

✅

702

Boot State

Support Boot-State for Firmware Up/Download

✅

✅

703

SoE

SoE Protocol

Support SoE Services

✅

✅

801

AoE

AoE Protocol

Support AoE Protocol

✅

✅

901

VoE

VoE Protocol

External Connectivity supported

✅

✅

1001

Synchronization with Distributed Clock (DC)

DC support

Support of Distributed Clocks

✅

– (*2)

1101

Continuous Propagation Delay compensation

Continuous Calculation of the propagation delay

✅

– (*2)

1102

Sync window monitoring

Continuous monitoring of the Synchronization difference in the slaves

✅

– (*2)

1103

Slave-to-Slave Communication

via Master

Information is given in ENI file or can be part of any other network configuration. Copying of the data can be handled by master stack or master’s application

✅

✅

1201

Master information

Master Object Dictionary

FP

– (*2)

1301

1.3. Protected version

The EC-Master software can be delivered in 3 different versions:

Protected

Binary with MAC protection

Unrestricted

Binary without MAC protection

Dongled

Encrypted binary

The protected version will automatically stop after about 1 hour of continuous operation. In order to remove this restriction a valid runtime license key is required. The runtime license protection is based on the MAC address of the Ethernet controller used for the EtherCAT protocol. With a valid License Key the protected version of EC-Master will automatically become an unrestricted version.

1.3.1. Licensing procedure for Development Licenses

  1. Installation of EC-Master protected version

  2. Determine the MAC Address by calling emGetSrcMacAddress() or from a sticker applied on the hardware near the Ethernet controller

  3. Send an Email with the subject “Development License Key Request, Commission your commission number” with the MAC address to sales@acontis.com

  4. Acontis will create the license keys and return them in a License Key Text File (CSV format).

    Number;MAC Address;License Key
    1;00-00-5A-11-77-FE;DA1099F2-15C249E9-54327FBC
    2;64-31-50-80-20-4E;1B7C1F86-D08E40A8-4F96F2BA
    3;2C-F0-5D-03-CB-2B;10005078-DFD9A2C3-5FD4B1CD-35041597-F8094AA4-6C7CCE7E
    
  5. Activate the License Key by calling emSetLicenseKey() with the license key that corresponds to the MAC address on the hardware and check the return code. The license key is 26 or 53 characters long.

    dwRes = emSetLicenseKey(0, "DA1099F2-15C249E9-54327FBC");
    

1.3.2. Licensing procedure for Runtime Licenses

  1. Installation of EC-Master protected version

  2. Determine the MAC Address by calling emGetSrcMacAddress() or from a sticker applied on the hardware near the Ethernet controller

  3. Provide the MAC Addresses and numbers from previously ordered and unused runtime license stickers in a text file to acontis as described in the example below. Please use a separate line for each runtime license sticker number and MAC Address.

    S/N; MAC Address
    100-105-1-1/1603310001;00-00-5A-11-77-FE
    100-105-1-1/1603310002;64-31-50-80-20-4E
    100-105-1-1/1603310003;2C-F0-5D-03-CB-2B
    
  4. Send an Email with the subject “Runtime License Key Request, Commission your commission number” with the MAC address to sales@acontis.com

  5. Acontis will create the license keys and return them in a License Key Text File.

    Number;MAC Address;License Key
    1;00-00-5A-11-77-FE;DA1099F2-15C249E9-54327FBC
    2;64-31-50-80-20-4E;1B7C1F86-D08E40A8-4F96F2BA
    3;2C-F0-5D-03-CB-2B;10005078-DFD9A2C3-5FD4B1CD-35041597-F8094AA4-6C7CCE7E
    
  6. Activate the License Key by calling emSetLicenseKey() with the license key that corresponds to the MAC address on the hardware and check the return code.

    dwRes = emSetLicenseKey(0, "DA1099F2-15C249E9-54327FBC");
    

1.4. Dongled version

The Master library is encrypted and requires a dongle to execute. The following dongles are supported:

  • USB dongle

  • ASIC dongle

  • Virtual dongle using a WibuCmRaU file

1.4.1. Licensing using a virtual WibuCmRaU File on Linux

To create a virtual dongle using a WibuCmRaU file on a Linux machine, the following steps are required:

  • Download the codemeter package from Wibu website and install it on the linux machine:

  • Import the LIF file provided by acontis
    cmu --import --file *.WibuCmLIF
    
  • List the Wibu licenses, to get the serial number
    cmu --list
    
  • Use the serial number to generate a WibuCmRaC file
    cmu --serial your_serial_number --context 6001978 --file *.WibuCmRaC
    
  • Send the WibuCmRaC to acontis and acontis will provide a WibuCmRaU file.

  • Import the WibuCmRaU file
    cmu --import --file *.WibuCmRaU
    

1.4.2. Maintain the license after a linux image update

In case of a complete Linux image update, the following steps are required:

  • Make a backup of the WibuCmRaU file and the following folder /var/lib/Codemeter/CmAct from the old image.

  • On the new image install Codemeter

  • Restore the 6001978_* files from /var/lib/Codemeter/CmAct

  • Change the user rights of the 4 files to daemon
    sudo chown daemon:daemon 6001978_*
    
  • Import the WibuCmRaU backup file
    cmu --import --file *.WibuCmRaU
    

1.5. License

1.5.1. EC-Master license

According to EC-Master Software License Agreement (SLA).

1.5.2. Free Open Source Software contained in EC-Master

1.5.2.1. Expat XML parser license V2.6.0

Copyright (c) 1997-2000 Thai Open Source Software Center Ltd
Copyright (c) 2000      Clark Cooper <coopercc@users.sourceforge.net>
Copyright (c) 2000-2005 Fred L. Drake, Jr. <fdrake@users.sourceforge.net>
Copyright (c) 2001-2002 Greg Stein <gstein@users.sourceforge.net>
Copyright (c) 2002-2016 Karl Waclawek <karl@waclawek.net>
Copyright (c) 2016-2024 Sebastian Pipping <sebastian@pipping.org>
Copyright (c) 2016      Cristian Rodríguez <crrodriguez@opensuse.org>
Copyright (c) 2016      Thomas Beutlich <tc@tbeu.de>
Copyright (c) 2017      Rhodri James <rhodri@wildebeest.org.uk>
Copyright (c) 2022      Thijs Schreijer <thijs@thijsschreijer.nl>
Copyright (c) 2023      Hanno Böck <hanno@gentoo.org>
Copyright (c) 2023      Sony Corporation / Snild Dolkow <snild@sony.com>
Licensed under the MIT license:

Permission is  hereby granted,  free of charge,  to any  person obtaining
a  copy  of  this  software   and  associated  documentation  files  (the
"Software"),  to  deal in  the  Software  without restriction,  including
without  limitation the  rights  to use,  copy,  modify, merge,  publish,
distribute, sublicense, and/or sell copies of the Software, and to permit
persons  to whom  the Software  is  furnished to  do so,  subject to  the
following conditions:

The above copyright  notice and this permission notice  shall be included
in all copies or substantial portions of the Software.

THE  SOFTWARE  IS  PROVIDED  "AS  IS",  WITHOUT  WARRANTY  OF  ANY  KIND,
EXPRESS  OR IMPLIED,  INCLUDING  BUT  NOT LIMITED  TO  THE WARRANTIES  OF
MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN
NO EVENT SHALL THE AUTHORS OR  COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM,
DAMAGES OR  OTHER LIABILITY, WHETHER  IN AN  ACTION OF CONTRACT,  TORT OR
OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE
USE OR OTHER DEALINGS IN THE SOFTWARE.

1.5.3. Free Open Source Software supported by EC-Master

The following components are not part of EC-Master, but relate to it:

1.5.3.1. acontis atemsys Linux kernel module

The acontis atemsys is licensed under the GPL:

Copyright (c) 2009 - 2020 acontis technologies GmbH, Ravensburg, Germany
All rights reserved.

This program is free software; you can redistribute  it and/or modify it
under  the terms of  the GNU General  Public License as published by the
Free Software Foundation;  either version 2 of the  License, or (at your
option) any later version.

1.5.3.2. WinPCap

The WinPCap library is supported, but not shipped with EC-Master.

1.5.3.3. Npcap

The Npcap library is supported, but not shipped with EC-Master.

1.6. Versioning

EC-Master follows the following versioning scheme: VMAJOR. MINOR. SERVICEPACK. BUILD (e.g. V3.2.1.04).

The libraries are binary compatible by unchanged MAJOR and MINOR digits. If SERVICEPACK increments, BUILD restarts with 01. BUILD 99 is reserved for test builds that have not been officially released for productive usage.