6.11. CAN application protocol over EtherCAT (CoE)
6.11.1. emCoeSdoDownload
-
static EC_T_DWORD ecatCoeSdoDownload(EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoDownload(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Execute a CoE SDO download to an EtherCAT slave device.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
wObIndex – [in] Object Index
byObSubIndex – [in] Object SubIndex. If Complete Access only 0 or 1 allowed.
pbyData – [in] Buffer containing transferred data. Must not be EC_NULL if dwDataLen > 0.
dwDataLen – [in] Buffer length [bytes]. Can be 0 for example for array.
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, pbyData is EC_NULL and dwDataLen > 0, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeSdoDownload Example
The following code demonstrates how to download a CoE object to a slave using the API emCoeSdoDownload().
EC_T_DWORD CoeSdoDownloadExample()
{
EC_T_DWORD dwRetVal = EC_E_ERROR;
EC_T_DWORD dwRes = EC_E_ERROR;
/* slave with station address 2002 used for CoE SDO download */
EC_T_DWORD dwSlaveId = ecatGetSlaveId(2002);
EC_T_BYTE abyBuf[4];
OsMemset(abyBuf, 0, sizeof(abyBuf));
/* download value 123 to object index 0x40A2, subindex 2, timeout 5s, no complete access */
EC_SET_FRM_DWORD(abyBuf, 123);
dwRes = ecatCoeSdoDownload(dwSlaveId, 0x40A2, 2, abyBuf, (EC_T_DWORD)sizeof(abyBuf), 5000, 0);
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
dwRetVal = EC_E_NOERROR;
Exit:
return dwRetVal;
}
See also
6.11.2. emCoeSdoDownloadReq
-
static EC_T_DWORD ecatCoeSdoDownloadReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoDownloadReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Initiates a CoE SDO download to an EtherCAT slave device and returns immediately.
The length of the data to be downloaded must be set in EC_T_MBXTFER.dwDataLen. A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object
dwSlaveId – [in] Slave ID
wObIndex – [in] Object Index
byObSubIndex – [in] Object SubIndex. If Complete Access only 0 or 1 allowed
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeSdoDownloadReq Example
The following code demonstrates how to download a CoE object to a slave using the non-blocking API emCoeSdoDownloadReq().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
EC_T_DWORD CoeSdoDownloadReqExample()
{
EC_T_DWORD dwRetVal = EC_E_ERROR;
EC_T_DWORD dwRes = EC_E_ERROR;
/* needed only for notifications, see
- ecatRegisterClient(...)
- pAppContext->pNotificationHandler->GetClientID() */
EC_T_DWORD dwClientId = 0;
/* slave with station address 2002 used for CoE SDO download */
EC_T_DWORD dwSlaveId = ecatGetSlaveId(2002);
EC_T_MBXTFER* pMbxTferObject = EC_NULL;
EC_T_BYTE abyBuf[4];
EC_T_MBXTFER_DESC oObjectDataTferDesc;
OsMemset(abyBuf, 0, sizeof(abyBuf));
OsMemset(&oObjectDataTferDesc, 0, sizeof(EC_T_MBXTFER_DESC));
/* create mailbox transfer object */
oObjectDataTferDesc.pbyMbxTferDescData = abyBuf;
oObjectDataTferDesc.dwMaxDataLen = sizeof(abyBuf);
pMbxTferObject = ecatMbxTferCreate(&oObjectDataTferDesc);
if (EC_NULL == pMbxTferObject)
{
dwRes = EC_E_NOMEMORY;
dwRetVal = dwRes;
goto Exit;
}
/* create mailbox transfer object */
pMbxTferObject->dwClntId = dwClientId;
pMbxTferObject->dwTferId = 1; /* assigned by application. should be unique for each object */
/* request download of value 123 to object index 0x40A2, subindex 2, timeout 5s, no complete access */
EC_SET_FRM_DWORD(abyBuf, 123);
dwRes = ecatCoeSdoDownloadReq(pMbxTferObject, dwSlaveId, 0x40A2, 2, 5000, 0);
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
/* wait for transfer finished */
while (eMbxTferStatus_Pend == pMbxTferObject->eTferStatus)
{
OsSleep(10);
}
/* check transfer result */
dwRes = pMbxTferObject->dwErrorCode;
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
dwRetVal = EC_E_NOERROR;
Exit:
if (EC_NULL != pMbxTferObject)
{
pMbxTferObject->eTferStatus = eMbxTferStatus_Idle;
ecatMbxTferDelete(pMbxTferObject);
}
return dwRetVal;
}
6.11.3. emNotify - eMbxTferType_COE_SDO_DOWNLOAD
SDO download transfer completion.
- emNotify - eMbxTferType_COE_SDO_DOWNLOAD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, this structure contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The request parameters stored in element EC_T_MBX_DATA::CoE of type EC_T_MBX_DATA_COE are part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
6.11.4. emCoeSdoUpload
-
static EC_T_DWORD ecatCoeSdoUpload(EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD *pdwOutDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoUpload(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD *pdwOutDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Execute a CoE SDO upload from an EtherCAT slave device to the master.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index
byObSubIndex – [in] Object SubIndex. If Complete Access only 0 or 1 allowed
pbyData – [out] Buffer receiving transferred data
dwDataLen – [in] Buffer length in bytes
pdwOutDataLen – [out] Length of received data in bytes
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeSdoUpload Example
The following code demonstrates how to upload a CoE object from a slave using the API emCoeSdoUpload().
EC_T_DWORD CoeSdoUploadExample()
{
EC_T_DWORD dwRetVal = EC_E_ERROR;
EC_T_DWORD dwRes = EC_E_ERROR;
/* slave with station address 2002 used for CoE SDO upload */
EC_T_DWORD dwSlaveId = ecatGetSlaveId(2002);
EC_T_BYTE abyBuf[4];
OsMemset(abyBuf, 0, sizeof(abyBuf));
/* upload object index 0x1018, subindex 1, timeout 5s, no complete access */
dwRes = ecatCoeSdoUpload(dwSlaveId, 0x1018, 1, abyBuf, (EC_T_DWORD)sizeof(abyBuf), EC_NULL, 5000, 0);
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
dwRetVal = EC_E_NOERROR;
Exit:
return dwRetVal;
}
See also
6.11.5. emCoeSdoUploadReq
-
static EC_T_DWORD ecatCoeSdoUploadReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoUploadReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Initiates a CoE SDO upload from an EtherCAT slave device to the master and returns immediately.
The length of the data to be uploaded must be set in EC_T_MBXTFER.dwDataLen. A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object created with emMbxTferCreate
dwSlaveId – [in] Slave ID
wObIndex – [in] Object Index
byObSubIndex – [in] Object SubIndex. If Complete Access only 0 or 1 allowed
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeSdoUploadReq Example
The following code demonstrates how to upload a CoE object from a slave using the non-blocking API emCoeSdoUploadReq().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
EC_T_DWORD CoeSdoUploadReqExample()
{
EC_T_DWORD dwRetVal = EC_E_ERROR;
EC_T_DWORD dwRes = EC_E_ERROR;
/* needed only for notifications, see
- ecatRegisterClient(...)
- pAppContext->pNotificationHandler->GetClientID() */
EC_T_DWORD dwClientId = 0;
/* slave with station address 2002 used for CoE SDO upload */
EC_T_DWORD dwSlaveId = ecatGetSlaveId(2002);
EC_T_MBXTFER* pMbxTferObject = EC_NULL;
EC_T_BYTE abyBuf[4];
EC_T_MBXTFER_DESC oObjectDataTferDesc;
OsMemset(abyBuf, 0, sizeof(abyBuf));
OsMemset(&oObjectDataTferDesc, 0, sizeof(EC_T_MBXTFER_DESC));
/* create mailbox transfer object */
oObjectDataTferDesc.pbyMbxTferDescData = abyBuf;
oObjectDataTferDesc.dwMaxDataLen = sizeof(abyBuf);
pMbxTferObject = ecatMbxTferCreate(&oObjectDataTferDesc);
if (EC_NULL == pMbxTferObject)
{
dwRes = EC_E_NOMEMORY;
dwRetVal = dwRes;
goto Exit;
}
/* create mailbox transfer object */
pMbxTferObject->dwClntId = dwClientId;
pMbxTferObject->dwTferId = 1; /* assigned by application. should be unique for each object */
/* request upload of object index 0x1018, subindex 1, timeout 5s, no complete access */
dwRes = ecatCoeSdoUploadReq(pMbxTferObject, dwSlaveId, 0x1018, 1, 5000, 0);
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
/* wait for transfer finished */
while (eMbxTferStatus_Pend == pMbxTferObject->eTferStatus)
{
OsSleep(10);
/* transfer can be canceled using ecatMbxTferAbort(...) if it takes too long */
}
/* check transfer result */
dwRes = pMbxTferObject->dwErrorCode;
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
dwRetVal = EC_E_NOERROR;
Exit:
if (EC_NULL != pMbxTferObject)
{
pMbxTferObject->eTferStatus = eMbxTferStatus_Idle;
ecatMbxTferDelete(pMbxTferObject);
}
return dwRetVal;
}
6.11.6. emNotify - eMbxTferType_COE_SDO_UPLOAD
SDO upload transfer completion.
- emNotify - eMbxTferType_COE_SDO_UPLOAD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The request parameters stored in element EC_T_MBX_DATA::CoE of type EC_T_MBX_DATA_COE are part of EC_T_MBXTFER::MbxData.
The SDO data stored in EC_T_MBXTFER::pbyMbxTferData may have to be buffered by the client.
Access to the memory area referenced by EC_T_MBXTFER::pbyMbxTferData outside of the notification caller context is illegal and the results are undefined.
6.11.7. emCoeGetODListReq
-
static EC_T_DWORD ecatCoeGetODListReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_COE_ODLIST_TYPE eListType, EC_T_DWORD dwTimeout)
-
EC_T_DWORD emCoeGetODListReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_COE_ODLIST_TYPE eListType, EC_T_DWORD dwTimeout)
Gets a list of object IDs that are available in a slave.
A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion.
This function may not be called from within the JobTask’s context.
Note
The mailbox transfer object will receive the slave response containing the list type followed by the list itself. Therefore the buffer must be 2 bytes bigger than the expected list size.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer
dwSlaveId – [in] Slave ID
eListType – [in] which object types shall be transferred
dwTimeout – [in] Timeout [ms]. The function will block at most for this time. If the timeout value is set to EC_NOWAIT the function will return immediately.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeGetODListReq Example
The following code demonstrates how to get the list of objects that are available in a slave using the non-blocking API emCoeGetODListReq().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
EC_T_MBXTFER* pMbxTfer = EC_NULL;
EC_T_MBXTFER_DESC oMbxTferDesc;
OsMemset(&oMbxTferDesc, 0, sizeof(EC_T_MBXTFER_DESC));
oMbxTferDesc.dwMaxDataLen = CROD_ODLTFER_SIZE;
/* allocate payload memory */
oMbxTferDesc.pbyMbxTferDescData = (EC_T_BYTE*)OsMalloc(oMbxTferDesc.dwMaxDataLen);
if (EC_NULL == oMbxTferDesc.pbyMbxTferDescData)
{
dwRetVal = EC_E_NOMEMORY;
goto Exit;
}
/* create mailbox transfer object */
pMbxTfer = emMbxTferCreate(dwInstanceId, &oMbxTferDesc);
if (EC_NULL == pMbxTfer)
{
dwRetVal = EC_E_NOMEMORY;
goto Exit;
}
dwRes = emCoeGetODListReq(dwInstanceId, pMbxTfer, dwSlaveId, eODListType_ALL, 5000 /* timeout */);
if (dwRes != EC_E_NOERROR)
{
dwRetVal = dwRes;
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "emCoeGetODList: %s (0x%lx))\n", ecatGetText(dwRes), dwRes));
goto Exit;
}
/* wait for transfer finished, see also emMbxTferAbort(...) */
while (eMbxTferStatus_Pend == pMbxTfer->eTferStatus)
{
OsSleep(10);
}
dwRetVal = pMbxTfer->dwErrorCode;
Exit:
if (EC_NULL != pMbxTfer)
{
if (eMbxTferStatus_Pend == pMbxTfer->eTferStatus)
{
emMbxTferAbort(dwInstanceId, pMbxTfer);
}
emMbxTferDelete(dwInstanceId, pMbxTfer);
}
SafeOsFree(oMbxTferDesc.pbyMbxTferDescData);
See also
See
CoeReadObjectDictionary()in EcSdoServices.cpp as an example foremCoeGetODListReq().
6.11.8. emNotify - eMbxTferType_COE_GETODLIST
Object dictionary list upload transfer completion.
- emNotify - eMbxTferType_COE_GETODLIST
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The object list stored in element EC_T_MBX_DATA::CoE_ODList of type EC_T_COE_ODLIST is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
-
struct EC_T_COE_ODLIST
Public Members
-
EC_T_COE_ODLIST_TYPE eOdListType
list type
-
EC_T_COE_ODLIST_TYPE eOdListType
6.11.9. emCoeGetObjectDescReq
-
static EC_T_DWORD ecatCoeGetObjectDescReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_DWORD dwTimeout)
-
EC_T_DWORD emCoeGetObjectDescReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_DWORD dwTimeout)
Determines the description of a specific object.
A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion. This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index
dwTimeout – [in] Timeout [ms]. The function will block at most for this time. If the timeout value is set to EC_NOWAIT the function will return immediately.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeGetObjectDescReq Example
The following code demonstrates how to determine the description of a specific object using the non-blocking API emCoeGetObjectDescReq().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
EC_T_MBXTFER* pMbxTfer = EC_NULL;
EC_T_MBXTFER_DESC oMbxTferDesc; /* mailbox transfer descriptor */
OsMemset(&oMbxTferDesc, 0, sizeof(EC_T_MBXTFER_DESC));
oMbxTferDesc.dwMaxDataLen = CROD_OBDESC_SIZE;
/* allocate payload memory */
oMbxTferDesc.pbyMbxTferDescData = (EC_T_BYTE*)OsMalloc(oMbxTferDesc.dwMaxDataLen);
if (EC_NULL == oMbxTferDesc.pbyMbxTferDescData)
{
dwRetVal = EC_E_NOMEMORY;
goto Exit;
}
/* create mailbox transfer object */
pMbxTfer = emMbxTferCreate(dwInstanceId, &oMbxTferDesc);
if (EC_NULL == pMbxTfer)
{
dwRetVal = EC_E_NOMEMORY;
goto Exit;
}
dwRes = emCoeGetObjectDescReq(dwInstanceId, pMbxTfer, dwSlaveId, 0x6411, 5000);
if (dwRes != EC_E_NOERROR)
{
dwRetVal = dwRes;
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "emCoeGetObjectDescReq: %s (0x%lx))\n", ecatGetText(dwRes), dwRes));
goto Exit;
}
/* wait for transfer finished, see also emMbxTferAbort(...) */
while (eMbxTferStatus_Pend == pMbxTfer->eTferStatus)
{
OsSleep(10);
}
dwRetVal = pMbxTfer->dwErrorCode;
Exit:
if (EC_NULL != pMbxTfer)
{
if (eMbxTferStatus_Pend == pMbxTfer->eTferStatus)
{
emMbxTferAbort(dwInstanceId, pMbxTfer);
}
emMbxTferDelete(dwInstanceId, pMbxTfer);
}
SafeOsFree(oMbxTferDesc.pbyMbxTferDescData);
See also
See
CoeReadObjectDictionary()in EcSdoServices.cpp as an example foremCoeGetObjectDescReq().
6.11.10. emNotify - eMbxTferType_COE_GETOBDESC
Completion of a SDO information service transfer to get a object description.
- emNotify - eMbxTferType_COE_GETOBDESC
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The object description stored in element EC_T_MBX_DATA::CoE_ObDesc of type EC_T_COE_OBDESC is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
See also
A more detailed description of the values for data type, object code etc. can be found in the EtherCAT specification ETG.1000, section 5.
6.11.11. emCoeGetEntryDescReq
-
static EC_T_DWORD ecatCoeGetEntryDescReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE byValueInfo, EC_T_DWORD dwTimeout)
-
EC_T_DWORD emCoeGetEntryDescReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE byValueInfo, EC_T_DWORD dwTimeout)
Determines the description of a specific object entry.
A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion. This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object
dwSlaveId – [in] Slave ID
wObIndex – [in] Object Index
byObSubIndex – [in] Object SubIndex
byValueInfo – [in] The value info bit mask includes which elements shall be in the response. See Value info flags for available values.
dwTimeout – [in] Timeout [ms]. The function will block at most for this time. If the timeout value is set to EC_NOWAIT the function will return immediately
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
emCoeGetEntryDescReq Example
The following code demonstrates how to get the description of a specific object entry using the non-blocking API emCoeGetEntryDescReq().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
EC_T_MBXTFER* pMbxTfer = EC_NULL;
EC_T_MBXTFER_DESC oMbxTferDesc; /* mailbox transfer descriptor */
OsMemset(&oMbxTferDesc, 0, sizeof(EC_T_MBXTFER_DESC));
oMbxTferDesc.dwMaxDataLen = CROD_ENTRYDESC_SIZE;
oMbxTferDesc.pbyMbxTferDescData = (EC_T_BYTE*)OsMalloc(oMbxTferDesc.dwMaxDataLen);
/* allocate payload memory */
if (EC_NULL == oMbxTferDesc.pbyMbxTferDescData)
{
dwRetVal = EC_E_NOMEMORY;
goto Exit;
}
/* create transfer object */
pMbxTfer = emMbxTferCreate(dwInstanceId, &oMbxTferDesc);
if (EC_NULL == pMbxTfer)
{
dwRetVal = EC_E_NOMEMORY;
goto Exit;
}
dwRes = emCoeGetEntryDescReq(dwInstanceId, pMbxTfer, dwSlaveId, 0x6411, 1, 0, 5000);
if (dwRes != EC_E_NOERROR)
{
dwRetVal = dwRes;
goto Exit;
}
/* wait for transfer finished, see also emMbxTferAbort(...) */
while (eMbxTferStatus_Pend == pMbxTfer->eTferStatus)
{
OsSleep(10);
}
dwRetVal = pMbxTfer->dwErrorCode;
Exit:
if (EC_NULL != pMbxTfer)
{
if (eMbxTferStatus_Pend == pMbxTfer->eTferStatus)
{
emMbxTferAbort(dwInstanceId, pMbxTfer);
}
emMbxTferDelete(dwInstanceId, pMbxTfer);
}
SafeOsFree(oMbxTferDesc.pbyMbxTferDescData);
Value info flags
See also
See
CoeReadObjectDictionary()in EcSdoServices.cpp as an example foremCoeGetEntryDescReq().
6.11.12. emNotify - eMbxTferType_COE_GETENTRYDESC
Completion of a SDO information service transfer to get a object entry description.
- emNotify - eMbxTferType_COE_GETENTRYDESC
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The object entry description stored in element EC_T_MBX_DATA::CoE_EntryDesc of type EC_T_COE_ENTRYDESC is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
-
struct EC_T_COE_ENTRYDESC
Public Members
-
EC_T_BYTE byValueInfo
Bit mask which information is included in pbyData. See Value info flags
-
EC_T_BYTE byObAccess
Access rights. See Object access flags
-
EC_T_BYTE byValueInfo
Object access flags
See also
An example for the evaluation of
EC_T_COE_ENTRYDESC::pbyDatacomes with EcMasterDemo.A more detailed description of the values can be found in the EtherCAT specification ETG.1000, section 5 and 6.
6.11.13. emCoeProfileGetChannelInfo
-
static EC_T_DWORD ecatCoeProfileGetChannelInfo(EC_T_BOOL bStationAddress, EC_T_WORD wSlaveAddress, EC_T_DWORD dwChannel, EC_T_PROFILE_CHANNEL_INFO *pInfo)
-
EC_T_DWORD emCoeProfileGetChannelInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_DWORD dwChannel, EC_T_PROFILE_CHANNEL_INFO *pInfo)
Return information about a configured CoE profile channel from the ENI file.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
dwChannel – [in] Channel
pInfo – [out] Channel info
- Returns:
EC_E_NOERROR or error code
emCoeProfileGetChannelInfo Example
The following code demonstrates how to return information about a configured CoE profile channel from the ENI file using the non-blocking API emCoeProfileGetChannelInfo().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
/* get information about CoE profile channel configured in ENI */
EC_T_PROFILE_CHANNEL_INFO oInfo;
dwRes = emCoeProfileGetChannelInfo(dwInstanceId, EC_TRUE, wSlaveAddress, 0, &oInfo);
6.11.14. emNotify - EC_NOTIFY_COE_INIT_CMD
Indicates a COE mailbox transfer completion during slave state transition. This notification is disabled by default.
- emNotify - EC_NOTIFY_COE_INIT_CMD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The EC_T_MBX_DATA::CoE_InitCmd element of type EC_T_MBX_DATA_COE_INITCMD is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
-
struct EC_T_MBX_DATA_COE_INITCMD
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_SLAVE_PROP SlaveProp
6.11.15. CoE Emergency (emNotify - eMbxTferType_COE_EMERGENCY)
Indication of a CoE emergency request. A emNotify - EC_NOTIFY_MBOXRCV is given with EC_T_MBXTFER::eMbxTferType = EC_T_MBXTFER_TYPE::eMbxTferType_COE_EMERGENCY.
- emNotify - eMbxTferType_COE_EMERGENCY
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
In case of an emergency notification all registered clients will get this notification.
The corresponding mailbox transfer object will be created inside the EtherCAT master. The content in EC_T_MBXTFER::dwTferId is undefined as it is not needed by the client and the master.
The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The emergency data stored in element EC_T_MBX_DATA::CoE_Emergency of type EC_T_COE_EMERGENCY is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
CoE Emergency Example
/* send CoE Emergency */
EC_T_BYTE abyEmergencyData[6] = { 0x01, 0x02, 0x03, 0x04, 0x05, 0x06 };
dwRes = esSendSlaveCoeEmergency(dwSimulatorId, wSlaveAddress, 0x1234 /* code */, abyEmergencyData, 6 /* data length */);
if (dwRes != EC_E_NOERROR)
{
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "esSendSlaveCoeEmergency failed: %s (0x%lx))\n", esGetText(dwSimulatorId, dwRes), dwRes));
goto Exit;
}
See also
A more detailed description of the values can be found in the EtherCAT specification ETG.1000, section 5.
6.11.16. CoE Abort (emNotify - EC_NOTIFY_MBSLAVE_COE_SDO_ABORT)
The application can abort asynchronous CoE Uploads and Downloads.
The slave may abort CoE Uploads and Downloads which is indicated at the return code of emCoeSdoUpload(), … .
This notification is given if an SDO transfer aborts while sending init commands.
- emNotify - EC_NOTIFY_MBSLAVE_COE_SDO_ABORT
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
Detailed error information is stored in structure EC_T_MBOX_SDO_ABORT_DESC of the union element SdoAbortDesc.
-
struct EC_T_MBOX_SDO_ABORT_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_SLAVE_PROP SlaveProp
See also
6.11.17. emConvertEcErrorToCoeError
-
EC_T_DWORD emConvertEcErrorToCoeError(EC_T_DWORD dwInstanceID, EC_T_DWORD dwErrorCode)
Convert master error code to CoE error code.
- Returns:
CoE error code according to the following specifications:
CoE Abort Codes defined in ETG.1000.6 V1.0.4, Table 41: SDO Abort Codes
Additional codes defined in ETG.1020, V1.2.0, Table 21: CoE Abort Codes (extension)
emConvertEcErrorToCoeError Example
The following code demonstrates how to convert master error code to CoE error code using the non-blocking API emConvertEcErrorToCoeError().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
dwCoeError = emConvertEcErrorToCoeError(dwInstanceId, EC_E_NOERROR);