6.16. EtherCAT Bus Scan
The acontis EtherCAT Master stack supports scanning the EtherCAT Bus to determine which devices are available. If a configuration was provided the connected slaves are validated against the given ENI.
See also
6.16.1. emIoControl - EC_IOCTL_SB_ENABLE
Enables Busscan support.
- emIoControl - EC_IOCTL_SB_ENABLE
- Parameter
pbyInBuf: [in] Pointer to Timeout Parameter Value in MSec (EC_T_DWORD). Timeout Parameter is used for timeout during Bus Topology determination.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
The Scanbus support is enabled by default.
6.16.2. emIoControl - EC_IOCTL_SB_RESTART
This call will restart the bus scanning cycle. On completion the Notfication emNotify - EC_NOTIFY_SB_STATUS is given.
- emIoControl - EC_IOCTL_SB_RESTART
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
The timeout value given by emIoControl - EC_IOCTL_SB_ENABLE will be used.
This function may be called prior to running emConfigureNetwork(). In such a case a first bus scan will be executed before master configuration. This feature may be used to dynamically create or adjust the XML configuration file. When issuing this IoControl, the application has to take care emExecJob() is called cyclically to trigger master state machines, timers, send acyc and receive frames accordingly.
6.16.3. emIoControl - EC_IOCTL_SB_STATUS_GET
This call will get the status of the last bus scan.
- emIoControl - EC_IOCTL_SB_STATUS_GET
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_SB_STATUS_NTFY_DESC.dwOutBufSize: [in] Size of the output buffer in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Return
EC_E_NOERROR or error code
See also
6.16.4. emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAY
This call will set the topology changed delay value. The master will wait this duration in msec to react on appearing links in topology. The default value is 1000 ms.
- emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAY
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD containing the delay information in msecdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
6.16.5. emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAYS
This call will set the topology changed delay values individually. The master will wait individual durations in msec (0 msec: disabled) for slave ports, main link and red link to react on appearing links in topology. The default value is 1000 ms.
- emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAYS
- Parameter
pbyInBuf: [in] Pointer to EC_T_TOPOLOGY_CHANGED_DELAYS containing the delay information in msecdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
6.16.6. emIoControl - EC_IOCTL_SB_SET_ERROR_ON_CROSSED_LINES
This call will enable or disable bus mismatch if IN and OUT connectors are swapped. If enabled the swapped IN and OUT connectors will lead to bus mismatch. By default swapped IN and OUT connectors will lead to bus mismatch.
- emIoControl - EC_IOCTL_SB_SET_ERROR_ON_CROSSED_LINES
- Parameter
pbyInBuf: [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE swapped IN and OUT connectors will lead to bus mismatch, if set to EC_FALSE swapped IN and OUT connectors are tolerated.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
6.16.7. emIoControl - EC_IOCTL_SB_SET_ERROR_ON_LINEBREAK
This call will enable or disable bus mismatch if a line is broken in a redundant network. If enabled, line breaks in cable or junction redundant networks will lead to bus mismatch.
- emIoControl - EC_IOCTL_SB_SET_ERROR_ON_LINEBREAK
- Parameter
pbyInBuf: [in] Pointer to EC_T_BOOL. EC_TRUE: Return error code, EC_FALSE: Return no error.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
Default: No error on line break.
Error codes:
EC_E_REDLINEBREAK: Line break in a cable redundant network.EC_E_JUNCTION_RED_LINE_BREAK: Line break in a junction redundant network.
6.16.8. emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGE_AUTO_MODE
Warning
This documentation is preliminary and is subject to change
This call will enable or disable the automatical topology change mode. By default the automatical mode is enabled.
- emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGE_AUTO_MODE
- Parameter
pbyInBuf: [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE the automatical mode is enabled.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
In automatical mode, new slaves will be discovered automatically. In manual mode, after new slaves have been connected, a emNotify - EC_NOTIFY_HC_TOPOCHGDONE notification will be given without opening the ports of the slaves on bus. When the application is able to handle the new slaves, it should call emIoControl - EC_IOCTL_SB_ACCEPT_TOPOLOGY_CHANGE
6.16.9. emIoControl - EC_IOCTL_SB_ACCEPT_TOPOLOGY_CHANGE
Warning
This documentation is preliminary and is subject to change
This call will trigger a scan bus. On completion the Notfication emNotify - EC_NOTIFY_SB_STATUS is given.
- emIoControl - EC_IOCTL_SB_ACCEPT_TOPOLOGY_CHANGE
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
This function may be called after a emNotify - EC_NOTIFY_HC_TOPOCHGDONE notification was given if the automatical topology change mode was previously disabled using emIoControl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGE_AUTO_MODE.
During this scan bus the ports of the slaves will be (re)open and new slaves can be detected.
The timeout value given by emIoControl - EC_IOCTL_SB_ENABLE will be used. When issuing this IoControl, the application has to take care emExecJob() is called cyclically to trigger master state machines, timers, send acyc and receive frames accordingly.
6.16.10. emNotify - EC_NOTIFY_SB_STATUS
Scan bus status notification.
This notification is enabled by default.
- emNotify - EC_NOTIFY_SB_STATUS
- Parameter
pbyInBuf: [in] Pointer to EC_T_SB_STATUS_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
See also
emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED for how to control the deactivation
6.16.11. emNotify - EC_NOTIFY_SB_MISMATCH
This notification will be initiated if scan bus detects mismatch of connected slaves and configuration, due to unexpected slaves or missing mandatory slaves.
- emNotify - EC_NOTIFY_SB_MISMATCH
- Parameter
pbyInBuf: [in] Pointer to EC_T_SB_MISMATCH_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
This notification is enabled by default. In case of permanent frame loss no slaves can be found although the slaves are connected.
See also
emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED for how to control the deactivation
6.16.12. emNotify - EC_NOTIFY_SB_DUPLICATE_HC_NODE
Scan bus mismatch was detected while scan because of a duplicated slave(s). An application get this notification if the there are two slaves on the network with the same product code, vendor ID and identification value (alias address or switch id).
- emNotify - EC_NOTIFY_SB_DUPLICATE_HC_NODE
- Parameter
pbyInBuf: [in] Pointer to EC_T_SB_MISMATCH_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The members of EC_T_SB_MISMATCH_DESC have the following meaning:
EC_T_SB_MISMATCH_DESC::wCfgFixedAddressDuplicated slave (config) station AddressEC_T_SB_MISMATCH_DESC::wCfgAIncAddressDuplicated slave (config) Auto-Increment Address.EC_T_SB_MISMATCH_DESC::dwCfgVendorIdDuplicated slave (config) Vendor IDEC_T_SB_MISMATCH_DESC::dwCfgProdCodeDuplicated slave (config) Product codeEC_T_SB_MISMATCH_DESC::dwCfgRevisionNoDuplicated slave (config) Revision NumberEC_T_SB_MISMATCH_DESC::dwCfgSerialNoDuplicated slave (config) Serial Number
6.16.13. emNotify - EC_NOTIFY_SLAVE_PRESENCE
This notification is given, if slave appears or disappears from the network.
This notification is enabled by default.
- emNotify - EC_NOTIFY_SLAVE_PRESENCE
- Parameter
pbyInBuf: [in] Pointer to EC_T_SLAVE_PRESENCE_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
Disconnecting the slave from the network, powering it off or a bad connection can produce this notification.
See also
emIoControl - EC_IOCTL_SET_NOTIFICATION_ENABLED for how to control the deactivation
6.16.14. emNotify - EC_NOTIFY_SLAVES_PRESENCE
This notification collects notifications of the type emNotify - EC_NOTIFY_SLAVE_PRESENCE Notification is given either upon completion or when master status is changed, whichever comes first. Disconnecting slaves from the network, turning them off, or having a bad connection can lead to this notification.
This notification is disabled by default.
- emNotify - EC_NOTIFY_SLAVES_PRESENCE
- Parameter
pbyInBuf: [in] Pointer to EC_T_SLAVES_PRESENCE_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_SLAVES_PRESENCE_NTFY_DESC
Public Members
-
EC_T_SLAVE_PRESENCE_NTFY_DESC SlavePresence[MAX_SLAVES_PRESENCE_NTFY_ENTRIES]
slave presence descriptions
-
EC_T_SLAVE_PRESENCE_NTFY_DESC SlavePresence[MAX_SLAVES_PRESENCE_NTFY_ENTRIES]
6.16.15. emNotify - EC_NOTIFY_LINE_CROSSED
Cable swapping detected. All slaves’ port 0 must lead to Master.
- emNotify - EC_NOTIFY_LINE_CROSSED
- Parameter
pbyInBuf: [in] Pointer to EC_T_LINE_CROSSED_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_LINE_CROSSED_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
slave properties
-
EC_T_SLAVE_PROP SlaveProp
6.16.16. emNotify - EC_NOTIFY_SLAVE_NOTSUPPORTED
Is currently generated during Bus Scan if emConfigureNetwork() (GenOp/Preop) and a wrong category type is detected in the EEPROM. This notification should only print a log message or be ignored (Master print log message itself).
- emNotify - EC_NOTIFY_SLAVE_NOTSUPPORTED
- Parameter
pbyInBuf: [in] Pointer to EC_T_ERROR_NOTIFICATION_DESC containing EC_T_SLAVE_NOTSUPPORTED_DESC.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_SLAVE_NOTSUPPORTED_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_SLAVE_PROP SlaveProp
6.16.17. emNotify - EC_NOTIFY_FRAMELOSS_AFTER_SLAVE
Is currently generated and automatically handled during emRescueScan() if opening port destroys communication (frameloss). This notification should only print a log message or be ignored.
- emNotify - EC_NOTIFY_FRAMELOSS_AFTER_SLAVE
- Parameter
pbyInBuf: [in] Pointer to EC_T_ERROR_NOTIFICATION_DESC containing EC_T_FRAMELOSS_AFTER_SLAVE_NTFY_DESC.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
6.16.18. emNotify - Bus Scan notifications for Feature Packs
The notifications EC_NOTIFY_RED_LINEBRK, EC_NOTIFY_RED_LINEFIXED belong to the Feature Pack Redundancy.
The notifications EC_NOTIFY_HC_DETECTADDGROUPS, EC_NOTIFY_HC_PROBEALLGROUPS belong to the Feature Pack Hot Connect.
6.16.19. emIoControl - EC_IOCTL_SB_NOTIFY_UNEXPECTED_BUS_SLAVES
Specifies if unexpected bus slaves must be notified as bus mismatch.
- emIoControl - EC_IOCTL_SB_NOTIFY_UNEXPECTED_BUS_SLAVES
- Parameter
pbyInBuf: [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE unexpected bus slaves on the network will be notified by EC_NOTIFY_SB_MISMATCH.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
6.16.20. emIsTopologyChangeDetected
-
EC_T_DWORD emIsTopologyChangeDetected(EC_T_DWORD dwInstanceID, EC_T_BOOL *pbTopologyChangeDetected)
Returns whether topology change detected.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pbTopologyChangeDetected – [out] Pointer to EC_T_BOOL value: EC_TRUE if Topology Change Detected, EC_FALSE if not.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
6.16.21. emNotify - EC_NOTIFY_HC_TOPOCHGDONE
This notification is raised when topology change has completely processed.
- emNotify - EC_NOTIFY_HC_TOPOCHGDONE
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD (EC_E_NOERROR on success, Error code otherwise)dwInBufSize: [in] sizeof(EC_T_DWORD).pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The notification is raised when the slaves have been detected and DC initialized.
6.16.22. emIoControl - EC_IOCTL_SB_SET_NO_DC_SLAVES_AFTER_JUNCTION
Declares that no DC slaves are located after junction
- emIoControl - EC_IOCTL_SB_SET_NO_DC_SLAVES_AFTER_JUNCTION
- Parameter
pbyInBuf: [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE the hidden slave detection and the junction redundancy specific propagation delay measurement are not executeddwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
- Return
EC_E_NOERROR or error code
Calling this IOCTL if DC slaves are located in or after a junction redundancy segment will generate an undefined behavior.