5.16. INtime HPE - emllHPE

emllHPE is part of EC-Master for INtime. emllHPE uses the INtime High-Performance Ethernet (HPE) interface. The parameters to emllHPE are setup-specific. The function CreateLinkParmsFromCmdLineHPE() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_HPE

Name of Ethernet Interface, e.g. “ie1g0”

Receive buffer count

Transmit buffer count

Don’t change target MAC address to FF:FF:FF:FF:FF:FF