5.31. AMD Tri-Mode Ethernet Media Access Controller (TEMAC)

The parameters to the TEMAC Real-time Ethernet Driver are setup-specific. The function CreateLinkParmsFromCmdLineTemac() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_TEMAC

Receive buffer count, 0: default to 100

5.31.1. Encustra Mercury_XU5_PE1

Support for FPGA designs with TEMAC with XAE_SOFT_TEMAC_LOW_SPEED and XPAR_AXI_FIFO.