5.36. Virtual Local Area Network - emllVlan
The parameters to the VLAN Real-time Ethernet Driver are setup-specific. The function “CreateLinkParmsFromCmdLineVlan” in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.
-
struct EC_T_LINK_PARMS_VLAN
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_MULTIPLIER
-
EC_T_LINK_PARMS *pHwLinkParms
Link parameters of network adapter connected to the uplink of the Multiplier
-
EC_T_LINK_PARMS linkParms
5.36.1. Switch Configuration
Ensure that the Spanning Tree Protocol (STP) is disabled on the ports used for EtherCAT, because it can lead to permanent frame loss.