9.10. Hot Connect

9.10.1. emonHCGetNumGroupMembers

EC_T_DWORD emonHCGetNumGroupMembers(EC_T_DWORD dwInstanceID, EC_T_DWORD dwGroupIndex)

Get number of slaves belonging to a specific Hot-Connect group.

Parameters:
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • dwGroupIndex – [in] Index of Hot-Connect group, 0 is the mandatory group

Returns:

Number of slaves

9.10.2. emonHCGetSlaveIdsOfGroup

EC_T_DWORD emonHCGetSlaveIdsOfGroup(EC_T_DWORD dwInstanceID, EC_T_DWORD dwGroupIndex, EC_T_DWORD *adwSlaveId, EC_T_DWORD dwMaxNumSlaveIds)

Get the list of Slave IDs belonging to a specific Hot-Connect group.

Parameters:
  • dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)

  • dwGroupIndex – [in] Index of Hot-Connect group, 0 is the mandatory group

  • adwSlaveId – [out] Preallocated Slave ID list buffer

  • dwMaxNumSlaveIds – [in] Size of Slave ID list buffer

Returns:

EC_E_NOERROR or error code

9.10.3. emonNotify - EC_NOTIFY_HC_DETECTADDGROUPS

This notification is raised when HotConnect group detection is finished, after slave addition.

emonNotify - EC_NOTIFY_HC_DETECTADDGROUPS
Parameter
  • pbyInBuf: [in] pointer to notification descriptor EC_T_HC_DETECTALLGROUP_NTFY_DESC

  • dwInBufSize: [in] sizeof(EC_T_HC_DETECTALLGROUP_NTFY_DESC)

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

struct EC_T_HC_DETECTALLGROUP_NTFY_DESC

Public Members

EC_T_DWORD dwResultCode

Result of Group detection

EC_T_DWORD dwGroupCount

Total number of Groups

EC_T_DWORD dwGroupsPresent

Number of connected groups

EC_T_DWORD dwGroupMask

Bitmask of first 32 Groups. 1 = present, 0 = absent

EC_T_DWORD adwGroupMask[100]

Bitmask of first 3200 Groups.

9.10.4. emonNotify - EC_NOTIFY_HC_PROBEALLGROUPS

This notification is raised when HotConnect Group Detection is finished, after Slave Disappearance.

emonNotify - EC_NOTIFY_HC_PROBEALLGROUPS
Parameter
  • pbyInBuf: [in] pointer to notification descriptor EC_T_HC_DETECTALLGROUP_NTFY_DESC

  • dwInBufSize: [in] sizeof(EC_T_HC_DETECTALLGROUP_NTFY_DESC)

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

struct EC_T_HC_DETECTALLGROUP_NTFY_DESC
EC_T_DWORD dwResultCode
EC_T_DWORD dwGroupCount
EC_T_DWORD dwGroupsPresent
EC_T_DWORD dwGroupMask
EC_T_DWORD adwGroupMask[100]

9.10.5. emonNotify - EC_NOTIFY_HC_TOPOCHGDONE

This notification is raised when HotConnect has completely processed a topology change.

emonNotify - EC_NOTIFY_HC_TOPOCHGDONE
Parameter
  • pbyInBuf: [in] Pointer to EC_T_DWORD (EC_E_NOERROR on success, Error code otherwise)

  • dwInBufSize: [in] sizeof(EC_T_DWORD)

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

The notification is raised when the slaves reached the current bus state.