9.2. Packet Capture

9.2.1. emonOpenPacketCapture

EC_T_DWORD emonOpenPacketCapture(EC_T_DWORD dwInstanceID, EC_T_PACKETCAPTURE_PARMS *pParms)

Open packet capture file (PCAP).

Opens a PCAP trace for further processing within the JobTask. No LinkLayer must have been loaded.

Parameters:
  • dwInstanceID – [in] Instance ID

  • pParms – [in] Packet capture parameter

Returns:

struct EC_T_PACKETCAPTURE_PARMS

Public Members

EC_T_CHAR szFileName[EC_PACKETCAPTURE_FILE_NAME_SIZE]

[in] File name. Supported formats are *.pcap or *.pcapng

EC_T_BOOL bReadMultipleFiles

[in] Read multiple contiguous files. File name format must be “fileName.nnnnn.pcap[ng]”, e.g. wireshark.00000.pcap

EC_T_DWORD dwMaxFrameCnt

[in] Creates a new file every time the number of frames written exceeds this limit. Disabled with a value set to 0.

EC_T_DWORD dwMaxFileSize

[in] Creates a new file every time the number of bytes written exceeds this limit. Disabled with a value set to 0.

EC_T_DWORD dwRingBufferFileCnt

[in] Form a ring buffer of the capture files with the given number of files. Only if EC_T_PACKETCAPTURE_PARMS::dwMaxFrameCnt or EC_T_PACKETCAPTURE_PARMS::dwMaxFileSize are set. Disabled with a value set to 0.

Example
EC_T_PACKETCAPTURE_PARMS PacketCaptureParms;
OsMemset(&PacketCaptureParms, dwInstanceId, sizeof(EC_T_PACKETCAPTURE_PARMS));

OsStrcpy(PacketCaptureParms.szFileName, "C:\\ecat.pcap");
dwRes = emonOpenPacketCapture(0, &PacketCaptureParms);
if (EC_E_NOERROR != dwRes)
{
    EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "Cannot open packet capture: %s (0x%lx))\n",
        ecatGetText(dwRes), dwRes));
}

9.2.2. emonClosePacketCapture

EC_T_DWORD emonClosePacketCapture(EC_T_DWORD dwInstanceID)

Close packet capture file (PCAP).

Parameters:

dwInstanceID – [in] Instance ID

Returns:

9.2.3. emonGetPacketCaptureInfo

EC_T_DWORD emonGetPacketCaptureInfo(EC_T_DWORD dwInstanceID, EC_T_PACKETCAPTURE_INFO *pInfo)

Get packet capture file processing status information.

Parameters:
  • dwInstanceID – [in] Instance ID

  • pInfo – [out] Packet capture info descriptor

Returns:

struct EC_T_PACKETCAPTURE_INFO

Public Members

EC_T_PACKETCAPTURE_STATUS eStatus

[out] Status of packet capture processing

EC_T_CHAR szFileName[EC_PACKETCAPTURE_FILE_NAME_SIZE]

[out] File name of current processed capture

EC_T_UINT64 qwFrameNumberTotal

[out] Total number of processed frames from all capture files

EC_T_UINT64 qwFrameNumberCur

[out] Last processed frame number from the current packet capture file

EC_T_UINT64 qwBytesProcessed

[out] Number of processed bytes from the current packet capture file

EC_T_UINT64 qwFileSize

[out] File size[bytes] of the current packet capture

EC_T_UINT64 qwTimeStamp

[out] Time stamp[ns] of the last processed frame from the current packet capture file

EC_T_DWORD dwCyclesProcessed

[out] Number of EtherCAT cycles processed

enum EC_T_PACKETCAPTURE_STATUS

Values:

enumerator ePcapStatus_Unknown

Unknown packet capture status

enumerator ePcapStatus_NotLoaded

No packet capture loaded

enumerator ePcapStatus_Running

Packet capture processing running

enumerator ePcapStatus_Finished

Packet capture processing finished

enumerator ePcapStatus_Dummy

9.2.4. emonStartLivePacketCapture

EC_T_DWORD emonStartLivePacketCapture(EC_T_DWORD dwInstanceID, EC_T_PACKETCAPTURE_PARMS *pParms)

Start live packet capture (PCAP).

Starts a live recording of the EtherCAT frames in a specified PCAP file.

Note

Only the PCAP file format is currently supported.

Parameters:
  • dwInstanceID – [in] Instance ID

  • pParms – [in] Packet capture parameter

Returns:

9.2.5. emonStopLivePacketCapture

EC_T_DWORD emonStopLivePacketCapture(EC_T_DWORD dwInstanceID)

Stop live packet capture (PCAP).

Stops a previously started live recording of the EtherCAT frames.

Parameters:

dwInstanceID – [in] Instance ID

Returns:

9.2.6. emonBacktracePacketCapture

EC_T_DWORD emonBacktracePacketCapture(EC_T_DWORD dwInstanceID, EC_T_PACKETCAPTURE_PARMS *pParms)

Dump packet capture (PCAP) from backtrace buffer.

Writes a backtrace of the received frames in a specified PCAP file. The number of frames in the backtrace buffer is parameterized via EC_T_MONITOR_INIT_PARMS::dwBacktraceFrames.

Note

Only the PCAP file format is currently supported.

Parameters:
  • dwInstanceID – [in] Instance ID

  • pParms – [in] Packet capture parameter

Returns: