9.1. General functions
9.1.1. emonInitMonitor
-
EC_T_DWORD emonInitMonitor(EC_T_DWORD dwInstanceId, EC_T_MONITOR_INIT_PARMS *pParms)
Initialize EC-Monitor.
This function has to be called prior to calling any other function of EC-Monitor.
- Parameters:
dwInstanceId – [in] Instance ID
pParms – [in] Monitor initialization parameters
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_MONITOR_INIT_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Set to MONITOR_SIGNATURE
-
EC_T_DWORD dwSize
[in] Set to sizeof(EC_T_MONITOR_INIT_PARMS)
-
EC_T_LOG_PARMS LogParms
[in] Logging parameters
-
EC_T_OS_PARMS *pOsParms
[in] Operation system layer parameters
-
EC_T_LINK_PARMS *pLinkParms
[in] Link layer parameters
-
EC_T_ETHERNET_TAP_TYPE eEthTapType
[in] Type of Ethernet TAP
-
EC_T_DWORD dwBusCycleTimeUsec
[in] Bus cycle time [usec]
-
EC_T_DWORD dwMaxBusSlaves
[in] Maximum pre-allocated bus slave objects
-
EC_T_DWORD dwBacktraceFrames
[in] Number of frames held in backtrace buffer. Total memory requirements of the buffer: \( 2 \times dwBacktraceFrames \times 1536 bytes \)
-
EC_T_PERF_MEAS_INTERNAL_PARMS PerfMeasInternalParms
[in] Internal performance measurement parameters
-
EC_T_WORKER_THREAD_PARMS WorkerThreadParms
[in] Internal worker thread parameters
-
EC_T_DWORD dwCommunicationTimeoutMsec
[in] Timeout [msec] for communication on the Ethernet TAP. 0: defaults to 3 sec, EC_WAITINFINITE: disables monitoring
-
EC_T_BOOL bApiLockByApp
[in] Lock pending API against emonDeinitMonitor(). EC_FALSE (default): locked internally. EC_TRUE: application is responsible for locking.
-
EC_T_CHAR szFileStoragePath[EC_FILESTORAGE_PATH_SIZE]
[in] Path used to store records and files, e.g. FoE transfers. EC_NULL: defaults to “”
-
EC_T_MBX_PARMS MbxParms
[in] Mailbox monitoring parameters
-
EC_T_BOOL bProcessRestructuredCyclicCmds
[in] Support processing of restructured cyclic command layout. All cyclic commands are processed as long as they are within the process data boundary of the ENI.
-
EC_T_DWORD dwSignature
-
enum EC_T_ETHERNET_TAP_TYPE
Values:
-
enumerator eEthTap_AutoDetect
Auto detect TAP type. If no suitable type is detected, eEthTap_Generic is used
-
enumerator eEthTap_AutoDetect
-
struct EC_T_OS_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Set to EC_OS_PARMS_SIGNATURE
-
EC_T_DWORD dwSize
[in] Set to sizeof(EC_T_OS_PARMS)
-
EC_T_LOG_PARMS *pLogParms
[in] Pointer to logging parameters
-
EC_PF_SYSTIME pfSystemTimeGet
[in] Function to get host time in nanoseconds since 1st January 2000. Used as time base for DC Initialization.
-
EC_T_DWORD dwSupportedFeatures
[in/out] reserved
-
EC_T_DWORD dwSignature
-
struct EC_T_LOG_PARMS
Public Members
-
EC_T_DWORD dwLogLevel
[in] Log level. See EC_LOG_LEVEL_…
-
EC_PF_LOGMSGHK pfLogMsg
[in] Log callback function called on every message
-
EC_T_DWORD dwLogLevel
-
typedef EC_T_DWORD (*EC_PF_LOGMSGHK)(EC_T_LOG_CONTEXT *pContext, EC_T_DWORD dwLogMsgSeverity, const EC_T_CHAR *szFormat, ...)
- Param pContext:
[in] Context pointer. This pointer is used as parameter when the callback function is called
- Param dwLogMsgSeverity:
[in] Log message severity, EC_LOG_LEVEL_…
- Param szFormat:
[in] String that contains the text to be written. It can optionally contain embedded format specifiers that are replaced by the values specified in subsequent additional arguments and formatted as requested.
- Return:
EC_E_NOERROR or error code
-
struct EC_T_PERF_MEAS_INTERNAL_PARMS
Public Members
-
EC_T_BOOL bEnabled
[in] enable/disable internal performance counters.
-
EC_T_PERF_MEAS_COUNTER_PARMS CounterParms
[in] Timer function settings. When not provided OsMeasGetCounterTicks is used
-
EC_T_PERF_MEAS_HISTOGRAM_PARMS HistogramParms
[in] Histogram settings. When not provided the histogram is disabled.
-
EC_T_BOOL bEnabled
-
struct EC_T_PERF_MEAS_COUNTER_PARMS
Public Members
-
EC_PF_PERF_MEAS_GETCOUNTERTICKS pfGetCounterTicks
[in] Function returning the current counter ticks
-
EC_T_UINT64 qwFrequency
[in] Frequency in Hz used by the timer in GetCounterTicks
-
EC_PF_PERF_MEAS_GETCOUNTERTICKS pfGetCounterTicks
-
typedef EC_T_UINT64 (*EC_PF_PERF_MEAS_GETCOUNTERTICKS)(EC_T_VOID *pvContext)
- Param pvContext:
[in] Arbitrarily application-defined parameter passed to callback
-
struct EC_T_PERF_MEAS_HISTOGRAM_PARMS
Public Members
-
EC_T_DWORD dwBinCount
[in] amount of bins to use for the histogram.
-
EC_T_UINT64 qwMinTicks
[in] results below qwMinTicks are stored in the first bin
-
EC_T_UINT64 qwMaxTicks
[in] results above qwMaxTicks are stored in the last bin
-
EC_T_DWORD dwBinCount
-
struct EC_T_WORKER_THREAD_PARMS
Public Members
-
EC_T_DWORD dwPrio
[in] Priority to use for the worker thread
-
EC_T_DWORD dwPrio
-
struct EC_T_MBX_PARMS
Public Members
-
EC_T_DWORD dwMemoryPoolSize
[in] Memory for each slave supporting mailbox communication to record e.g. the CoE dictionary. The memory is asynchronously increased by dwBufferSize by the WorkerThread when it is over 80% full. 0: defaults to 1kb
-
EC_T_MBX_PARMS_COE Coe
[in] CoE parameters
-
EC_T_MBX_PARMS_FOE Foe
[in] FoE parameters
-
EC_T_DWORD dwMemoryPoolSize
-
struct EC_T_MBX_PARMS_FOE
Public Members
-
EC_T_BOOL bDisableNotifications
[in] Disable all FoE related EC_NOTIFY_MBOXRCV notifications
-
EC_T_BOOL bDisableFileStorage
[in] Disable storage of FoE transfers as a file on the file system
-
EC_T_DWORD dwMaxQueuedMbxTransfers
[in] Maximum number of queued single FoE mailbox transfers that be used as a file write buffer. 0: defaults to 32
-
EC_T_BOOL bDisableNotifications
9.1.2. emonDeinitMonitor
-
EC_T_DWORD emonDeinitMonitor(EC_T_DWORD dwInstanceId)
Deinitialize EC-Monitor.
Waits for pending API calls if emonInitMonitor() was called with EC_T_MONITOR_INIT_PARMS::bApiLockByApp = EC_FALSE (default).
- Parameters:
dwInstanceId – [in] Instance ID
- Returns:
EC_E_NOERROR or error code
9.1.3. emonConfigureNetwork
-
EC_T_DWORD emonConfigureNetwork(EC_T_DWORD dwInstanceID, EC_T_CNF_TYPE eCnfType, EC_T_PBYTE pbyCnfData, EC_T_DWORD dwCnfDataLen)
Configure the Network.
This function must be called after the initialization. Among others the EtherCAT topology defined in the given XML configuration file will be stored internally.
Note
A client must not be registered prior to calling this function. Existing client registrations will be dropped.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
eCnfType – [in] Type of configuration data provided
pbyCnfData – [in] Filename / configuration data, or EC_NULL if eCnfType is eCnfType_GenEBI
dwCnfDataLen – [in] Length of configuration data in byte, or zero if eCnfType is eCnfType_GenEBI
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized or eCnfType is eCnfType_GenPreopENI or eCnfType_GenOpENI and link is disconnected
EC_E_INVALIDPARM if dwInstanceID is out of range or pParms is EC_NULL contains some values out of range
EC_E_LINK_DISCONNECTED if link is disconnected
EC_E_FEATURE_DISABLED if a configured feature is not included in the license key
EC_E_NOTSUPPORTED if a configured feature is not supported (e.g not compiled in the library)
EC_E_CFGFILENOTFOUND if the ENI file cannot be found
EC_E_WRONG_FORMAT if some format error have been detected in the ENI or EEPROM in case of eCnfType_GenPreopENI or eCnfType_GenOpENI
EC_E_OEM_SIGNATURE_MISMATCH if the OEM signature in the ENI file doesn’t match the used OEM key
EC_E_ENI_ENCRYPTION_WRONG_VERSION if the ENI encryption version is not supported (e.g. the library is too old)
EC_E_ENI_ENCRYPTED if the ENI is encrypted and no OEM key has been set
EC_E_XML_CYCCMDS_MISSING if the ENI doesn’t contain cyclic commands
EC_E_XML_ALSTATUS_READ_MISSING if the ENI doesn’t contain any read AL status command
EC_E_XML_CYCCMDS_SIZEMISMATCH if the size of the cyclic commands in the ENI mismatch
EC_E_XML_INVALID_INP_OFF if some input offset in the ENI are invalid
EC_E_XML_INVALID_OUT_OFF if some output offset in the ENI are invalid
EC_E_XML_INVALID_CMD_WITH_RED if the ENI contains LRW commands and cable redundancy is configured
EC_E_XML_PREV_PORT_MISSING if some previous port information are missing in the ENI
EC_E_XML_DC_CYCCMDS_MISSING if the DC related cyclic commands are missing in the ENI
EC_E_XML_AOE_NETID_INVALID if the ENI contains some invalid NetID
-
enum EC_T_CNF_TYPE
Values:
-
enumerator eCnfType_GenOpENI
Generate ENI based on bus-scan result to get into OP state. The default PDO mapping read from the slaves is activated. See ETG2010 “SII Specification”, Table 14 “Structure Category TXPDO and RXPDO for each PDO”
-
enumerator eCnfType_GenOpENI
9.1.4. emonGetMonitorStatus
-
EC_T_DWORD emonGetMonitorStatus(EC_T_DWORD dwInstanceID, EC_T_MONITOR_STATUS *pStatus)
Get current Monitor status.
Information about the current status of the EtherCAT frame / cycle processing
- Parameters:
dwInstanceID – [in] Instance ID
pStatus – [out] Monitor status descriptor
- Returns:
EC_E_NOERROR on success
EC_E_INVALIDSTATE if Monitor isn’t initialized
EC_E_INVALIDPARM if pStatus invalid
-
struct EC_T_MONITOR_STATUS
Public Members
-
EC_T_BOOL bNextFramesReceived
[out] Indicates whether further unprocessed frames form the next EtherCAT cycle were received
-
EC_T_DWORD dwCyclesProcessed
[out] Number of EtherCAT cycles processed
-
EC_T_WORD wEthTapPositionAutoIncAddr
[out] Ethernet tap position as auto increment address
-
EC_T_BOOL bNextCyclicEntryReceived
[out] Indicates whether all frames from the next EtherCAT cycle have been received and have not yet been processed
-
EC_T_ETHERNET_TAP_TYPE eEthTapType
[out] Type of Ethernet TAP. Detected TAP if EC_T_MONITOR_INIT_PARMS::eEthTapType = eEthTap_AutoDetect is set
-
EC_T_BOOL bTopologyKnown
[out] Topology successfully detected and validated
-
EC_T_BOOL bPdoAssigned
[out] PDO assignment of all slaves detected and validated
-
EC_T_BOOL bPdoMapped
[out] PDO mapping (SyncSM/FMMU) of all slaves detected and validated
-
EC_T_BOOL bPdCommunicationDetected
[out] Process Data communication detected
-
EC_T_WORD wDeviceStatesDetected
[out] Bit mask that indicates which slave states already detected/monitored, see Slave device state’s
-
EC_T_BOOL bNextFramesReceived
Slave device state’s
9.1.5. emonSetLicenseKey
-
EC_T_DWORD emonSetLicenseKey(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szLicenseKey)
Sets the license key for the protected version of EC-Master.
Must be called after initialization and before configuration. This function may not be called if a non protected version is used.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
szLicenseKey – [in] License key as zero terminated string with 26, 53 or 56 characters.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_INVALIDSIZE the format of the license key is wrong. The correct length is 26, 53 or 56 characters
EC_E_LICENSE_MISSING the license key doesn’t match the MAC Address
Example
dwRes = emonSetLicenseKey(dwInstanceId, "DA1099F2-15C249E9-54327FBC");
if (dwRes != EC_E_NOERROR)
{
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "ERROR: Cannot set license key: %s (0x%lx))\n",
ecatGetText(dwRes), dwRes));
}
See also
9.1.6. emonRegisterClient
-
EC_T_DWORD emonRegisterClient(EC_T_DWORD dwInstanceID, EC_PF_NOTIFY pfnNotify, EC_T_VOID *pCallerData, EC_T_REGISTERRESULTS *pRegResults)
Register the application as a client with the EtherCAT stack for notifications (EC_NOTIFY_… )
It must be called after configuration, otherwise the registration handle is lost. This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pfnNotify – [in] Notification callback function. This function will be called every time a state change occurs, an error occurs or a mailbox transfer terminates.
pCallerData – [in] Parameter passed to the application when the notification callback is called. The parameter can be arbitrarily defined by the application.
pRegResults – [out] Registration results
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_NOMEMORY if some memory cannot be allocated
-
typedef EC_T_DWORD (*EC_PF_NOTIFY)(EC_T_DWORD dwCode, EC_T_NOTIFYPARMS *pParms)
- Param dwCode:
[in] Notification code, see EC_NOTIFY_…
- Param pParms:
[in] Notification code depending data.
-
struct EC_T_REGISTERRESULTS
Public Members
-
EC_T_DWORD dwClntId
[out] Client ID
-
EC_T_BYTE *pbyPDIn
[out] Pointer to process data input memory
-
EC_T_DWORD dwPDInSize
[out] Size of process data input memory (in bytes)
-
EC_T_BYTE *pbyPDOut
[out] Pointer to process data output memory
-
EC_T_DWORD dwPDOutSize
[out] Size of process data output memory (in bytes)
-
EC_T_DWORD dwClntId
9.1.7. emonUnregisterClient
-
EC_T_DWORD emonUnregisterClient(EC_T_DWORD dwInstanceID, EC_T_DWORD dwClntId)
Deregister a client from the EtherCAT stack.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwClntId – [in] Client ID from registeration with the EtherCAT stack
- Returns:
EC_E_NOERROR or error code
9.1.8. emonGetSrcMacAddress
-
EC_T_DWORD emonGetSrcMacAddress(EC_T_DWORD dwInstanceID, ETHERNET_ADDRESS *pMacSrc)
Gets the source MAC address.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMacSrc – [out] 6-byte buffer to write source MAC address to.
- Returns:
EC_E_NOERROR or error code
-
struct ETHERNET_ADDRESS
Public Members
-
EC_T_BYTE b[6]
MAC address
-
EC_T_BYTE b[6]
See also
9.1.9. emonExecJob
-
EC_T_DWORD emonExecJob(EC_T_DWORD dwInstanceID, EC_T_USER_JOB eUserJob, EC_T_USER_JOB_PARMS *pUserJobParms)
Execute or initiate the requested EtherCAT stack job.
To achieve maximum speed, this function is implemented non re-entrant. It is highly recommended that only one single task is calling all required jobs to run the stack. If multiple tasks are calling this function, the calls have to be synchronized externally. Calling it in a context that doesn’t support operating system calls can lead to unpredictable behavior.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
eUserJob – [in] user requested job
pUserJobParms – [in] optional user job parameters
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_LINK_DISCONNECTED if the link is disconnected
EC_E_FEATURE_DISABLED for eUsrJob_SwitchEoeFrames if EC_IOCTL_SET_EOE_DEFFERED_SWITCHING_ENABLED hasn’t be called before
EC_E_ADS_IS_RUNNING if ADS server is running
Brief job overview:
-
union EC_T_USER_JOB_PARMS
Public Members
-
EC_T_BOOL bAllCycFramesProcessed
-
EC_T_DWORD dwNumFramesSent
-
EC_T_DWORD dwTaskIdToSend
-
struct EC_T_USER_JOB_PARMS::_SEND_CYCFRAME_BY_TASKID SendCycFramesByTaskId
-
struct EC_T_USER_JOB_PARMS::_PROCESS_RXFRAME_BY_TASKID ProcessRxFramesByTaskId
-
struct EC_T_USER_JOB_PARMS::_SWITCH_EOE_FRAMES SwitchEoeFrames
-
struct EC_T_USER_JOB_PARMS::_START_TASK StartTask
-
struct EC_T_USER_JOB_PARMS::_STOP_TASK StopTask
-
struct _SEND_CYCFRAME_BY_TASKID
Public Members
-
EC_T_DWORD dwTaskId
-
EC_T_DWORD dwTaskId
-
struct _START_TASK
Public Members
-
EC_T_DWORD dwTaskId
-
EC_T_DWORD dwTaskId
-
struct _STOP_TASK
Public Members
-
EC_T_DWORD dwTaskId
-
EC_T_DWORD dwTaskId
-
EC_T_BOOL bAllCycFramesProcessed
Detailed job description:
eUsrJob_ProcessAllRxFramesWhen the Real-time Ethernet Driver operates in polling mode this call will process all currently received frames, when the Real-time Ethernet Driver operates in interrupt mode all received frames are processed immediately and this call just returns with nothing done.
pUserJobParms->bAllCycFramesProcessed
This flag is set to a value of
EC_TRUEit indicates that all previously initiated cyclic frames (eUsrJob_SendAllCycFrames) are received and processed within this call. Not used if pUserJobParms set toEC_NULL.Return: EC_E_NOERROR if successful, error code in case of failures.
eUsrJob_MonitorTimerTo trigger the monitor and slave state machines as well as the mailbox handling this call has to be executed cyclically. The monitor cycle time is determined by the period between calling
emonExecJob()(eUsrJob_MonitorTimer). The state-machines are handling the EtherCAT® state change transfers.Return: EC_E_NOERROR if successful, error code in case of failures.
9.1.10. emonGetMonitorParms
-
EC_T_DWORD emonGetMonitorParms(EC_T_DWORD dwInstanceID, EC_T_MONITOR_INIT_PARMS *pParms, EC_T_DWORD dwParmsBufSize)
Gets current Monitor Init Parameters.
If the given buffer is larger than the actual size of struct EC_T_MONITOR_INIT_PARMS, the parameters of EC_T_MONITOR_INIT_PARMS.pOsParms, EC_T_MONITOR_INIT_PARMS.pLinkParms are appended.
- Parameters:
dwInstanceID – [in] Instance ID
pParms – [out] Buffer to store parameters
dwParmsBufSize – [in] Size of buffer in bytes
- Returns:
EC_E_NOERROR on success
EC_E_INVALIDSTATE if Monitor isn’t initialized
EC_E_INVALIDPARM if buffer pParms is too small
Example
/* Read all monitor init parameters, including OS and Link parameters */
EC_T_BYTE abyBuffer[sizeof(EC_T_MONITOR_INIT_PARMS) + sizeof(EC_T_OS_PARMS) + 512 /* LinkLayer parameters */];
EC_T_MONITOR_INIT_PARMS* pParms = (EC_T_MONITOR_INIT_PARMS*)abyBuffer;
OsMemset(abyBuffer, 0, sizeof(abyBuffer));
dwRes = emonGetMonitorParms(dwInstanceId, pParms, sizeof(abyBuffer));
if (EC_E_NOERROR != dwRes)
{
EcLogMsg(EC_LOG_LEVEL_ERROR, (pEcLogContext, EC_LOG_LEVEL_ERROR, "Cannot get monitor parameters: %s (0x%lx))\n",
ecatGetText(dwRes), dwRes));
}
See also
9.1.11. emonSetMonitorParms
-
EC_T_DWORD emonSetMonitorParms(EC_T_DWORD dwInstanceID, EC_T_MONITOR_INIT_PARMS *pParms)
Change Monitor Init Parameters.
OS parms, Main Link parms cannot be changed.
- Parameters:
dwInstanceID – [in] Instance ID
pParms – [in] New Monitor init parameters
- Returns:
EC_E_NOERROR on success
EC_E_INVALIDSTATE if Monitor isn’t initialized
See also
9.1.12. emonGetVersion
-
EC_T_DWORD emonGetVersion(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwVersion, EC_T_DWORD *pdwVersionType)
Gets the version information.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwVersion – [out] Pointer to EC_T_DWORD to carry out version number as a 32-bit value
pdwVersionType – [out] Pointer to EC_T_DWORD to carry out version type. See EC_VERSION_TYPE
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
9.1.13. emonGetText
-
const EC_T_CHAR *emonGetText(EC_T_DWORD dwInstanceID, EC_T_DWORD dwTextId)
Return text tokens by ID.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns:
Textual description of the given ID
9.1.14. emonGetMemoryUsage
-
EC_T_DWORD emonGetMemoryUsage(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwCurrentUsage, EC_T_DWORD *pdwMaxUsage)
Returns information about memory usage.
All calls to malloc/free and new/delete are monitored.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwCurrentUsage – [out] Current memory usage in Bytes at the time where this function is called
pdwMaxUsage – [out] Maximum memory usage in Bytes since initialization at the time where this function is called
- Returns:
EC_E_NOERROR or error code
9.1.15. emonGetMasterState
-
EC_T_STATE emonGetMasterState(EC_T_DWORD dwInstanceID)
Get the EtherCAT master current state.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns:
EtherCAT master state
9.1.16. emonGetMasterStateEx
-
EC_T_DWORD emonGetMasterStateEx(EC_T_DWORD dwInstanceID, EC_T_WORD *pwCurrState, EC_T_WORD *pwReqState)
Get the EtherCAT master current and requested state. Possible return values for current and requested state:
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pwCurrState – [out] Current master state.
pwReqState – [out] Requested master state
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointers are EC_NULL
Limitation
Since it is not possible to determine the actual requested master state, the highest slave state of all slaves is assumed to be the requested master state.
9.1.17. emonFindInpVarByName - “Inputs.DevicesState”
The device status of all slaves (OR-linked) is part of the process data with name “Inputs.DevicesState”.
-
EC_T_DWORD emonFindInpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
9.1.18. emonFindInpVarByName - “Inputs.BusTime”
The DC system time (written to ESC register 0x0910) is part of the process data with name “Inputs.BusTime”.
-
EC_T_DWORD emonFindInpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
9.1.19. emonExportEniBuilderConfig
-
EC_T_DWORD emonExportEniBuilderConfig(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szFileName)
Export an EniBuilder file describing the observed network topology.
- Parameters:
dwInstanceID – [in] Instance ID
szFileName – [in] null-terminated export file path
- Returns:
EC_E_NOERROR on success
EC_E_INVALIDPARM if parameter file name invalid
EC_E_OPENFAILED if file could not be opened
EC_E_NOMEMORY if not enough memory available
See also
9.1.20. emonIoControl
With emonIoControl a generic control interface exists between the application and the EC-Monitor and its Real-time Ethernet Drivers.
-
struct EC_T_IOCTLPARMS
Public Members
-
EC_T_BYTE *pbyInBuf
[in] Pointer to control input parameter.
-
EC_T_DWORD dwInBufSize
[in] Size of the input buffer provided at pbyInBuf in bytes
-
EC_T_BYTE *pbyOutBuf
[out] Pointer to control output buffer where the results will be copied into
-
EC_T_DWORD dwOutBufSize
[in] Size of the output buffer provided at pbyOutBuf in bytes
-
EC_T_DWORD *pdwNumOutData
[out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer
-
EC_T_BYTE *pbyInBuf
9.1.21. emonIoControl - EC_IOCTL_REGISTER_CYCFRAME_RX_CB
This function call registers an callback function which is called after the cyclic frame is received. Typically this is used when the Real-time Ethernet Driver operates interrupt mode to get an event when the new input data (cyclic frame) is available.
The callback function has to be registered after calling emonInitMonitor() before starting the job task.
- emonIoControl - EC_IOCTL_REGISTER_CYCFRAME_RX_CB
- Parameter
pbyInBuf: [in] Cyclic frame received callback descriptor (EC_T_CYCFRAME_RX_CBDESC)dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_CYCFRAME_RX_CBDESC
Public Members
-
EC_T_VOID *pCallbackContext
[in] Context pointer. This pointer is used as parameter every time when the callback function is called
-
EC_PF_CYCFRAME_RECV pfnCallback
[in] This function will be called after the cyclic frame is received, if there is more than one cyclic frame after the last frame. The application has to assure that these functions will not block.
-
EC_T_VOID *pCallbackContext
-
typedef EC_T_VOID (*EC_PF_CYCFRAME_RECV)(EC_T_DWORD dwTaskId, EC_T_VOID *pvContext)
- Param dwTaskId:
[in] Task ID of the received cyclic frame (ENI: Cyclic/TaskId)
- Param pvContext:
[in] Arbitrarily application-defined parameter passed to callback
9.1.22. emonIoControl - EC_IOCTL_GET_CYCLIC_CONFIG_INFO
Get cyclic configuration details from ENI configuration file.
- emonIoControl - EC_IOCTL_GET_CYCLIC_CONFIG_INFO
- Parameter
pbyInBuf: [in] Pointer to dwCycEntryIndex: cyclic entry index for which to get informationdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Pointer to EC_T_CYC_CONFIG_DESC data typedwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
-
struct EC_T_CYC_CONFIG_DESC
Public Members
-
EC_T_DWORD dwNumCycEntries
[out] Total number of cyclic entries
-
EC_T_DWORD dwTaskId
[out] Task ID of selected cyclic entry (ENI: Cyclic/TaskId)
-
EC_T_DWORD dwPriority
[out] Priority of selected cyclic entry
-
EC_T_DWORD dwCycleTime
[out] Cycle time of selected cyclic entry
-
EC_T_DWORD dwNumCycEntries
9.1.23. emonIoControl - EC_IOCTL_IS_SLAVETOSLAVE_COMM_CONFIGURED
Determine if any slave-to-slave communication is configured.
- emonIoControl - EC_IOCTL_IS_SLAVETOSLAVE_COMM_CONFIGURED
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_DWORD. If value is EC_TRUE slave-to-slave communication is configured, if EC_FALSE it is not.dwOutBufSize: [in] Size of the output buffer in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.