7.1. Linux
7.1.1. OS optimizations
Linux itself is not real-time capable, so it is recommended to use it with the additional PREEMPT_RT patch.
The power management can disrupt cyclical processing, it is advisable to disable the CPUIDLE sub-system and CPUFREQ sub-system. The sub-systems can be disabled by changing the kernel command line parameters in the boot loader. On x86, x86_64 systems this is usually GRUB, on embedded devices with ARM, ARM64 is usually u-boot. It is also possible to build a custom kernel without these sub-systems.
Running a EC-Monitor application on a dedicated CPU core that is isolated from the Linux scheduler (ISOLCPUS) can provide additional stability.
7.1.1.1. CPUIDLE sub-system
- Check if CPUFREQ sub-system is enabled:
$ ls /sys/devices/system/cpu/
If cpuidle appears in the list, it is enabled.
- Disable CPUIDLE via the kernel command-line in GRUB:
linux /boot/vmlinuz-4.19.0-16-rt-amd64 cpuidle.off=1
7.1.1.2. CPUFREQ sub-system
- Check if CPUFREQ sub-system is enabled:
$ ls /sys/devices/system/cpu/
If cpufreq appears in the list, it is enabled.
- Disable CPUFREQ sub-system via the kernel command-line GRUB:
linux /boot/vmlinuz-4.19.0-16-rt-amd64 cpufreq.off=1
If CPUFREQ is not to be deactivated, the governor should be set to performance.
- The currently active governor can be determined as follows:
$ cat /sys/devices/system/cpu/cpu*/cpufreq/scaling_governor
- The available governors with:
$ cat /sys/devices/system/cpu/cpu*/cpufreq/scaling_available_governors
- To change governor use:
$ echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
7.1.1.3. ISOLCPUS
- Isolate CPU core number 4 of a quad-core processor via the kernel command-line GRUB:
linux /boot/vmlinuz-4.19.0-16-rt-amd64 isolcpus=3
isolcpus alone removes scheduler tasks from selected CPUs, but does not prevent timer interrupts, RCU callbacks, or device IRQs. To fully isolate a CPU for real-time workloads, nohz_full, rcu_nocbs, and irqaffinity should be used together to eliminate kernel noise and ensure deterministic execution.
- Enhanced isolation of CPU core 4 via the kernel command-line GRUB:
linux /boot/vmlinuz-4.19.0-16-rt-amd64 isolcpus=3 nohz_full=3 rcu_nocbs=3 rcu_nocb_poll irqaffinity=0-2
- Running EcMonitorDemo on the isolated CPU core by setting the CPU affinity
-a: $ ./EcMonitorDemo -a 3
7.1.2. atemsys kernel module
To use Real-time Ethernet Driver under Linux, the atemsys kernel module must be compiled and loaded. atemsys grants direct access to hardware to improve the performance.
All necessary scripts, source code and a detailed description of the installation can be found on https://github.com/acontis/atemsys. A ready-to-use Yocto recipe is also available on https://github.com/acontis/meta-acontis
7.1.2.1. atemsys as Device Tree Ethernet Driver
atemsys can also be used as a device tree driver to avoid certain conflicts between the Real-time Ethernet Driver and the Linux kernel, e.g. power management, shared MDIO bus, etc..
A detailed guide on how to customize the device tree accordingly can also be found on https://github.com/acontis/atemsys. Example device tree modifications for different Real-time Ethernet Drivers/SoC can be found in https://github.com/acontis/atemsys/wiki.
Note
This is the preferred solution on all embedded devices with device tree support.
7.1.2.2. atemsys and PHY OS Driver
To use the PHY OS Driver, the acontis kernel module atemsys has to be included in the kernel device tree as an official driver for the Ethernet controller and doesn’t required any additional configuration at the application level. As a result atemsys can interact with Linux drivers.
7.1.3. Unbind Ethernet Driver instance
Ethernet Driver instances used by Real-time Ethernet Drivers may not be bound by kernel drivers modules! Unbind can be done by unloading the kernel driver module, via the unbind interface of the driver or by modifying the device tree.
7.1.3.1. Unbind from kernel driver
The following command unbinds an instance without unloading the kernel driver module:
PCI
$ echo "<Instance-ID>" > /sys/bus/pci/drivers/<driver-name>/unbind
Example:
$ echo "0000:00:19.0" > /sys/bus/pci/drivers/e1000e/unbind
This call requires the PCI bus, device, function codes (in the above example it is 0000:00:19.0). The codes can be found using Linux commands like, for example:
$ ls /sys/bus/pci/drivers/e1000e
SoC
$ echo "<Instance-ID>" > /sys/bus/platform/drivers/<driver-name>/unbind
Example:
$ echo "2188000.ethernet" > /sys/bus/platform/drivers/fec/unbind
7.1.3.2. Unload kernel driver
Not all drivers allow unbinding of network adapters. If unbinding is not supported the corresponding Linux kernel driver must not be loaded.
The following command lists the loaded kernel modules that may conflict with Real-time Ethernet Driver:
$ lsmod | egrep "<module-name>"
Example:
$ lsmod | egrep "e1000|e1000e|igb"
PCI/PCIe: The command lspci -v shows which driver is assigned to which network card, e.g.:
$ lspci -v
...
11:0a.0 Ethernet controller: Intel Corporation 82541PI Gigabit Ethernet Controller (rev 05)
...
Kernel driver in use: e1000e
Modules can be prevented from loading with the following commands:
$ echo blacklist <module-name> | sudo tee -a /etc/modprobe.d/blacklist.conf
$ update-initramfs -k all -u
$ sudo reboot
The following table shows the Kernel modules related to the Real-time Ethernet Driver:
Chip |
Real-time Ethernet Driver |
Kernel driver(s) |
Remarks |
|---|---|---|---|
Broadcom Genet |
emllBcmGenet |
genet |
Unbind not supported |
Beckhoff CCAT |
emllCCAT |
ec_bhf |
|
CPSW |
emllCPSW |
ti_cpsw |
|
Generic |
emllDpdk |
||
DesignWare 3504 |
emllDW3504 |
stmmac |
|
emllEG20T |
|||
Freescale TSEC/eTSEC v1/2 |
emllETSEC |
gianfar_driver |
|
Freescale FEC and ENET controller |
emllFslFec |
fec, fec_ptp |
|
Cadence GEM/MACB |
emllGEM |
gem, macb |
|
Intel Pro/1000 |
emllI8254x |
igb, e1000, e1000e |
|
Intel Pro/1000 |
emllIntelGbe |
igb, e1000, e1000e |
|
Intel Pro/100 |
emllI8255x |
e100 |
|
ICSS |
emllICSS |
prueth,pruss |
Unbind not supported |
RDC R6040 |
emllR6040 |
||
Realtek RTL8139 |
emllRTL8139 |
8139too, 8139cp |
|
Realtek RTL8169 / RTL8111 / RTL8168 |
emllRTL8169 |
r8169 |
Unbind not supported |
SuperH |
emllSHEth |
sh_eth |
Unbind not supported |
Generic |
emllSockRaw |
||
Generic |
emllSockXdp |
7.1.4. Docker
It is possible to operate EC-Monitor within a Docker container with realtime priority. The atemsys kernel module should be installed on the host in order to operate the container with the lowest possible capabilities and privileges.
The following additional settings, permissions for docker run are required:
- Add atemsys device to container
--device=/dev/atemsys:/dev/atemsys
- Allow max realtime priority
--ulimit rtprio=99
- Add capability to set priority an lock memory
--cap-add=sys_nice --cap-add=ipc_lock
- Publish RAS server port 6000
-p 6000:6000
7.1.5. Setting up and running EcMonitorDemo
Unbind Ethernet Driver instance, e.g.
$ echo 0000:00:19.0 > /sys/bus/pci/drivers/e1000e/unbind
Load atemsys kernel module
$ insmod atemsys.ko
Copy files from EC-Monitor package
/binand aeni.xmlto directory e.g./tmp.Adjust LD_LIBRARY_PATH search locations for Real-time Ethernet Driver if necessary, e.g.
$ export LD_LIBRARY_PATH=/tmp:$LD_LIBRARY_PATH
Run EcMonitorDemo
$ cd /tmp $ ./EcMonitorDemo -intelgbe 1 1 -f eni.xml -perf
See also
7.1.5.1. Run in Docker container
Unbind Ethernet Driver instance and load atemsys on the host.
Create a directory on the host (e.g.
~/docker) and copy files from EC-Monitor package/binandexi.xmlinto this directory.- Start bash console in container
$ sudo docker run -it \ --name atem_container \ --device=/dev/atemsys:/dev/atemsys \ --ulimit rtprio=99 \ --cap-add=sys_nice --cap-add=ipc_lock \ -v ~/docker:/home/docker \ -p 6000:6000 \ ubuntu bash
Command line arguments:
-itAllocate a pseudo-TTY and run container--name atem_containerContainer name--device=/dev/atemsys:/dev/atemsysAdd atemsys device to container--ulimit rtprio=99Allow max realtime priority--cap-add=sys_niceAdd Linux capability to set priority--cap-add=ipc_lockAdd Linux capability to lock memory-v ~/docker:/home/dockerMount previously create directory to container-p 6000:6000Publish RAS server port 6000ubuntu bashUse Docker image ubuntu and start bash
Run EcMonitorDemo in container
# cd /home/docker # export LD_LIBRARY_PATH=. # ./EcMonitorDemo -intelgbe 2 1 -f eni.xml -perf
7.1.6. OS Compiler settings
Besides the general settings from Compiling the EcMonitorDemo the following settings are necessary to build the example application for Linux
- Possible ARCHs (see ATECAT_ARCHSTR in
SDK/INC/Linux/EcOsPlatform.h): aarch64 (ARM 64Bit)
armv4t-eabi (ARM 32Bit)
armv6-vfp-eabihf (ARM 32Bit)
armv7-vfp-eabihf (ARM 32Bit)
PPC (PPC 32Bit with “-te500v2”)
riscv64 (RISC-V 64Bit)
x64 (x86 64Bit)
x86 (x86 32Bit)
- The ARM 32Bit architectures armv4t-eabi and armv6-vfp-eabihf/armv7-vfp-eabihf are incompatible with each other. An ARM VFP system returns success on
$ readelf -A /proc/self/exe | grep Tag_ABI_VFP_args
- Extra include paths
<InstallPath>/Examples/Common/Linux <InstallPath>/SDK/INC/Linux
- Extra source paths
<InstallPath>/Examples/Common/Linux <InstallPath>/Sources/OsLayer/Linux
- Extra library paths to the main EtherCAT components
<InstallPath>/SDK/LIB/Linux/<Arch>
- Extra libraries (in this order)
EcMonitor pthread dl rt
7.1.7. Build using cmake on Linux
Example usage to build Linux x64 Debug with cmake:
$ cmake -DEC_OS=Linux -DEC_ARCH=x64
$ cmake --build .
7.1.8. Cross-platform development under Windows
The following steps describe how to develop Linux cross-platform developing on Windows for Linux , you can follow :
-DEC_OS=Windows -DEC_ARCH=x64
- Install MinGW
Download the latest version of MinGW from the MinGW official website https://osdn.net/projects/mingw/
Install the mingw-get-setup.exe tool to C:\MinGW
Select the ‘’Basic Setup’’
Apply changes
- Install a cross platform toolchain
Download a cross-platform toolchain from e.g. the Linaro release storage server https://releases.linaro.org/components/toolchain/gcc-linaro/
Unpack it to C:\MinGW\opt
Build using cmake on Linux
Example usage to build for Linux x64 Debug on Windows with cmake and ninja:
$ cmake -DEC_OS=Linux -DEC_ARCH=x64 -DCMAKE_BUILD_TYPE=Debug . $ cmake --build .
Build for LxWin using cmake on Linux
Example usage to build EcMasterDemo for Linux x64 Debug on Windows with cmake and ninja:
Workspace/LxWin/cmake/x64/Debug> cmake.exe -G Ninja ../../../../.. -DCMAKE_TOOLCHAIN_FILE=../../../../Linux/Toolchain.cmake -DEC_OS=LxWin -DEC_ARCH=x64 -DCMAKE_BUILD_TYPE=Debug Workspace/LxWin/cmake/x64/Debug> ninja.exe EcMasterDemo
Cross build using cmake for Linux on Windows
Example usage to build EcMasterDemo for Linux x64 Debug on Windows with cmake and ninja:
Workspace/Linux/cmake/x64/Debug> cmake.exe -G Ninja ../../../../.. -DCMAKE_TOOLCHAIN_FILE=../../../Toolchain.cmake -DEC_OS=Linux -DEC_ARCH=x64 -DCMAKE_BUILD_TYPE=Debug Workspace/Linux/cmake/x64/Debug> ninja.exe EcMasterDemo
- Cross build using Eclipse CDT on Windows
Download and install the latest version of Eclipse CDT from the Eclipse official website https://projects.eclipse.org/projects/tools.cdt
Create a start batch file for eclipse
set PATH=C:\MinGW\bin;C:\MinGW\msys\1.0\bin;%LINUX_CROSS_GCC_ARM_PATH%;%PATH% set LINUX_CROSS_GCC_ARM_PATH=C:\MinGW\opt\gcc-linaro-7.3.1-2018.05-i686-mingw32_aarch64-linux-gnu\bin set CFLAGS=-IC:\MinGW\opt\gcc-linaro-7.3.1-2018.05-i686-mingw32_aarch64-linux-gnu\aarch64-linux-gnu\libc\usr\include set CROSS_COMPILE=aarch64-linux-gnu- set ARCH=aarch64 eclipse.exe