9.5. Diagnosis
9.5.1. emonGetDiagnosisImagePtr
-
EC_T_BYTE *emonGetDiagnosisImagePtr(EC_T_DWORD dwInstanceID)
Gets the diagnosis image pointer.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns:
Diagnosis image pointer
9.5.2. emonGetDiagnosisImageSize
-
EC_T_DWORD emonGetDiagnosisImageSize(EC_T_DWORD dwInstanceID)
Gets the diagnosis image size.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns:
Diagnosis image size
9.5.3. emonGetMasterSyncUnitInfoNumOf
-
EC_T_DWORD emonGetMasterSyncUnitInfoNumOf(EC_T_DWORD dwInstanceID)
Get number of Master Sync Units info entries.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns:
Number of Master Sync Units info entries
9.5.4. emonGetMasterSyncUnitInfo
-
EC_T_DWORD emonGetMasterSyncUnitInfo(EC_T_DWORD dwInstanceID, EC_T_WORD wMsuId, EC_T_MSU_INFO *pMsuInfo)
Get information about specific Master Sync Unit.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
wMsuId – [in] Master Sync Unit to get the information from
pMsuInfo – [out] Pointer to an EC_T_MSU_INFO structure receiving the Master Sync Unit information
- Returns:
EC_E_NOERROR or error code
MSU_ID_ALL_INFO_ENTRIES retrieves the information from all master sync units at once. The application must ensure that pMsuInfo is capable for all entries.
-
struct EC_T_MSU_INFO
Public Members
-
EC_T_WORD wMsuId
[out] Master Sync Unit ID (ENI: Slave/ProcessData/RxPdo[1..4]@Su, Slave/ProcessData/TxPdo[1..4]@Su, comment at Cyclic/Frame/Cmd)
-
EC_T_DWORD dwBitOffsIn
[out] Process Data Image INPUTs bit offset
-
EC_T_DWORD dwBitSizeIn
[out] Process Data Image INPUTs bit length
-
EC_T_DWORD dwBitOffsOut
[out] Process Data Image OUTPUTs bit offset
-
EC_T_DWORD dwBitSizeOut
[out] Process Data Image OUTPUTs bit length
-
EC_T_WORD wWkcStateDiagOffsIn
[out] INPUTs WkcState bit offset in Diagnosis Image. (Bit values: 0 = Process Data valid, 1 = Process Data invalid)
-
EC_T_WORD wWkcStateDiagOffsOut
[out] OUTPUTs WkcState bit offset in Diagnosis Image. (Bit values: 0 = Process Data valid, 1 = Process Data invalid)
-
EC_T_DWORD adwReserved[16]
reserved
-
EC_T_WORD wMsuId
See also
9.5.5. emonGetSlaveStatistics
-
EC_T_DWORD emonGetSlaveStatistics(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_SLVSTATISTICS_DESC *pSlaveStatisticsDesc)
Get Slave’s statistics counter.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave id
pSlaveStatisticsDesc – [out] Pointer to structure EC_T_SLVSTATISTICS_DESC
- Returns:
EC_E_NOERROR or error code
9.5.6. emonIoControl - EC_IOCTL_GET_SLVSTATISTICS
Get Slave’s statistics counter. Counters are collected on a regularly base (default: off) and show errors on Real-time Ethernet Drivers.
- emonIoControl - EC_IOCTL_GET_SLVSTATISTICS
- Parameter
pbyInBuf: [in] Pointer to a EC_T_DWORD type variable containing the slave id.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Pointer to struct EC_T_SLVSTATISTICS_DESCdwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
-
struct EC_T_SLVSTATISTICS_DESC
Public Members
-
EC_T_BYTE abyInvalidFrameCnt[ESC_PORT_COUNT]
[out] Invalid Frame Counters per Slave Port
-
EC_T_BYTE abyRxErrorCnt[ESC_PORT_COUNT]
[out] RX Error Counters per Slave Port
-
EC_T_BYTE abyFwdRxErrorCnt[ESC_PORT_COUNT]
[out] Forwarded RX Error Counters per Slave Port
-
EC_T_BYTE byProcessingUnitErrorCnt
[out] Processing Unit Error Counter
-
EC_T_BYTE byPdiErrorCnt
[out] PDI Error Counter
-
EC_T_WORD wAlStatusCode
[out] AL Status Code
-
EC_T_BYTE abyLostLinkCnt[ESC_PORT_COUNT]
[out] Lost Link Counters per Slave Port
-
EC_T_UINT64 qwReadTime
[out] Timestamp of the last read [ns]
-
EC_T_UINT64 qwChangeTime
[out] Timestamp of the last counter change [ns]
-
EC_T_BYTE abyInvalidFrameCnt[ESC_PORT_COUNT]
9.5.7. emonClearSlaveStatistics
-
EC_T_DWORD emonClearSlaveStatistics(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId)
Clears all error registers of a slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave Id, INVALID_SLAVE_ID clears all slaves
- Returns:
EC_E_NOERROR or error code
Note
Only the buffered error register values are deleted. The actual counters on the slaves remain unchanged.
See also
9.5.8. emonIoControl - EC_IOCTL_CLR_SLVSTATISTICS
Clear all buffered error registers for all slaves. The actual counters on the slaves remain unchanged.
- emonIoControl - EC_IOCTL_CLR_SLVSTATISTICS
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
9.5.9. emonIoControl - EC_IOCTL_SB_STATUS_GET
This call will get the status of the last bus scan.
- emonIoControl - EC_IOCTL_SB_STATUS_GET
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_SB_STATUS_NTFY_DESC.dwOutBufSize: [in] Size of the output buffer in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
See also