11. RAS-Server for EC-Inspector and EC-Engineer

11.1. Integration Requirements

To use the diagnosis tool EC-Inspector with a customer application, some modifications have to be done during integration of the EC-Monitor. The task is to integrate and start the Remote API Server system within the custom application, which provides a socket based uplink, which later on is connected by the EC-Inspector.

skinparam monochrome true
skinparam SequenceMessageAlign direction

node "EC-Inspector" {
    [RAS-Client]
}
node "EC-Monitor application" {
    [RAS-Server]
    [EC-Monitor core]
}

[RAS-Client] - [RAS-Server]
[RAS-Server] - [EC-Monitor core]

An example on how to integrate the Remote API Server within the application is given with the example application, which in case is pre-configured to listen for EC-Inspector on TCP Port 6000 when command line parameter “-sp” is given.

To clarify the steps, which are needed within a custom application, a developer may use the following pseudo-code segment as a point of start. The Remote API Server library “EcMonitorRasServer.lib” (or respectively “EcMonitorRasServer.a”) must be linked.

11.2. Application programming interface

11.2.1. emonRasSrvStart

EC_T_DWORD EC_NAMESPACE::emonRasSrvStart(ECMASTERRAS_T_SRVPARMS *pParms, EC_T_PVOID *ppHandle)

Initializes and start remote API Server Instance.

The Remote API Server will be initialized and started by calling this function.

Parameters:
  • pParms – [in] Server start-up parameters

  • ppHandle – [out] Handle to opened instance, used for ctrl access

Returns:

EC_E_NOERROR or error code

struct ECMASTERRAS_T_SRVPARMS

RAS Server init parameters.

Public Members

EC_T_DWORD dwSignature

[in] Set to ECMASTERRASSERVER_SIGNATURE

EC_T_DWORD dwSize

[in] Set to sizeof(ECMASTERRAS_T_SRVPARMS)

EC_T_LOG_PARMS LogParms

[in] Logging parameters

EC_T_IPADDR oAddr

[in] Remote Access Server (RAS) listen IP address

EC_T_WORD wPort

[in] Remote Access Server (RAS) listen port

EC_T_WORD wMaxClientCnt

[in] Max. clients in parallel (0: unlimited)

EC_T_DWORD dwCycleTime

[in] Cycle Time of RAS Network access (acceptor, worker)

EC_T_DWORD dwCommunicationTimeout

[in] timeout before automatically closing connection

EC_T_CPUSET oAcceptorThreadCpuAffinityMask

[in] Acceptor Thread CPU affinity mask

EC_T_DWORD dwAcceptorThreadPrio

[in] Acceptor Thread Priority

EC_T_DWORD dwAcceptorThreadStackSize

[in] Acceptor Thread Stack Size

EC_T_CPUSET oClientWorkerThreadCpuAffinityMask

[in] Client Worker Thread CPU affinity mask

EC_T_DWORD dwClientWorkerThreadPrio

[in] Client Worker Thread Priority

EC_T_DWORD dwClientWorkerThreadStackSize

[in] Client Worker Thread Stack Size

EC_T_DWORD dwMaxQueuedNotificationCnt

[in] Amount of concurrently queue able Notifications

EC_T_DWORD dwMaxParallelMbxTferCnt

[in] Amount of concurrent active mailbox transfers

EC_PF_NOTIFY pfnRasNotify

[in] Function pointer called to notify error and status information generated by Remote API Layer

EC_T_VOID *pvRasNotifyCtxt

[in] Notification context returned while calling pfNotification

EC_T_DWORD dwCycErrInterval

[in] Interval which allows cyclic Notifications

EC_T_DWORD dwMaxQueuedNotificationSize

[in] Size of concurrent active mailbox transfers

EC_PF_CHECK_TOKEN pfCheckToken

[in] Function pointer called to check token

EC_T_VOID *pvCheckTokenContext

[in] Check token context

EC_T_BYTE *pbyTlsCert

[in] TLS certificate filename string

EC_T_DWORD dwTlsCertSize

[in] Size of TLS certeficate

EC_T_TLS_CERT_TYPE eTlsCertType

[in] TLS certeficate type

EC_T_BYTE *pbyTlsPrivKey

[in] TLS private key filename string

EC_T_DWORD dwTlsPrivKeySize

[in] Size of TLS private key

EC_T_TLS_PRIVKEY_TYPE eTlsPrivKeyType

[in] TLS certeficate type

ECMASTERRAS_T_SRV_SOCKETBYAPP_DESC *pSocketByAppDesc

[in] Socket by app parameters

union EC_T_IPADDR
#include <EthernetServices.h>

Public Members

EC_T_INNER_IPADDR sAddr

IPv4 address (endianness independent)

EC_T_DWORD dwAddr

Reserved, use EC_T_IPADDR::sAddr.by instead. OS-Layer socket API calls (SOCKADDR_IN::sin_addr)

struct EC_T_INNER_IPADDR

Public Members

EC_T_BYTE by[4]

IPv4 address (endianness independent)

11.2.2. emonRasSrvStop

EC_T_DWORD EC_NAMESPACE::emonRasSrvStop(EC_T_PVOID pvHandle, EC_T_DWORD dwTimeout)

Stop and de-initialize remote API Server Instance.

Parameters:
  • pvHandle – [in] Handle to previously started Server

  • dwTimeout – [in] Timeout [ms] used to shut down all spawned threads, it’s multiplied internally by the amount of threads spawned.

Returns:

EC_E_NOERROR or error code

11.2.3. emonRasNotify

Callback function called by Remote API Server in case of State changes or error situations.

typedef EC_T_DWORD (*EC_PF_NOTIFY)(EC_T_DWORD dwCode, EC_T_NOTIFYPARMS *pParms)

11.2.4. emonRasNotify - ECMASTERRAS_NOTIFY_CONNECTION

Notification about a change in the Remote API’s state.

emonRasNotify - ECMASTERRAS_T_CONNOTIFYDESC
Parameter
  • pbyInBuf: [in] Pointer to data of type ECMASTERRAS_T_CONNOTIFYDESC

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

struct ECMASTERRAS_T_CONNOTIFYDESC

Public Members

EC_T_DWORD dwCause

[in] Cause of state connection state change

EC_T_DWORD dwCookie

[in] Unique identification cookie of connection instance.

11.2.5. emonRasNotify - ECMASTERRAS_NOTIFY_REGISTER

Notification about a connected application registered a client to the EC-Monitor.

emonRasNotify - ECMASTERRAS_NOTIFY_REGISTER
Parameter
  • pbyInBuf: [in] Pointer to data of type ECMASTERRAS_T_REGNOTIFYDESC

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

struct ECMASTERRAS_T_REGNOTIFYDESC

Public Members

EC_T_DWORD dwCookie

[in] Unique identification cookie of connection instance

EC_T_DWORD dwResult

[in] Result of registration request

EC_T_DWORD dwInstanceId

[in] Master Instance client registered to

EC_T_DWORD dwClientId

[in] Client ID of registered client

11.2.6. emonRasNotify - ECMASTERRAS_NOTIFY_UNREGISTER

Notification about a connected application un-registered a client from the EC-Monitor.

emonRasNotify - ECMASTERRAS_NOTIFY_UNREGISTER
Parameter
  • pbyInBuf: [in] Pointer to data of type ECMASTERRAS_T_REGNOTIFYDESC

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

11.2.7. emonRasNotify - ECMASTERRAS_NOTIFY_MARSHALERROR

Notification about an error during marshalling in Remote API Server connection layer.

emonRasNotify - ECMASTERRAS_NOTIFY_MARSHALERRORDESC
Parameter
  • pbyInBuf: [in] Pointer to data of type ECMASTERRAS_T_MARSHALERRORDESC

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

struct ECMASTERRAS_T_MARSHALERRORDESC

Public Members

EC_T_DWORD dwCookie

[in] Unique identification cookie of connection instance

EC_T_DWORD dwCause

[in] Cause of the command marshalling error

EC_T_DWORD dwLenStatCmd

[in] Length faulty command

EC_T_DWORD dwCommandCode

[in] Command code of faulty command

11.2.8. emonRasNotify - ECMASTERRAS_NOTIFY_ACKERROR

Notification about an error during creation of ack / nack packet.

emonRasNotify - ECMASTERRAS_NOTIFY_ACKERROR
Parameter
  • pbyInBuf: [in] Pointer to EC_T_DWORD containing error code

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

11.2.9. emonRasNotify - ECMASTERRAS_NOTIFY_NONOTIFYMEMORY

Notification given, when no empty buffers for notifications are available in pre-allocated notification store. This points to a configuration error.

emonRasNotify - ECMASTERRAS_NOTIFY_NONOTIFYMEMORY
Parameter
  • pbyInBuf: [in] Pointer to EC_T_DWORD containing unique identification cookie of connection instance

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

11.2.10. emonRasNotify - ECMASTERRAS_NOTIFY_STDNOTIFYMEMORYSMALL

Notification given, when buffersize for standard notifications available in pre-allocated notification store are too small to carry a specific notification. This points to a configuration error.

emonRasNotify - ECMASTERRAS_NOTIFY_STDNOTIFYMEMORYSMALL
Parameter
  • pbyInBuf: [in] Pointer to EC_T_DWORD containing unique identification cookie of connection instance

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

11.2.11. emonRasNotify - ECMASTERRAS_NOTIFY_MBXNOTIFYMEMORYSMALL

Notification given, when buffer size for Mailbox notifications available in pre-allocated notification store are too small to carry a specific notification. This points to a configuration error. This is a serious error. If this error is given, Mailbox Transfer objects may have been become out of sync and therefore no more valid usable. Mailbox notifications should be dimensioned correctly see emonRasSrvStart()

emonRasNotify - ECMASTERRAS_NOTIFY_MBXNOTIFYMEMORYSMALL
Parameter
  • pbyInBuf: [in] Pointer to EC_T_DWORD containing unique identification cookie of connection instance

  • dwInBufSize: [in] Size of the input buffer in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL