8.7. Linux SockRaw - emllSockRaw

emllSockRaw is part of EC-Monitor for Linux. emllSockRaw uses the native network adapter, e.g. eth0, eth1, etc . The network adapter must be exclusively used for EtherCAT and cannot be used for LAN (local area network) at the same time. Because the native Linux driver for the network adapter type is typically not fully real-time capable, it cannot be used for real time applications. If possible, an acontis Real-time Ethernet Driver, e.g. emllIntelGbe, should be used instead. emllSockRaw does not need the atemsys driver.

Note

Root privileges are required. A cycle time of 4 ms or higher may be needed.

To run the application without root privileges, set the Linux capability ‘cap_net_raw’ to the application.
$ sudo setcap 'cap_net_raw+pe' ./EcMasterDemo
To run python scripts without root privileges, create a python environment and set the Linux capability ‘cap_net_raw’ to the python interpreter.
$ cd Bin/Linux
$ python3 -m venv --copies PyEnv/
$ source PyEnv/bin/activate
$ sudo setcap 'cap_net_raw+pe' PyEnv/bin/python3

The parameters to emllSockRaw are setup-specific. The function CreateLinkParmsFromCmdLineSockRaw() in EcSelectLinkLayer.cpp demonstrates how to initialize the parameters.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_SOCKRAW

Native ETH device name, e.g. “eth0” (zero terminated)

Don’t change target MAC address to FF:FF:FF:FF:FF:FF

Prevent adding Ethernet padding to work-around EtherCAT corruption bugs from native Linux driver(s).

Use PACKET_MMAP PACKET_RX_RING for receive

Set Coalescing parameters to enhance the link layer performance

Enable promiscuous mode at network adapter