6.1. Header files
Function prototypes, definitions etc. of the API can be found in the header file EcSimulator.h which is the main header file to include when using EC-Simulator.
6.2. Generic API return status values
Most of the functions and also some notifications will return an error status value to indicate whether a function was successfully executed or not. Some of the return status values have a generic meaning unspecific to the called API function.
EC_E_NOERROR: The function was successfully executed.
EC_E_NOTSUPPORTED: Unsupported feature or functionality.
EC_E_BUSY: The stack currently is busy and the function has to be re-tried at a later time.
EC_E_NOMEMORY: Not enough memory or frame buffer resources available.
EC_E_INVALIDPARM: Invalid or inconsistent parameters.
EC_E_TIMEOUT: Timeout error.
EC_E_SLAVE_ERROR: A slave error was detected.
EC_E_INVALID_SLAVE_STATE: The slave is not in the requested state to execute the operation (e.g. when initiating a mailbox transfer the slave must be at least in PREOP state).
EC_E_SLAVE_NOT_ADDRESSABLE: The slave does not respond to its station address (e.g. when requesting its AL_STATUS value). The slave may be removed from the bus or powered-off.
EC_E_LINK_DISCONNECTED: Link cable not connected.
EC_E_MASTERCORE_INACCESSIBLE: Master core inaccessible. This result code usually means a remote connected server / EC-Simulator stack does not respond anymore
6.3. Multiple EtherCAT Network Support
6.3.1. Overview
The acontis EC-Simulator stack supports multiple EtherCAT network instances within the same application process. The first parameter of all esXxx API functions is the Instance ID, starting with 0. The maximum Instance ID of the EC-Simulator SDK is defined as MAX_NUMOF_SIMULATOR_INTERFACES - 1. Implementing multiple EtherCAT network instances is realized by using multiple Instance IDs.
The Real-time Ethernet Driver can be of same or different type (emllPcap, emllIntelGbe, …).
6.3.2. Licensing
For each network identified with the unique Instance ID a separate runtime license is required.
6.4. General functions
6.4.1. esInitSimulator
-
EC_T_DWORD esInitSimulator(EC_T_DWORD dwInstanceId, EC_T_SIMULATOR_INIT_PARMS *pParms)
Initialize EC-Simulator HiL.
This function has to be called prior to calling any other function of EC-Simulator HiL. For EC-Simulator SiL (emllSimulator) this function is implicitely called by emInitMaster() and may not be called explicitely.
- Parameters:
dwInstanceId – [in] Simulator Instance ID
pParms – [in] Pointer to init parameters
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_SIMULATOR_INIT_PARMS
Public Members
-
EC_T_OS_PARMS *pOsParms
[in] OS layer parameters
-
EC_T_LINK_PARMS *apLinkParms[EC_SIMULATOR_MAX_LINK_PARMS]
[in] Link layer parameters
-
EC_T_SIMULATOR_DEVICE_CONNECTION_DESC aoDeviceConnection[EC_SIMULATOR_MAX_LINK_PARMS]
[in] see EC_SIMULATOR_DEVICE_CONNECTION_TYPE_…
-
EC_T_BOOL bConnectHcGroups
[in] connect hot connect groups in topology (floating group heads to free ports)
-
EC_T_PERF_MEAS_INTERNAL_PARMS PerfMeasInternalParms
[in] Internal performance measurement parameters
-
EC_T_OS_PARMS *pOsParms
-
struct EC_T_OS_PARMS
Public Members
-
EC_T_LOG_PARMS *pLogParms
[in] Pointer to logging parameters
-
EC_T_LOG_PARMS *pLogParms
-
struct EC_T_LOG_PARMS
Public Members
-
EC_T_DWORD dwLogLevel
[in] Log level. See EC_LOG_LEVEL_…
-
EC_PF_LOGMSGHK pfLogMsg
[in] Log callback function called on every message
-
EC_T_DWORD dwLogLevel
EC_LOG_LEVEL… The following log levels are defined:
-
typedef EC_T_DWORD (*EC_PF_LOGMSGHK)(EC_T_LOG_CONTEXT *pContext, EC_T_DWORD dwLogMsgSeverity, const EC_T_CHAR *szFormat, ...)
- Param pContext:
[in] Context pointer. This pointer is used as parameter when the callback function is called
- Param dwLogMsgSeverity:
[in] Log message severity, EC_LOG_LEVEL_…
- Param szFormat:
[in] String that contains the text to be written. It can optionally contain embedded format specifiers that are replaced by the values specified in subsequent additional arguments and formatted as requested.
- Return:
EC_E_NOERROR or error code
Log messages are passed from the EC-Simulator to the callback given at EC_T_LOG_PARMS::pfLogMsg. EcLogging.cpp demonstrates how messages can be handled by the application.
For performance reasons the EC-Simulator automatically filters log messages according to EC_T_LOG_PARMS::dwLogLevel. E.g. messages of severity EC_LOG_LEVEL_WARNING are not passed to the application if EC_T_LOG_PARMS::dwLogLevel is set to EC_LOG_LEVEL_ERROR.
The application can provide customized log message handlers of type EC_PF_LOGMSGHK if the default handler in EcLogging.cpp does not fulfill the application’s needs. Note: The callback is typically called from the Job Task’s context and should return as fast as possible.
-
struct EC_T_PERF_MEAS_INTERNAL_PARMS
Public Members
-
EC_T_PERF_MEAS_COUNTER_PARMS CounterParms
[in] Timer function settings. When not provided OsMeasGetCounterTicks is used
-
EC_T_PERF_MEAS_HISTOGRAM_PARMS HistogramParms
[in] Histogram settings. When not provided the histogram is disabled.
-
EC_T_PERF_MEAS_COUNTER_PARMS CounterParms
-
struct EC_T_PERF_MEAS_COUNTER_PARMS
Public Members
-
EC_PF_PERF_MEAS_GETCOUNTERTICKS pfGetCounterTicks
[in] Function returning the current counter ticks
-
EC_PF_PERF_MEAS_GETCOUNTERTICKS pfGetCounterTicks
6.4.2. esDeinitSimulator
-
EC_T_DWORD esDeinitSimulator(EC_T_DWORD dwInstanceId)
Deinitialize EC-Simulator HiL.
Waits for pending API calls if esInitSimulator() was called with EC_T_SIMULATOR_INIT_PARMS::bApiLockByApp = EC_FALSE (default). For EC-Simulator SiL (emllSimulator) this function is implicitely called by emDeinitMaster() and may not be called explicitely.
- Parameters:
dwInstanceId – [in] Simulator Instance ID
- Returns:
EC_E_NOERROR or error code
6.4.3. esGetSimulatorParms
-
EC_T_DWORD esGetSimulatorParms(EC_T_DWORD dwInstanceId, EC_T_SIMULATOR_INIT_PARMS *pParms, EC_T_DWORD dwParmsBufSize)
Get Simulator parameters provided by esInitSimulator(…) or esSetSimulatorParms(…).
- Parameters:
dwInstanceId – [in] Simulator Instance ID
pParms – [out] Pointer to simulator parameters
dwParmsBufSize – [in] Size of buffer at pParms
- Returns:
EC_E_NOERROR or error code
See also
6.4.4. esSetSimulatorParms
-
EC_T_DWORD esSetSimulatorParms(EC_T_DWORD dwInstanceId, EC_T_SIMULATOR_INIT_PARMS *pParms)
Change Simulator parameters provided by esInitSimulator(…).
- Parameters:
dwInstanceId – [in] Simulator Instance ID
pParms – [in] Pointer to simulator parameters
- Returns:
EC_E_NOERROR or error code
See also
6.4.5. esSetLogParms
-
EC_T_DWORD esSetLogParms(EC_T_DWORD dwInstanceID, EC_T_LOG_PARMS *pLogParms)
Sets log parameters. Used to change the parameters provided by esInitSimulator().
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pLogParms – [in] New Log parameters
See also
See also
6.4.6. esGetSrcMacAddress
-
EC_T_DWORD esGetSrcMacAddress(EC_T_DWORD dwInstanceID, ETHERNET_ADDRESS *pMacSrc)
Gets the source MAC address.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMacSrc – [out] 6-byte buffer to write source MAC address to.
- Returns:
EC_E_NOERROR or error code
Refers to adapter from EC_T_SIMULATOR_INIT_PARMS.pLinkParms at esInitSimulator().
6.4.7. esSetLicenseKey (HiL)
-
EC_T_DWORD esSetLicenseKey(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szLicenseKey)
Sets the license key for the protected version of EC-Master.
Must be called after initialization and before configuration. This function may not be called if a non protected version is used.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
szLicenseKey – [in] License key as zero terminated string with 26, 53 or 56 characters.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_INVALIDSIZE the format of the license key is wrong. The correct length is 26, 53 or 56 characters
EC_E_LICENSE_MISSING the license key doesn’t match the MAC Address
Must be called after esInitSimulator() and before esConfigureNetwork().This function may not be called if a non protected version is used.
Example:
dwRes = esSetLicenseKey(dwInstanceID, "DA1099F2-15C249E9-54327FBC");
6.4.8. esSetOemKey (HiL)
Must be called after esInitSimulator() and before esConfigureNetwork().
Example:
dwRes = esSetOemKey(dwInstanceID, 0x1234567812345678);
6.4.9. esConfigureNetwork
-
EC_T_DWORD esConfigureNetwork(EC_T_DWORD dwInstanceID, EC_T_CNF_TYPE eCnfType, EC_T_PBYTE pbyCnfData, EC_T_DWORD dwCnfDataLen)
Configure the Network.
This function must be called after the initialization. Among others the EtherCAT topology defined in the given XML configuration file will be stored internally.
Analyzing the network including mailbox communication can be done without specifying an ENI file using eCnfType_GenPreopENI.
Note
A client must not be registered prior to calling this function. Existing client registrations will be dropped.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
eCnfType – [in] Type of configuration data provided
pbyCnfData – [in] Filename / configuration data, or EC_NULL if eCnfType is eCnfType_GenPreopENI
dwCnfDataLen – [in] Length of configuration data in byte, or zero if eCnfType is eCnfType_GenPreopENI
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized or eCnfType is eCnfType_GenPreopENI or eCnfType_GenOpENI and link is disconnected
EC_E_INVALIDPARM if dwInstanceID is out of range or pParms is EC_NULL contains some values out of range
EC_E_LINK_DISCONNECTED if link is disconnected
EC_E_FEATURE_DISABLED if a configured feature is not included in the license key
EC_E_NOTSUPPORTED if a configured feature is not supported (e.g not compiled in the library)
EC_E_CFGFILENOTFOUND if the ENI file cannot be found
EC_E_WRONG_FORMAT if some format error have been detected in the ENI or EEPROM in case of eCnfType_GenPreopENI or eCnfType_GenOpENI
EC_E_OEM_SIGNATURE_MISMATCH if the OEM signature in the ENI file doesn’t match the used OEM key
EC_E_ENI_ENCRYPTION_WRONG_VERSION if the ENI encryption version is not supported (e.g. the library is too old)
EC_E_ENI_ENCRYPTED if the ENI is encrypted and no OEM key has been set
EC_E_XML_CYCCMDS_MISSING if the ENI doesn’t contain cyclic commands
EC_E_XML_ALSTATUS_READ_MISSING if the ENI doesn’t contain any read AL status command
EC_E_XML_CYCCMDS_SIZEMISMATCH if the size of the cyclic commands in the ENI mismatch
EC_E_XML_INVALID_INP_OFF if some input offset in the ENI are invalid
EC_E_XML_INVALID_OUT_OFF if some output offset in the ENI are invalid
EC_E_XML_INVALID_CMD_WITH_RED if the ENI contains LRW commands and cable redundancy is configured
EC_E_XML_PREV_PORT_MISSING if some previous port information are missing in the ENI
EC_E_XML_DC_CYCCMDS_MISSING if the DC related cyclic commands are missing in the ENI
EC_E_XML_AOE_NETID_INVALID if the ENI contains some invalid NetID
-
enum EC_T_CNF_TYPE
Values:
-
enumerator eCnfType_GenOpENI
Generate ENI based on bus-scan result to get into OP state. The default PDO mapping read from the slaves is activated. See ETG2010 “SII Specification”, Table 14 “Structure Category TXPDO and RXPDO for each PDO”
-
enumerator eCnfType_GenOpENI
6.4.10. esGetCfgSlaveInfo
-
EC_T_DWORD esGetCfgSlaveInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_CFG_SLAVE_INFO *pSlaveInfo)
Return information about a configured slave from the ENI file.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
pSlaveInfo – [out] Information about the slave.
- Returns:
EC_E_NOERROR or error code
Content of EC_T_CFG_SLAVE_INFO is subject to be extended.
-
struct EC_T_CFG_SLAVE_INFO
Public Members
-
EC_T_CHAR abyDeviceName[ECAT_DEVICE_NAMESIZE]
[out] Slave’s configured name (80 Byte) (from ENI file)
-
EC_T_DWORD dwMbxSupportedProtocols
[out] Mailbox protocols supported by the slave (from ENI file). Combination of Supported mailbox protocols flags
-
EC_T_WORD wWkcStateDiagOffsIn[EC_CFG_SLAVE_PD_SECTIONS]
[out] Offset of WkcState bit in diagnosis image (ENI: ProcessData/Recv[1..4]/BitStart): 0xFFFFFFFF = offset not available. WkcState bit values: 0 = Data valid, 1 = Data invalid
-
EC_T_WORD wWkcStateDiagOffsOut[EC_CFG_SLAVE_PD_SECTIONS]
[out] Offset of WkcState bit in diagnosis image (ENI: ProcessData/Send[1..4]/BitStart): 0xFFFFFFFF = offset not available. WkcState bit values: 0 = Data valid, 1 = Data invalid
-
EC_T_WORD awMasterSyncUnitIn[EC_CFG_SLAVE_PD_SECTIONS]
[out] Sync Unit (ENI: ProcessData/TxPdo[1..4]@Su)
-
EC_T_WORD awMasterSyncUnitOut[EC_CFG_SLAVE_PD_SECTIONS]
[out] Sync Unit (ENI: ProcessData/RxPdo[1..4]@Su)
-
EC_T_BOOL bDisconnected
[out] Slave disconnected by API SetSlaveDisconnected / SetSlavesDisconnected.
-
EC_T_CHAR abyDeviceName[ECAT_DEVICE_NAMESIZE]
Supported mailbox protocols flags
esGetCfgSlaveInfo() Example
/* get information about slave configured in ENI file */
EC_T_CFG_SLAVE_INFO oSlaveInfo;
OsMemset(&oSlaveInfo, 0, sizeof(EC_T_CFG_SLAVE_INFO));
dwRes = esGetCfgSlaveInfo(dwInstanceId, EC_TRUE, 1001, &oSlaveInfo);
6.4.11. esGetCfgSlaveSmInfo
-
EC_T_DWORD esGetCfgSlaveSmInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_CFG_SLAVE_SM_INFO *pSlaveSmInfo)
Return SyncManager information of a configured slave from the ENI file.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
pSlaveSmInfo – [out] Slave SyncManager information
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_CFG_SLAVE_SM_INFO
Public Members
-
EC_T_CFG_SLAVE_SM_ENTRY aoSmInfos[ECREG_SYNCMANAGER_MAX_NUMOF]
[out] Sync managers info
-
EC_T_CFG_SLAVE_SM_ENTRY aoSmInfos[ECREG_SYNCMANAGER_MAX_NUMOF]
esGetCfgSlaveSmInfo() Example
/* get information about slave's sync managers configured in ENI file */
EC_T_CFG_SLAVE_SM_INFO oSlaveSmInfo;
OsMemset(&oSlaveSmInfo, 0, sizeof(EC_T_CFG_SLAVE_SM_INFO));
dwRes = esGetCfgSlaveSmInfo(dwInstanceId, EC_TRUE, 1001, &oSlaveSmInfo);
6.4.12. esSetSlaveSscApplication
-
EC_T_DWORD esSetSlaveSscApplication(EC_T_DWORD dwInstanceId, EC_T_WORD wCfgFixedAddress, EC_T_SLAVE_SSC_APPL_DESC *pApp)
Register slave application’s callback functions for slave without device emulation.
- Parameters:
dwInstanceId – [in] Simulator Instance ID
wCfgFixedAddress – [in] Slave’s station address
pApp – [in] Pointer to application descriptor
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_SLAVE_SSC_APPL_DESC
Public Members
-
EC_PF_SSC_APPL_MAIN_INIT pfnMainInit
[in] SSC_APPL-callback for APPL_MainInit, called by SSC when slave initialization finished
-
EC_PF_SSC_APPL_ACK_ERROR_IND pfnAckErrorInd
[in] SSC_APPL-callback for APPL_AckErrorInd, called by SSC on error acknowledge by master
-
EC_PF_SSC_APPL_APPLICATION pfnApplication
[in] SSC_APPL-callback for APPL_Application, called after frame processing
-
EC_PF_SSC_APPL_GET_DEVICE_ID pfnGetDeviceID
[in] SSC_APPL-callback for APPL_GetDeviceID, called by SSC on Explicit Device ID request by master
-
EC_PF_SSC_APPL_START_MAILBOX_HANDLER pfnStartMailboxHandler
[in] SSC_APPL-callback for APPL_StartMailboxHandler, called by SSC on INIT to PREOP and INIT to BOOT transition
-
EC_PF_SSC_APPL_STOP_MAILBOX_HANDLER pfnStopMailboxHandler
[in] SSC_APPL-callback for APPL_StopMailboxHandler, called by SSC on PREOP to INIT and BOOT to INIT transition
-
EC_PF_SSC_APPL_START_INPUT_HANDLER pfnStartInputHandler
[in] SSC_APPL-callback for APPL_StartInputHandler, called by SSC on PREOP to SAFEOP transition (even if no INPUTs configured)
-
EC_PF_SSC_APPL_STOP_INPUT_HANDLER pfnStopInputHandler
[in] SSC_APPL-callback for APPL_StopInputHandler, called by SSC on SAFEOP to PREOP transition (even if no INPUTs configured)
-
EC_PF_SSC_APPL_START_OUTPUT_HANDLER pfnStartOutputHandler
[in] SSC_APPL-callback for APPL_StartOutputHandler, called by SSC on SAFEOP to OP transition (even if no OUTPUTs configured)
-
EC_PF_SSC_APPL_STOP_OUTPUT_HANDLER pfnStopOutputHandler
[in] SSC_APPL-callback for APPL_StopOutputHandler, called by SSC on OP to SAFEOP transition (even if no OUTPUTs configured)
-
EC_PF_SSC_APPL_GENERATE_MAPPING pfnGenerateMapping
[in] SSC_APPL-callback for APPL_GenerateMapping, called by SSC on PREOP to SAFEOP transition
-
EC_PF_SSC_APPL_INPUT_MAPPING pfnInputMapping
[in] SSC_APPL-callback for APPL_InputMapping, called by SSC to map (copy) INPUTs
-
EC_PF_SSC_APPL_OUTPUT_MAPPING pfnOutputMapping
[in] SSC_APPL-callback for APPL_OutputMapping, called by SSC to map (copy) OUTPUTs
-
EC_T_PF_AOE_READ_CB pfnAoeRead
[in] SSC_APPL-callback for APPL_AoeRead, called by SSC on AoE read request
-
EC_T_PF_AOE_WRITE_CB pfnAoeWrite
[in] SSC_APPL-callback for APPL_AoeWrite, called by SSC on AoE write request
-
EC_T_PF_AOE_READWRITE_CB pfnAoeReadWrite
[in] SSC_APPL-callback for APPL_AoeReadWrite, called by SSC on AoE read/write request
-
EC_PF_SSC_APPL_EOE_RECEIVE pfnEoeReceive
[in] SSC_APPL-callback for APPL_EoeReceive, called by SSC on received EoE Ethernet frame completion
-
EC_PF_SSC_APPL_EOE_SETTING_IND pfnEoeSettingInd
[in] SSC_APPL-callback for APPL_EoeSettingInd, called by SSC on EoE settings received
-
EC_PF_SSC_APPL_FOE_WRITE pfnFoeWrite
[in] SSC_APPL-callback for APPL_FoeWrite, called by SSC on FoE write request
-
EC_PF_SSC_APPL_FOE_WRITE_DATA pfnFoeWriteData
[in] SSC_APPL-callback for APPL_FoeWriteData, called by SSC when FoE data received
-
EC_PF_SSC_APPL_FOE_READ pfnFoeRead
[in] SSC_APPL-callback for APPL_FoeRead, called by SSC on FoE read request to transmit first FoE data
-
EC_PF_SSC_APPL_FOE_READ_DATA pfnFoeReadData
[in] SSC_APPL-callback for APPL_FoeReadData, called by SSC to transmit next FoE read data, 2..n
-
EC_PF_SSC_APPL_FOE_ERROR pfnFoeError
[in] SSC_APPL-callback for APPL_FoeError, called by SSC on FoE abort by master
-
EC_PF_SSC_APPL_SET_PROC_VAR_PTR pfnSetProcVarPtr
[in] SSC_APPL-callback for APPL_SetProcVarPtr, called on esConfigureNetwork() for each process data variable
-
EC_PF_SSC_APPL_MAIN_INIT pfnMainInit
6.4.13. esRegisterClient
-
EC_T_DWORD esRegisterClient(EC_T_DWORD dwInstanceID, EC_PF_NOTIFY pfnNotify, EC_T_VOID *pCallerData, EC_T_REGISTERRESULTS *pRegResults)
Register the application as a client with the EtherCAT stack for notifications (EC_NOTIFY_… )
It must be called after configuration, otherwise the registration handle is lost. This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pfnNotify – [in] Notification callback function. This function will be called every time a state change occurs, an error occurs or a mailbox transfer terminates.
pCallerData – [in] Parameter passed to the application when the notification callback is called. The parameter can be arbitrarily defined by the application.
pRegResults – [out] Registration results
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_NOMEMORY if some memory cannot be allocated
-
typedef EC_T_DWORD (*EC_PF_NOTIFY)(EC_T_DWORD dwCode, EC_T_NOTIFYPARMS *pParms)
- Param dwCode:
[in] Notification code, see EC_NOTIFY_…
- Param pParms:
[in] Notification code depending data.
6.4.14. esUnregisterClient
-
EC_T_DWORD esUnregisterClient(EC_T_DWORD dwInstanceID, EC_T_DWORD dwClntId)
Deregister a client from the EtherCAT stack.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwClntId – [in] Client ID from registeration with the EtherCAT stack
- Returns:
EC_E_NOERROR or error code
6.4.15. esExecJob
-
EC_T_DWORD esExecJob(EC_T_DWORD dwInstanceID, EC_T_USER_JOB eUserJob, EC_T_USER_JOB_PARMS *pUserJobParms)
Execute or initiate the requested EtherCAT stack job.
To achieve maximum speed, this function is implemented non re-entrant. It is highly recommended that only one single task is calling all required jobs to run the stack. If multiple tasks are calling this function, the calls have to be synchronized externally. Calling it in a context that doesn’t support operating system calls can lead to unpredictable behavior.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
eUserJob – [in] user requested job
pUserJobParms – [in] optional user job parameters
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_LINK_DISCONNECTED if the link is disconnected
EC_E_FEATURE_DISABLED for eUsrJob_SwitchEoeFrames if EC_IOCTL_SET_EOE_DEFFERED_SWITCHING_ENABLED hasn’t be called before
EC_E_ADS_IS_RUNNING if ADS server is running
Brief job overview:
-
union EC_T_USER_JOB_PARMS
Public Members
-
struct EC_T_USER_JOB_PARMS::_SEND_CYCFRAME_BY_TASKID SendCycFramesByTaskId
-
struct EC_T_USER_JOB_PARMS::_PROCESS_RXFRAME_BY_TASKID ProcessRxFramesByTaskId
-
struct EC_T_USER_JOB_PARMS::_SWITCH_EOE_FRAMES SwitchEoeFrames
-
struct EC_T_USER_JOB_PARMS::_START_TASK StartTask
-
struct EC_T_USER_JOB_PARMS::_STOP_TASK StopTask
-
struct EC_T_USER_JOB_PARMS::_SEND_CYCFRAME_BY_TASKID SendCycFramesByTaskId
Detailed job description:
eUsrJob_ProcessAllRxFramesIf the Real-time Ethernet Driver operates in polling mode this call will process all currently received frames, in interrupt mode all received frames are processed immediately and this call just returns with nothing done.
pUserJobParms->bAllCycFramesProcessed
This flag is set to a value of
EC_TRUEit indicates that all previously initiated cyclic frames (eUsrJob_SendAllCycFrames) are received and processed within this call. Not used if pUserJobParms set toEC_NULL.Return: EC_E_NOERROR if successful, error code in case of failures.
eUsrJob_SimulatorTimerThis has to be called cyclically to trigger the slave state machines, copy process data from simulated slave firmware as well as the mailbox handling. The slave state machines handle the EtherCAT state transitions.
Return: EC_E_NOERROR if successful, error code in case of failures.
6.4.16. esGetMasterState
6.4.17. esIoControl
-
EC_T_DWORD esIoControl(EC_T_DWORD dwInstanceID, EC_T_DWORD dwCode, EC_T_IOCTLPARMS *pParms)
A generic control interface between the application, the EtherCAT stack and its Real-time Ethernet Drivers.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwCode – [in] Control code
pParms – [in/out] Control code depending parameters
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer
EC_E_NOMEMORY if some memory cannot be allocated
EC_E_ADS_IS_RUNNING if ADS server is running
6.4.18. esIoControl - EC_IOCTL_GET_PDMEMORYSIZE
Queries the necessary size the process data image has got. This IOCTL is to be called after esConfigureNetwork.
- esIoControl - EC_IOCTL_GET_PDMEMORYSIZE
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to memory where the memory size information will be stored (EC_T_MEMREQ_DESC)dwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData: [out] Should be set to EC_NULL
6.4.19. esIoControl - EC_IOCTL_REGISTER_CYCFRAME_RX_CB
This function call registers a callback function which is called after the cyclic frame is received. Typically this is used when the Real-time Ethernet Driver operates interrupt mode to get an event when the new input data (cyclic frame) is available.
The callback function has to be registered after calling esConfigureNetwork() before starting the job task.
- esIoControl - EC_IOCTL_REGISTER_CYCFRAME_RX_CB
- Parameter
pbyInBuf: [in] Cyclic frame received callback descriptor (EC_T_CYCFRAME_RX_CBDESC)dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_CYCFRAME_RX_CBDESC
Public Members
-
EC_T_VOID *pCallbackContext
[in] Context pointer. This pointer is used as parameter every time when the callback function is called
-
EC_PF_CYCFRAME_RECV pfnCallback
[in] This function will be called after the cyclic frame is received, if there is more than one cyclic frame after the last frame. The application has to assure that these functions will not block.
-
EC_T_VOID *pCallbackContext
6.4.20. esIoControl - EC_IOCTL_ISLINK_CONNECTED
Determine whether link between the EC-Simulator stack and the first slave is connected.
- esIoControl - EC_IOCTL_ISLINK_CONNECTED
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_DWORD. If value is EC_TRUE link is connected, if EC_FALSE it is not.dwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData: [out] Should be set to EC_NULL
Important
With cable redundancy support enabled, EC_FALSE is only set if all links are down.
6.4.21. esIoControl - EC_IOCTL_GET_CYCLIC_CONFIG_INFO
Get cyclic configuration details from ENI configuration file.
- esIoControl - EC_IOCTL_GET_CYCLIC_CONFIG_INFO
- Parameter
pbyInBuf: [in] Pointer to dwCycEntryIndex: cyclic entry index for which to get informationdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Pointer to EC_T_CYC_CONFIG_DESC data typedwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
6.4.22. esIoControl - EC_IOCTL_ADDITIONAL_VARIABLES_FOR_SPECIFIC_DATA_TYPES
Enable or disable additional variables for specific data types. Default: Enabled.
- esIoControl - EC_IOCTL_ADDITIONAL_VARIABLES_FOR_SPECIFIC_DATA_TYPES
- Parameter
pbyInBuf: [in] Pointer to value of EC_T_BOOL. EC_TRUE: enable, EC_FALSE: disable.dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
6.4.23. esIoControl - EC_IOCTL_SIMULATOR_SET_MBX_PROCESS_CTL
Enable or disable mailbox processing at slave. Default: Enabled.
- esIoControl - EC_IOCTL_SIMULATOR_SET_MBX_PROCESS_CTL
- Parameter
pbyInBuf: [in] Pointer to value of :cpp:struct:`EC_T_SIMULATOR_MBX_PROCESS_CTL_DESC`dwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
6.4.24. esIoControl - EC_IOCTL_SIMULATOR_GET_MBX_PROCESS_CTL
Enable or disable mailbox processing at slave. Default: Enabled.
- esIoControl - EC_IOCTL_SIMULATOR_GET_MBX_PROCESS_CTL
- Parameter
pbyInBuf: [in] Pointer to value of EC_T_WORD. Configured station address of slavedwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Pointer to value of :cpp:struct:`EC_T_SIMULATOR_MBX_PROCESS_CTL_DESC`dwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytespdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
6.4.25. esIoControl - EC_IOCTL_GET_LINKLAYER_MODE
This call allows the application to determine whether the Real-time Ethernet Driver is currently running in polling or in interrupt mode.
- emIoControl - EC_IOCTL_GET_LINKLAYER_MODE
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to struct EC_T_LINKLAYER_MODE_DESCdwOutBufSize: [in] Size of the output buffer in bytes.pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Return
EC_E_NOERROR or error code
-
struct EC_T_LINKLAYER_MODE_DESC
Public Members
-
EC_T_LINKMODE eLinkMode
[out] Operation mode of main interface
-
EC_T_LINKMODE eLinkModeRed
[out] Operation mode of redundancy interface
-
EC_T_LINKMODE eLinkMode
6.4.26. esIoControl - EC_LINKIOCTL_XXXX
With EC_LINKIOCTL_XXXX a generic control interface exists between the application and the EC-Simulator and its Real-time Ethernet Driver.
The generic control interface esIoControl() provides access to the main network adapter when adding EC_IOCTL_LINKLAYER_MAIN to the EC_LINKIOCTL_XXXX parameter at dwCode. EC_IOCTL_LINKLAYER_RED specifies the redundant network adapter.
Parameters pbyInBuf, dwInBufSize, pbyOutBuf, dwOutBufSize, pdwNumOutData are specific to EC_LINKIOCTL_XXXX, e.g. EC_LINKIOCTL_GET_ETHERNET_ADDRESS.
6.4.27. esIoControl - EC_LINKIOCTL_GET_ETHERNET_ADDRESS
Get MAC address of network adapter
- esIoControl - EC_LINKIOCTL_GET_ETHERNET_ADDRESS
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to MAC address buffer (6 bytes)dwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytespdwNumOutData: [out] Pointer to EC_T_DWORD: amount of bytes written to the output buffer
6.4.28. esIoControl - EC_LINKIOCTL_GET_SPEED
Get current network adapter’s speed in MBits.
- esIoControl - EC_LINKIOCTL_GET_SPEED
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_DWORD. Set by Real-time Ethernet Driver to 10/100/1000.dwOutBufSize: [in] Size of the output buffer provided at pbyOutBuf in bytespdwNumOutData: [out] Pointer to EC_T_DWORD: amount of bytes written to the output buffer
6.4.29. esIoControl - EC_LINKIOCTL_GET_PCI_INFO
Get current network adapter’s PCI information
- esIoControl - EC_LINKIOCTL_GET_PCI_INFO
- Parameter
pbyInBuf: [in] Should be set to EC_NULLdwInBufSize: [in] Should be set to 0pbyOutBuf: [out] Pointer to EC_T_PCI_INFO bufferdwOutBufSize: [in] Size of the output buffer in bytes. Must be at least the size of EC_T_PCI_INFOpdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer
-
struct EC_T_PCI_INFO
Public Members
-
EC_T_PCI_INFO_LOCATION Location
PCI location (bus, device, function)
-
EC_T_PCI_INFO_IDENIFICATION Ident
PCI identification (vendor id, device id)
-
EC_T_PCI_INFO_IOBAR aIoBar
PCI I/O bars info
-
EC_T_PCI_INFO_MEMBAR aMemBar
PCI Memory bars info
-
EC_T_PCI_INFO_INTERRUPT aInterrupt
PCI IRQ info
-
EC_T_PCI_INFO_LOCATION Location
6.4.30. esIoControl - EC_LINKIOCTL_FORCE_LINK_STATUS
Forces the current network adapter’s link status
- esIoControl - EC_LINKIOCTL_FORCE_LINK_STATUS
- Parameter
pbyInBuf: [in] Pointer to EC_T_BYTE. See EC_LINK_FORCE_LINK_STATUS_…dwInBufSize: [in] Size of the input buffer in bytes. Must be at least the size of EC_T_BYTEpbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
6.4.31. esGetVersion
-
EC_T_DWORD esGetVersion(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwVersion, EC_T_DWORD *pdwVersionType)
Gets the version information.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwVersion – [out] Pointer to EC_T_DWORD to carry out version number as a 32-bit value
pdwVersionType – [out] Pointer to EC_T_DWORD to carry out version type. See EC_VERSION_TYPE
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
6.4.32. esGetText
6.4.33. esGetMemoryUsage
-
EC_T_DWORD esGetMemoryUsage(EC_T_DWORD dwInstanceID, EC_T_DWORD *pdwCurrentUsage, EC_T_DWORD *pdwMaxUsage)
Returns information about memory usage.
All calls to malloc/free and new/delete are monitored.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pdwCurrentUsage – [out] Current memory usage in Bytes at the time where this function is called
pdwMaxUsage – [out] Maximum memory usage in Bytes since initialization at the time where this function is called
- Returns:
EC_E_NOERROR or error code
6.4.34. esLogFrameEnable
-
EC_T_DWORD esLogFrameEnable(EC_T_DWORD dwInstanceID, EC_T_PFLOGFRAME_CB pvLogFrameCallBack, EC_T_VOID *pvContext)
Setup a callback function to log the EtherCAT network traffic.
The callback function is called by the cyclic task. Therefore the code inside the callback has to be fast and non-blocking. The callback parameter dwLogFlags can be used as a filter to log just specific frames. The master discards the frame if the callback function modifies the Ethernet frame type at byte offset 12.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pvLogFrameCallBack – [in] Pointer to frame logging callback function
pvContext – [in] Pointer to function specific context
- Returns:
EC_E_NOERROR or error code
/********************************************************************************/
/** \brief Handler to log frames.
*
* CAUTION: Called by cyclic task! Do not consume too much CPU time!
*/
EC_T_VOID LogFrameHandler(EC_T_VOID* pvContext, EC_T_DWORD dwLogFlags, EC_T_DWORD dwFrameSize, EC_T_BYTE* pbyFrame)
{
EC_T_STATE eMasterState;
/* get master state */
eMasterState = (EC_T_STATE)(dwLogFlags & EC_LOG_FRAME_FLAG_MASTERSTATE_MASK);
/* skip tx frame */
if ((S_dwLogFrameLevel == 3) && !(dwLogFlags & EC_LOG_FRAME_FLAG_RX_FRAME))
return;
/* skip cyclic frame */
if ((S_dwLogFrameLevel == 2) && !(dwLogFlags & EC_LOG_FRAME_FLAG_ACYC_FRAME))
return;
/* skip red frame */
if (dwLogFlags & EC_LOG_FRAME_FLAG_RED_FRAME)
return;
/* do something with pbyFrame ... */
}
6.4.35. esLogFrameDisable
-
EC_T_DWORD esLogFrameDisable(EC_T_DWORD dwInstanceID)
Disable the frame logging callback.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
- Returns:
EC_E_NOERROR or error code