5.18. emllRemote
The emllRemote is used to tunnel EtherCAT frames within a TCP socket between EC-Master and EC-Simulator.
The parameters to the Remote Driver are setup-specific. The function CreateLinkParmsFromCmdLineRemote() in EcSelectLinkLayer.cpp demonstrates how to initialize the driver instance.
-
struct EC_T_LINK_PARMS_REMOTE
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_REMOTE
-
EC_T_LINK_PARMS linkParms
While EC-Simulator listens on the given port using emllRemote, the EC-Master can connect to it using emllRemote.
- EcSimulatorHilDemo command line example:
EcSimulatorHilDemo -remote 1 0 0.0.0.0 10001 0.0.0.0 0 -f eni.xml- EcMasterDemo command line example:
EcMasterDemo -remote 1 1 0.0.0.0 0 127.0.0.1 10001